Wi-SUN Services#

The Wi-SUN service software components are provided to help and accelerate Wi-SUN application developments by offering common functionalities. They can easily be added to an existing Wi-SUN application through Simplicity Studio graphical interface. The components are shared in source code in the Gecko SDK.

The service components are especially useful to build upon the Wi-SUN - SoC Empty project and start as close as possible to a final application targeted by a developer.

The following diagram shows the software components available for users to leverage in their Wi-SUN application. Moreover, it highlights each component dependencies to other software components. User Component OverviewUser Component Overview

Modules#

Util Functions

Application Core

Application Settings

CoAP

Ping

iPerf

Over-The-Air Device Firmware Upgrade (Alpha)

Trivial File Transfer Protocol (TFTP) Client (Alpha)

Application Memory Statistic (Alpha)

Application Status over CoAP (Alpha)

Silicon Labs socket API (deprecated)

Keychain