Association Group Information#
General information#
CC Association Group Information (CC AGI) reports which commands a device can control and which commands are reported to the Lifeline.
CC AGI configuration#
The Lifeline group is automatically configured, but other groups may be manually configured if desired. For instance, a wall switch might control a bulb using CC Binary Switch. In such case, the wall switch would need to have an association group defined that lists Binary Switch Set. Simplicity Studio / SLC generates this configuration automatically based on user configuration in *.cc_config files.
Example of configuration:
zw_cc_agi:
endpoints:
- endpoint: 0
groups:
- name: BTN0
profile_msb: ASSOCIATION_GROUP_INFO_REPORT_PROFILE_CONTROL
profile_lsb: ASSOCIATION_GROUP_INFO_REPORT_PROFILE_CONTROL_KEY01
commands:
- command_class: COMMAND_CLASS_BASIC_V2
command: BASIC_SET_V2
The specification of CC AGI can be found in https://github.com/Z-Wave-Alliance/AWG/tree/main/source/management_command_classes/command_class_definitions
Modules#
Configuration of CC Association Group Information
Functions#
Returns the number of configured association groups for a given endpoint.
Returns the association group ID that matches the given AGI profile, command class/command-pair and endpoint.
Function Documentation#
CC_AGI_groupCount_handler#
uint8_t CC_AGI_groupCount_handler (uint8_t endpoint)
Returns the number of configured association groups for a given endpoint.
[in] | endpoint | A given endpoint where 0 is the root device. |
This function will return 1 for any endpoint if the node is added to a Z-Wave LR network.
Returns
Number of configured association groups.
67
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Association/src/CC_AssociationGroupInfo.h
cc_agi_get_group_id#
uint8_t cc_agi_get_group_id (agi_profile_t const *const profile, ccc_pair_t const *const cmdGrp, uint8_t const endpoint)
Returns the association group ID that matches the given AGI profile, command class/command-pair and endpoint.
[in] | profile | AGI profile to search for. |
[in] | cmdGrp | Command class / command pair to search for. |
[in] | endpoint | Endpoint. |
Returns
Returns the group ID, if found. Otherwise 0xFF.
78
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Association/src/CC_AssociationGroupInfo.h