GET_INIT_DATA_FLAG#

Flags used in FUNC_ID_SERIAL_API_GET_INIT_DATA functionality.

Macro Definition Documentation#

GET_INIT_DATA_FLAG_SLAVE_API#

#define GET_INIT_DATA_FLAG_SLAVE_API
Value:
0x01

Definition at line 30 of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h

GET_INIT_DATA_FLAG_TIMER_SUPPORT#

#define GET_INIT_DATA_FLAG_TIMER_SUPPORT
Value:
0x02

Definition at line 31 of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h

GET_INIT_DATA_FLAG_CONTROLLER_STATUS#

#define GET_INIT_DATA_FLAG_CONTROLLER_STATUS
Value:
0x04 /* Obsolete. USE next */

Definition at line 32 of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h

GET_INIT_DATA_FLAG_SECONDARY_CTRL#

#define GET_INIT_DATA_FLAG_SECONDARY_CTRL
Value:
0x04

Definition at line 33 of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h

GET_INIT_DATA_FLAG_IS_SUC#

#define GET_INIT_DATA_FLAG_IS_SUC
Value:
0x08

Definition at line 34 of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_SerialAPI.h