Public Attributes#
void(*
uint8_t
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
uint8_t
Public Attribute Documentation#
pHandle#
void(* SCommandNetworkManagementDSK::pHandle) (void)
Definition at line
1766
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
mode#
uint8_t SCommandNetworkManagementDSK::mode
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
Definition at line
1769
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
dsk#
uint8_t SCommandNetworkManagementDSK::dsk[8]
Definition at line
1770
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h