Public Attributes#
uint32_t
Passed 1ms ticks.
uint8_t
Repeaters in route, zero for direct range.
struct s_rssi_val
rssi_values per hop for direct and routed frames.
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
int8_t
int8_t
Public Attribute Documentation#
TransmitTicks#
uint32_t _TX_STATUS_TYPE_::TransmitTicks
Passed 1ms ticks.
Definition at line
144
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bRepeaters#
uint8_t _TX_STATUS_TYPE_::bRepeaters
Repeaters in route, zero for direct range.
Definition at line
145
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
rssi_values#
struct s_rssi_val _TX_STATUS_TYPE_::rssi_values
rssi_values per hop for direct and routed frames.
Contains repeaters + 1 values.
Definition at line
148
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bACKChannelNo#
uint8_t _TX_STATUS_TYPE_::bACKChannelNo
Definition at line
149
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bLastTxChannelNo#
uint8_t _TX_STATUS_TYPE_::bLastTxChannelNo
Definition at line
150
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bRouteSchemeState#
uint8_t _TX_STATUS_TYPE_::bRouteSchemeState
Definition at line
151
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
pLastUsedRoute#
uint8_t _TX_STATUS_TYPE_::pLastUsedRoute[LAST_USED_ROUTE_SIZE]
Definition at line
152
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bRouteTries#
uint8_t _TX_STATUS_TYPE_::bRouteTries
Definition at line
153
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bLastFailedLink#
S_ROUTE_LINK_T _TX_STATUS_TYPE_::bLastFailedLink
Definition at line
154
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bUsedTxpower#
int8_t _TX_STATUS_TYPE_::bUsedTxpower
Definition at line
155
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bMeasuredNoiseFloor#
int8_t _TX_STATUS_TYPE_::bMeasuredNoiseFloor
Definition at line
156
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bDestinationAckUsedTxPower#
int8_t _TX_STATUS_TYPE_::bDestinationAckUsedTxPower
Definition at line
157
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bDestinationAckMeasuredRSSI#
int8_t _TX_STATUS_TYPE_::bDestinationAckMeasuredRSSI
Definition at line
158
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bDestinationAckMeasuredNoiseFloor#
int8_t _TX_STATUS_TYPE_::bDestinationAckMeasuredNoiseFloor
Definition at line
159
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h