Network Management#

Functions#

void

Command to set the maximum inclusion request interval.

void
ZAF_SendINIF(void(*pCallback)(uint8_t txStatus, TX_STATUS_TYPE *extendedTxStatus))

Broadcasts an Included Node Information Frame (INIF).

Function Documentation#

ZAF_SetMaxInclusionRequestIntervals#

void ZAF_SetMaxInclusionRequestIntervals (uint32_t intervals)

Command to set the maximum inclusion request interval.

Parameters
N/Aintervals

The maximum number of seconds in units of 128sec/tick in between SmartStart inclusion requests. Valid range 0 and 5-99. 0 is default value and corresponds to 512 sec. The range 5-99 corresponds to 640-12672sec.

A status message with type=EZWAVECOMMANDSTATUS_ZW_SET_MAX_INCL_REQ_INTERVALS is returned to the application command status queue when the command has completed.


Definition at line 37 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_network_management.h

ZAF_SendINIF#

void ZAF_SendINIF (void(*)(uint8_t txStatus, TX_STATUS_TYPE *extendedTxStatus) pCallback)

Broadcasts an Included Node Information Frame (INIF).

Parameters
N/ApCallback

Pointer to a callback function that will be invoked when transmission is successful or has failed.


Definition at line 45 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_network_management.h