Node info stored within the non-volatile memory This are the first (protocol part) payload bytes from the Node Infomation frame.

Public Attributes#

uint8_t

Network capabilities.

uint8_t

Network security.

uint8_t

Basic, Generic and Specific Device types - Basic is generated...

Public Attribute Documentation#

capability#

uint8_t _NODEINFO_::capability

Network capabilities.


Definition at line 66 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h

security#

uint8_t _NODEINFO_::security

Network security.


Definition at line 67 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h

reserved#

uint8_t _NODEINFO_::reserved

Definition at line 68 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h

nodeType#

NODE_TYPE _NODEINFO_::nodeType

Basic, Generic and Specific Device types - Basic is generated...


Definition at line 69 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h