Properties of the received frame.
Used mostly by command classes to prepare response to a command.
Public Attributes#
uint8_t
Frame header info.
uint8_t
true if supervision is active
uint8_t
Current sessionId.
uint8_t
Is statusUpdate enabled for current session.
Public Attribute Documentation#
rxStatus#
uint8_t _RECEIVE_OPTIONS_TYPE_EX_::rxStatus
Frame header info.
Definition at line
68
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
securityKey#
security_key_t _RECEIVE_OPTIONS_TYPE_EX_::securityKey
Definition at line
69
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
sourceNode#
MULTICHAN_SOURCE_NODE_ID _RECEIVE_OPTIONS_TYPE_EX_::sourceNode
Definition at line
70
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
destNode#
MULTICHAN_DEST_NODE_ID _RECEIVE_OPTIONS_TYPE_EX_::destNode
Definition at line
71
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
bSupervisionActive#
uint8_t _RECEIVE_OPTIONS_TYPE_EX_::bSupervisionActive
true if supervision is active
Definition at line
72
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
sessionId#
uint8_t _RECEIVE_OPTIONS_TYPE_EX_::sessionId
Current sessionId.
Definition at line
73
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
statusUpdate#
uint8_t _RECEIVE_OPTIONS_TYPE_EX_::statusUpdate
Is statusUpdate enabled for current session.
Definition at line
74
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h