Receive Status#

Status codes for receiving frames.

Macros#

#define

< A response route is locked by the application

#define

Received at low output power level, this must have the same value as TRANSMIT_OPTION_LOW_POWER.

#define

Mask for masking out the received frametype bits.

#define

Received frame is singlecast frame (rxOptions == xxxx00xx)

#define

Received frame is broadcast frame (rxOptions == xxxx01xx)

#define

Received frame is multicast frame (rxOptions == xxxx10xx)

#define

Received frame is an explore frame (rxOptions == xxx1xxxx) Only TYPE_BROAD can be active at the same time as TYPE_EXPLORE.

#define

Received frame is not send to me (rxOptions == x1xxxxxx)

Macro Definition Documentation#

RECEIVE_STATUS_ROUTED_BUSY#

#define RECEIVE_STATUS_ROUTED_BUSY
Value:
0x01

< A response route is locked by the application


Definition at line 65 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

RECEIVE_STATUS_LOW_POWER#

#define RECEIVE_STATUS_LOW_POWER
Value:
0x02

Received at low output power level, this must have the same value as TRANSMIT_OPTION_LOW_POWER.


Definition at line 70 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

RECEIVE_STATUS_TYPE_MASK#

#define RECEIVE_STATUS_TYPE_MASK
Value:
0x0C

Mask for masking out the received frametype bits.


Definition at line 74 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

RECEIVE_STATUS_TYPE_SINGLE#

#define RECEIVE_STATUS_TYPE_SINGLE
Value:
0x00

Received frame is singlecast frame (rxOptions == xxxx00xx)


Definition at line 78 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

RECEIVE_STATUS_TYPE_BROAD#

#define RECEIVE_STATUS_TYPE_BROAD
Value:
0x04

Received frame is broadcast frame (rxOptions == xxxx01xx)


Definition at line 82 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

RECEIVE_STATUS_TYPE_MULTI#

#define RECEIVE_STATUS_TYPE_MULTI
Value:
0x08

Received frame is multicast frame (rxOptions == xxxx10xx)


Definition at line 86 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

RECEIVE_STATUS_TYPE_EXPLORE#

#define RECEIVE_STATUS_TYPE_EXPLORE
Value:
0x10

Received frame is an explore frame (rxOptions == xxx1xxxx) Only TYPE_BROAD can be active at the same time as TYPE_EXPLORE.


Definition at line 91 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

RECEIVE_STATUS_FOREIGN_FRAME#

#define RECEIVE_STATUS_FOREIGN_FRAME
Value:
0x40

Received frame is not send to me (rxOptions == x1xxxxxx)

  • useful only in promiscuous mode


Definition at line 96 of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h