Supervision#
Description#
CC Supervision is built into the Application Framework and handles Supervision communication on S2 encapsulated frames. Supervision is only supported for Set and Report commands.
Command Class Supervision is default configuration to not support more Supervision reports on a Supervision Get command. In Supervision Get command is 'more status updates' field set to CC_SUPERVISION_STATUS_UPDATES_NOT_SUPPORTED.
Default configuration#
The default setting is that CC Supervision supports only one Supervision Report per Supervision Get command. In Supervision Get command, the 'more status updates' field is set to CC_SUPERVISION_STATUS_UPDATES_NOT_SUPPORTED.
Handle more Supervision Reports#
Device has the possibility to inform destination node that there is an operation in progress. Example is Wall controller with a display showing that a device is working (CC_SUPERVISION_STATUS_WORKING) until target value is reached (CC_SUPERVISION_STATUS_SUCCESS). Please see cc_supervision_report_recived_handler() for more details.
Control Supervision Reports#
Device has the possibility to send more Supervision Reports to report ongoing Request job. Example application Doorlock Keypad reports when Doorlock operation is started and also sends a new report when it's finished. For this purpose, cc_supervision_get_received_handler()
can be used. Please see cc_supervision_get_received_handler() for more details.
Modules#
SUPERVISION_GET_RECEIVED_HANDLER_ARGS
Enumerations#
Enum type is used in CC SUPERVISION_REPORT to allow a receiving node to advertise application status updates in future Supervision Report Commands.
Status of Supervision.
Typedefs#
Status of Supervision.
Structure used by supervision_event_handler() to process upcoming events Registered for CC Supervision.
Functions#
CmdClassSupervisionReportSend.
Creates payload for Supervision Get command by calling CommandClassSupervisionGetWrite and updates supervision session ID.
Generates payload for Supervision Get command.
Sets the payload length in a Supervision Get command.
Gets the length of encapsulated payload from the frame.
Invoked upon reception of a Supervision Get This function is weakly defined in CC_Supervision.c and can be defined in the application if desired.
Invoked upon reception of a Supervision Report This function is weakly defined in CC_Supervision.c and can be defined in the application if desired.
Returns whether transmission of status updates is enabled or disabled by default.
Macros#
extract session id from properties bits [0..5]
add session id from properties bits [0..5]
extract more status update field bit 7, CC SUPERVISION_REPORT
status values: {0,1}.
extract more status update field bit 7, CC SUPERVISION_GET
status values: {0,1}.
Enumeration Documentation#
cc_supervision_more_status_updates_t#
cc_supervision_more_status_updates_t
Enum type is used in CC SUPERVISION_REPORT to allow a receiving node to advertise application status updates in future Supervision Report Commands.
Enumerator | |
---|---|
CC_SUPERVISION_MORE_STATUS_UPDATES_THIS_IS_LAST | CC_SUPERVISION_MORE_STATUS_UPDATES_THIS_IS_LAST. |
CC_SUPERVISION_MORE_STATUS_UPDATES_REPORTS_TO_FOLLOW | CC_SUPERVISION_MORE_STATUS_UPDATES_REPORTS_TO_FOLLOW. |
77
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
_SUPERVISION_STATUS_#
_SUPERVISION_STATUS_
Status of Supervision.
Enumerator | |
---|---|
CC_SUPERVISION_STATUS_NOT_SUPPORTED | SUPERVISION_STATUS_NOT_SUPPORTED. |
CC_SUPERVISION_STATUS_WORKING | SUPERVISION_STATUS_WORKING. |
CC_SUPERVISION_STATUS_FAIL | SUPERVISION_STATUS_FAIL. |
CC_SUPERVISION_STATUS_CANCEL | CC Supervision shouldn't do anything with this frame, report will be sent from somewhere else. |
CC_SUPERVISION_STATUS_NOT_FOUND | CC handler was not found in CC handler map. |
CC_SUPERVISION_STATUS_SUCCESS | SUPERVISION_STATUS_SUCCESS. |
86
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
Typedef Documentation#
cc_supervision_status_t#
typedef enum _SUPERVISION_STATUS_ cc_supervision_status_t
Status of Supervision.
95
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
cc_supervision_report_event#
typedef struct _cc_supervision_report_event cc_supervision_report_event
Structure used by supervision_event_handler() to process upcoming events Registered for CC Supervision.
122
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
Function Documentation#
CmdClassSupervisionReportSend#
bool CmdClassSupervisionReportSend (zaf_tx_options_t * tx_options, uint8_t properties, cc_supervision_status_t status, uint8_t duration)
CmdClassSupervisionReportSend.
[in] | tx_options | Transmit options of type zaf_tx_options_t |
[in] | properties | includes: bit[0..5] Session ID bit[6] unused and bit[7] more status updates. This field is used to advertise if more Supervision Reports follow for the actual Session ID. [0] last report, [1] more report follow. |
[in] | status | Supervision status. |
[in] | duration | The duration must comply with the following: 0x00 0 seconds. (Already at the Target Value.) 0x01-0x7F 1 second (0x01) to 127 seconds (0x7F) in 1 second resolution. 0x80-0xFD 1 minute (0x80) to 126 minutes (0xFD) in 1 minute resolution. 0xFE Unknown duration 0xFF Reserved |
Returns
true if the frame was enqueued else false
142
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
CommandClassSupervisionGetAdd#
void CommandClassSupervisionGetAdd (ZW_SUPERVISION_GET_FRAME * pPayload)
Creates payload for Supervision Get command by calling CommandClassSupervisionGetWrite and updates supervision session ID.
[inout] | pPayload | pointer to supervision get payload |
Used by Framework and should not be used be application.
156
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
CommandClassSupervisionGetWrite#
void CommandClassSupervisionGetWrite (ZW_SUPERVISION_GET_FRAME * pbuf)
Generates payload for Supervision Get command.
[inout] | pbuf | Pointer to supervision get payload |
Used by Framework and should not be used be application.
166
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
CommandClassSupervisionGetSetPayloadLength#
void CommandClassSupervisionGetSetPayloadLength (ZW_SUPERVISION_GET_FRAME * pbuf, uint8_t payLoadlen)
Sets the payload length in a Supervision Get command.
[in] | pbuf | Pointer to supervision get payload |
[in] | payLoadlen | Payload length to be set. |
Used by Framework when sending supervision-encapsulated frames
175
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
CommandClassSupervisionGetGetPayloadLength#
uint8_t CommandClassSupervisionGetGetPayloadLength (ZW_SUPERVISION_GET_FRAME * pbuf)
Gets the length of encapsulated payload from the frame.
N/A | pbuf | Frame that contains the encapsulated command |
Used by framework to calculate the length of the payload in supervision-encapsulated frames.
Returns
length of the payload
185
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
cc_supervision_get_received_handler#
void cc_supervision_get_received_handler (SUPERVISION_GET_RECEIVED_HANDLER_ARGS * pArgs)
Invoked upon reception of a Supervision Get This function is weakly defined in CC_Supervision.c and can be defined in the application if desired.
N/A | pArgs | parameters for the handler |
26
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/cc_supervision_handlers.h
cc_supervision_report_recived_handler#
void cc_supervision_report_recived_handler (cc_supervision_status_t status, uint8_t duration)
Invoked upon reception of a Supervision Report This function is weakly defined in CC_Supervision.c and can be defined in the application if desired.
N/A | status | the required status |
N/A | duration | the required duration |
35
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/cc_supervision_handlers.h
cc_supervision_get_default_status_updates_enabled#
bool cc_supervision_get_default_status_updates_enabled ()
Returns whether transmission of status updates is enabled or disabled by default.
Used by the Supervion Command Class initialization
Returns
true if enabled, false if disabled
26
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/src/cc_supervision_config_api.h
Macro Definition Documentation#
CC_SUPERVISION_EXTRACT_SESSION_ID#
#define CC_SUPERVISION_EXTRACT_SESSION_IDValue:
(properties)
extract session id from properties bits [0..5]
54
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
CC_SUPERVISION_ADD_SESSION_ID#
#define CC_SUPERVISION_ADD_SESSION_IDValue:
(properties)
add session id from properties bits [0..5]
55
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
CC_SUPERVISION_EXTRACT_MORE_STATUS_UPDATE#
#define CC_SUPERVISION_EXTRACT_MORE_STATUS_UPDATEValue:
(status)
extract more status update field bit 7, CC SUPERVISION_REPORT
56
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
CC_SUPERVISION_ADD_MORE_STATUS_UPDATE#
#define CC_SUPERVISION_ADD_MORE_STATUS_UPDATEValue:
(status)
status values: {0,1}.
Set bit 7, CC SUPERVISION_REPORT
57
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
CC_SUPERVISION_EXTRACT_STATUS_UPDATE#
#define CC_SUPERVISION_EXTRACT_STATUS_UPDATEValue:
(status)
extract more status update field bit 7, CC SUPERVISION_GET
58
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
CC_SUPERVISION_ADD_STATUS_UPDATE#
#define CC_SUPERVISION_ADD_STATUS_UPDATEValue:
(status)
status values: {0,1}.
Set bit 7, CC SUPERVISION_GET
59
of file /mnt/raid/workspaces/ws.OEhokVcbw/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h