Zpal-status#
Defines status codes returned by zpal functions.
Typedefs#
typedef uint32_t
Macros#
#define
ZPAL_STATUS_OK ((zpal_status_t)0x0000)
No error.
#define
ZPAL_STATUS_FAIL ((zpal_status_t)0x0001)
Generic error.
#define
ZPAL_STATUS_BUFFER_FULL ((zpal_status_t)0x0002)
There is no more room in the buffer.
#define
ZPAL_STATUS_BUSY ((zpal_status_t)0x0003)
Process is busy.
#define
ZPAL_STATUS_INVALID_ARGUMENT ((zpal_status_t)0x0004)
At least one argument is invalid.
Typedef Documentation#
zpal_status_t#
typedef uint32_t zpal_status_t
Definition at line
29
of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_status.h
Macro Definition Documentation#
ZPAL_STATUS_OK#
#define ZPAL_STATUS_OKValue:
((zpal_status_t)0x0000)
No error.
Definition at line
31
of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_status.h
ZPAL_STATUS_FAIL#
#define ZPAL_STATUS_FAILValue:
((zpal_status_t)0x0001)
Generic error.
Definition at line
32
of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_status.h
ZPAL_STATUS_BUFFER_FULL#
#define ZPAL_STATUS_BUFFER_FULLValue:
((zpal_status_t)0x0002)
There is no more room in the buffer.
Definition at line
33
of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_status.h
ZPAL_STATUS_BUSY#
#define ZPAL_STATUS_BUSYValue:
((zpal_status_t)0x0003)
Process is busy.
Definition at line
34
of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_status.h
ZPAL_STATUS_INVALID_ARGUMENT#
#define ZPAL_STATUS_INVALID_ARGUMENTValue:
((zpal_status_t)0x0004)
At least one argument is invalid.
Definition at line
35
of file /mnt/raid/workspaces/ws.ptOyROOkM/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_status.h