Z-Wave Serial API#
Modules#
Enumerations#
enum
NVM_BACKUP_RESTORE_ADDR_SIZE = 2
NVM_EXT_BACKUP_RESTORE_ADDR_SIZE = 4
}
size of the address field of NVM_BACKUP_RESTORE or NVM_EXT_BACKUP_RESTORE frames.
Macros#
#define
SOF 0x01
Start Of Frame.
#define
ACK 0x06
Acknowledge successful frame reception.
#define
NAK 0x15
Not Acknowledge successful frame reception - please retransmit...
#define
CAN 0x18
Frame received (from host) was dropped - waiting for ACK.
Enumeration Documentation#
nvm_backup_restore_addr_size_t#
nvm_backup_restore_addr_size_t
size of the address field of NVM_BACKUP_RESTORE or NVM_EXT_BACKUP_RESTORE frames.
Item value is the size in byte of the address field.
Enumerator | |
---|---|
NVM_BACKUP_RESTORE_ADDR_SIZE | 2 bytes for the legacy NVM backup & restore command |
NVM_EXT_BACKUP_RESTORE_ADDR_SIZE | 4 bytes for the extended NVM backup & restore command |
Definition at line
374
of file /mnt/raid/workspaces/ws.aaL8QAxSV/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/SerialAPI.h
Macro Definition Documentation#
SOF#
#define SOFValue:
0x01
Start Of Frame.
Definition at line
16
of file /mnt/raid/workspaces/ws.aaL8QAxSV/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/SerialAPI.h
ACK#
#define ACKValue:
0x06
Acknowledge successful frame reception.
Definition at line
17
of file /mnt/raid/workspaces/ws.aaL8QAxSV/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/SerialAPI.h
NAK#
#define NAKValue:
0x15
Not Acknowledge successful frame reception - please retransmit...
Definition at line
18
of file /mnt/raid/workspaces/ws.aaL8QAxSV/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/SerialAPI.h
CAN#
#define CANValue:
0x18
Frame received (from host) was dropped - waiting for ACK.
Definition at line
19
of file /mnt/raid/workspaces/ws.aaL8QAxSV/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/SerialAPI.h