CentralScene#
Modules#
Typedefs#
Structure that describes a single scene.
Functions#
Initiates the transmission of a "Central Scene Notification" command.
Start or stop Central Scene Notification timer Used when event CENTRAL_SCENE_NOTIFICATION_KEY_ATTRIBUTES_KEY_HELD_DOWN happens.
Returns the array of central scenes.
Returns number of supported scenes.
Returns supported attributes for a given scene.
Gets 'identical' attribute that describes supported key attributes.
Macros#
Size of supported scenes.
Typedef Documentation#
cc_central_scene_t#
typedef struct _cc_central_scene_t cc_central_scene_t
Structure that describes a single scene.
Function Documentation#
cc_central_scene_notification_tx#
JOB_STATUS cc_central_scene_notification_tx (AGI_PROFILE * pProfile, uint8_t keyAttribute, uint8_t sceneNumber, ZAF_TX_Callback_t pCbFunc)
Initiates the transmission of a "Central Scene Notification" command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| AGI_PROFILE * | [in] | pProfile | pointer to AGI profile or NULL for lifeline |
| uint8_t | [in] | keyAttribute | The key event. |
| uint8_t | [in] | sceneNumber | The scene number. |
| ZAF_TX_Callback_t | [in] | pCbFunc | Callback function to be called when transmission is done/failed. |
Note
Source Endpoint is always set to Root in this function
Returns
Status of the job.
cc_central_scene_handle_notification_timer#
void cc_central_scene_handle_notification_timer (bool start_timer, uint8_t scene_number)
Start or stop Central Scene Notification timer Used when event CENTRAL_SCENE_NOTIFICATION_KEY_ATTRIBUTES_KEY_HELD_DOWN happens.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | start_timer | True if timer should be started, false will stop active timer. |
| uint8_t | N/A | scene_number | Number of active scene. |
App will send notifications periodically as long as the event is active. Frequency depends on whether slow refresh is enabled or not.
cc_central_scene_config_get_scenes_attributes#
cc_central_scene_t * cc_central_scene_config_get_scenes_attributes (void )
Returns the array of central scenes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
If scenes are identical, the array will contain only one element
Returns
Address of the first element in the central scene array.
cc_central_scene_config_get_number_of_scenes#
uint8_t cc_central_scene_config_get_number_of_scenes (void )
Returns number of supported scenes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Total amount of scenes supported by the app.
cc_central_scene_config_get_attribute_bitmask#
uint8_t cc_central_scene_config_get_attribute_bitmask (uint8_t scene_number)
Returns supported attributes for a given scene.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | scene_number | Number of scene to get supported attributes for |
Note
This function is used to prepare CENTRAL_SCENE_SUPPORTED_REPORT It is assumption that argument scene_number is higher than 1 only in case when scenes are not identical.
Returns
Supported attributes as bitmask
cc_central_scene_config_get_identical#
uint8_t cc_central_scene_config_get_identical (void )
Gets 'identical' attribute that describes supported key attributes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
True if all keys are identical, False if different key attributes supported
cc_central_scene_read#
bool cc_central_scene_read (central_scene_configuration_t * pConfig)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| central_scene_configuration_t * | N/A | pConfig |
cc_central_scene_write#
bool cc_central_scene_write (const central_scene_configuration_t * pConfig)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const central_scene_configuration_t * | N/A | pConfig |
cc_central_scene_migrate#
void cc_central_scene_migrate (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Macro Definition Documentation#
CC_CENTRAL_SCENE_SIZE_OF_SUPPORTED_SCENES_ATTRIBUTES#
#define CC_CENTRAL_SCENE_SIZE_OF_SUPPORTED_SCENES_ATTRIBUTESValue:
sizeof(((cc_central_scene_t *)0)->scene_attributes)
Size of supported scenes.
This field advertises the size of each "Supported Key Attributes" field measured in bytes. Note
: This value can have values 1-3, but all attributes available in current version of Central Scene (V3) can fit into a single byte.