MultilevelSensor#
Modules#
Enumerations#
Defined possible sensor types.
Defined possible sensor read size.
Defined possible sensor read precision.
Defined sensor interface return values.
Defined Multilevel Sensor return values.
Typedefs#
Defined possible sensor types.
Structure that holds the attributes of a sensor type.
Structure that holds a read result from the read interface.
Structure that administrate all of the registered sensors.
Functions#
This function will report the registered sensor's measured datas to the Lifeline group.
Calls the init function for all of the registered sensor interfaces.
Checks if the wanted scale is a legal one for an interface.
Checks if the wanted sensor type has a registered interface or not.
Registers an interface to a specific sensor type.
Fills an input buffer with flags where each flag represents a supported sensor.
Fills an input buffer with flags where each flag represents a supported scale.
Getter function for a sensor type's interface.
Gets the default sensor type value.
Initialize an iterator struct for the registered sensor interfaces.
Moves the iterator reference forward to the next registered interface, if the current is the last one then NULL If there is any registered interface the iterator will be NULL.
Returns the number of registered sensor interfaces.
Removes all of the registered sensor interfaces from the administration.
Returns a sensor_type_t struct from the sensor_types config table.
Initialize a sensor interface instance.
Adds a new scale to an existing interface.
Macros#
Defined possible sensor scales.
Absolute humidity.
Acidity.
Ampere.
A-weighted decibels.
Beats per minute.
Becquerel per cubic meter.
BMI Index.
Body wave.
Breaths per minute.
Btu/h.
Celsius.
Centimeter.
Cubic feet per minute.
Cubic meter.
Cubic meter per hour.
dBm
Decibel.
Degrees.
Degrees relative to north pole.
Diastolic.
Dimensionless value.
European Macroseismic.
Fahrenheit.
Feet.
Gallons.
Hertz.
Impedance.
Inches of Mercury.
Inches per hour.
Joule.
Kilogram.
Kilohertz.
Kilopascal.
Liedu.
Liter.
Liter per hour.
Local.
Lux.
Mercalli.
Meter.
Meter per second.
Meter per square second.
Microgram per cubic meter.
Micro gram per cubic meter.
Miles per hour.
Milliampere.
Milligram per liter.
Millimeter per hour.
Millivolt.
Mole per cubic meter.
Moment.
Newton.
Ohm meter.
Parts per million.
Percentage value.
Picocuries per liter.
Pounds.
Pound per square inch.
Revolutions per minute.
RSSI.
Second.
Shindo.
Siemens per meter.
Surface wave.
Systolic.
Unitless.
UV index.
Volt.
Volume water content.
Water activity.
Watt.
Watt per square meter.
Sensor scale aliases for backward compatibility.
Macros for sensor type definitions - allows inlining at call sites for better optimization These expand to compound literals that can be used directly in assignments.
Helper macro to generate a single case in the sensor type lookup Sensor types that are accessed by the application code are allocated statically.
Macro to map sensor_name_t enum to corresponding sensor type.
Structure that holds a read result from the read interface.
Enumeration Documentation#
sensor_name#
sensor_name
Defined possible sensor types.
| Enumerator | |
|---|---|
| SENSOR_NAME_AIR_TEMPERATURE | 0x01 - Air temperature |
| SENSOR_NAME_GENERAL_PURPOSE | 0x02 - General purpose |
| SENSOR_NAME_ILLUMINANCE | 0x03 - Illuminance |
| SENSOR_NAME_POWER | 0x04 - Power |
| SENSOR_NAME_HUMIDITY | 0x05 - Humidity |
| SENSOR_NAME_VELOCITY | 0x06 - Velocity |
| SENSOR_NAME_DIRECTION | 0x07 - Direction |
| SENSOR_NAME_ATMOSPHERIC_PRESSURE | 0x08 - Atmospheric pressure |
| SENSOR_NAME_BAROMETRIC_PRESSURE | 0x09 - Barometric pressure |
| SENSOR_NAME_SOLAR_RADIATION | 0x0A - Solar radiation |
| SENSOR_NAME_DEW_POINT | 0x0B - Dew point |
| SENSOR_NAME_RAIN_RATE | 0x0C - Rain rate |
| SENSOR_NAME_TIDE_LEVEL | 0x0D - Tide level |
| SENSOR_NAME_WEIGHT | 0x0E - Weight |
| SENSOR_NAME_VOLTAGE | 0x0F - Voltage |
| SENSOR_NAME_CURRENT | 0x10 - Current |
| SENSOR_NAME_CARBON_DIOXIDE_CO2_LEVEL | 0x11 - Carbon dioxide (CO2-level) |
| SENSOR_NAME_AIR_FLOW | 0x12 - Air flow |
| SENSOR_NAME_TANK_CAPACITY | 0x13 - Tank capacity |
| SENSOR_NAME_DISTANCE | 0x14 - Distance |
| SENSOR_NAME_ANGLE_POSITION | 0x15 - Angle position |
| SENSOR_NAME_ROTATION | 0x16 - Rotation |
| SENSOR_NAME_WATER_TEMPERATURE | 0x17 - Water temperature |
| SENSOR_NAME_SOIL_TEMPERATURE | 0x18 - Soil temperature |
| SENSOR_NAME_SEISMIC_INTENSITY | 0x19 - Seismic Intensity |
| SENSOR_NAME_SEISMIC_MAGNITUDE | 0x1A - Seismic magnitude |
| SENSOR_NAME_ULTRAVIOLET | 0x1B - Ultraviolet |
| SENSOR_NAME_ELECTRICAL_RESISTIVITY | 0x1C - Electrical resistivity |
| SENSOR_NAME_ELECTRICAL_CONDUCTIVITY | 0x1D - Electrical conductivity |
| SENSOR_NAME_LOUDNESS | 0x1E - Loudness |
| SENSOR_NAME_MOISTURE | 0x1F - Moisture |
| SENSOR_NAME_FREQUENCY | 0x20 - Frequency |
| SENSOR_NAME_TIME | 0x21 - Time |
| SENSOR_NAME_TARGET_TEMPERATURE | 0x22 - Target temperature |
| SENSOR_NAME_PARTICULATE_MATTER_2_5 | 0x23 - Particulate Matter 2.5 |
| SENSOR_NAME_FORMALDEHYDE_CH2O_LEVEL | 0x24 - Formaldehyde (CH2O-level) |
| SENSOR_NAME_RADON_CONCENTRATION | 0x25 - Radon concentration |
| SENSOR_NAME_METHANE_CH4_DENSITY | 0x26 - Methane (CH4) density |
| SENSOR_NAME_VOLATILE_ORGANIC_COMPOUND_LEVEL | 0x27 - Volatile Organic Compound level |
| SENSOR_NAME_CARBON_MONOXIDE_CO_LEVEL | 0x28 - Carbon monoxide (CO) level |
| SENSOR_NAME_SOIL_HUMIDITY | 0x29 - Soil humidity |
| SENSOR_NAME_SOIL_REACTIVITY | 0x2A - Soil reactivity |
| SENSOR_NAME_SOIL_SALINITY | 0x2B - Soil salinity |
| SENSOR_NAME_HEART_RATE | 0x2C - Heart rate |
| SENSOR_NAME_BLOOD_PRESSURE | 0x2D - Blood pressure |
| SENSOR_NAME_MUSCLE_MASS | 0x2E - Muscle mass |
| SENSOR_NAME_FAT_MASS | 0x2F - Fat mass |
| SENSOR_NAME_BONE_MASS | 0x30 - Bone mass |
| SENSOR_NAME_TOTAL_BODY_WATER_TBW | 0x31 - Total body water (TBW) |
| SENSOR_NAME_BASIS_METABOLIC_RATE_BMR | 0x32 - Basis metabolic rate (BMR) |
| SENSOR_NAME_BODY_MASS_INDEX_BMI | 0x33 - Body Mass Index (BMI) |
| SENSOR_NAME_ACCELERATION_X | 0x34 - Acceleration X-axis |
| SENSOR_NAME_ACCELERATION_Y | 0x35 - Acceleration Y-axis |
| SENSOR_NAME_ACCELERATION_Z | 0x36 - Acceleration Z-axis |
| SENSOR_NAME_SMOKE_DENSITY | 0x37 - Smoke density |
| SENSOR_NAME_WATER_FLOW | 0x38 - Water flow |
| SENSOR_NAME_WATER_PRESSURE | 0x39 - Water pressure |
| SENSOR_NAME_RF_SIGNAL_STRENGTH | 0x3A - RF signal strength |
| SENSOR_NAME_PARTICULATE_MATTER_10 | 0x3B - Particulate Matter 10 |
| SENSOR_NAME_RESPIRATORY_RATE | 0x3C - Respiratory rate |
| SENSOR_NAME_RELATIVE_MODULATION_LEVEL | 0x3D - Relative Modulation level |
| SENSOR_NAME_BOILER_WATER_TEMPERATURE | 0x3E - Boiler water temperature |
| SENSOR_NAME_DOMESTIC_HOT_WATER_DHW_TEMPERATURE | 0x3F - Domestic Hot Water (DHW) temperature |
| SENSOR_NAME_OUTSIDE_TEMPERATURE | 0x40 - Outside temperature |
| SENSOR_NAME_EXHAUST_TEMPERATURE | 0x41 - Exhaust temperature |
| SENSOR_NAME_WATER_CHLORINE_LEVEL | 0x42 - Water Chlorine level |
| SENSOR_NAME_WATER_ACIDITY | 0x43 - Water acidity |
| SENSOR_NAME_WATER_OXIDATION_REDUCTION_POTENTIAL | 0x44 - Water Oxidation reduction potential |
| SENSOR_NAME_HEART_RATE_LF_HF_RATIO | 0x45 - Heart Rate LF/HF ratio |
| SENSOR_NAME_MOTION_DIRECTION | 0x46 - Motion Direction |
| SENSOR_NAME_APPLIED_FORCE_ON_THE_SENSOR | 0x47 - Applied force on the sensor |
| SENSOR_NAME_RETURN_AIR_TEMPERATURE | 0x48 - Return Air temperature |
| SENSOR_NAME_SUPPLY_AIR_TEMPERATURE | 0x49 - Supply Air temperature |
| SENSOR_NAME_CONDENSER_COIL_TEMPERATURE | 0x4A - Condenser Coil temperature |
| SENSOR_NAME_EVAPORATOR_COIL_TEMPERATURE | 0x4B - Evaporator Coil temperature |
| SENSOR_NAME_LIQUID_LINE_TEMPERATURE | 0x4C - Liquid Line temperature |
| SENSOR_NAME_DISCHARGE_LINE_TEMPERATURE | 0x4D - Discharge Line temperature |
| SENSOR_NAME_SUCTION_INPUT_PUMP_COMPRESSOR_PRESSURE | 0x4E - Suction (input pump/compressor) Pressure |
| SENSOR_NAME_DISCHARGE_OUTPUT_PUMP_COMPRESSOR_PRESSURE | 0x4F - Discharge (output pump/compressor) Pressure |
| SENSOR_NAME_DEFROST_TEMPERATURE_DEFROST | 0x50 - Defrost temperature (sensor used to decide when to defrost) |
| SENSOR_NAME_OZONE_O3 | 0x51 - Ozone (O3) |
| SENSOR_NAME_SULFUR_DIOXIDE_SO2 | 0x52 - Sulfur dioxide (SO2) |
| SENSOR_NAME_NITROGEN_DIOXIDE_NO2 | 0x53 - Nitrogen dioxide (NO2) |
| SENSOR_NAME_AMMONIA_NH3 | 0x54 - Ammonia (NH3) |
| SENSOR_NAME_LEAD_PB | 0x55 - Lead (Pb) |
| SENSOR_NAME_PARTICULATE_MATTER_1 | 0x56 - Particulate Matter 1 |
| SENSOR_NAME_PERSON_COUNTER_ENTERING | 0x57 - Person counter (entering) |
| SENSOR_NAME_PERSON_COUNTER_EXITING | 0x58 - Person counter (exiting) |
| SENSOR_NAME_MAX_COUNT | |
sensor_read_result_size_t#
sensor_read_result_size_t
Defined possible sensor read size.
| Enumerator | |
|---|---|
| SENSOR_READ_RESULT_SIZE_1 | |
| SENSOR_READ_RESULT_SIZE_2 | |
| SENSOR_READ_RESULT_SIZE_4 | |
| SENSOR_READ_RESULT_SIZE_END | |
sensor_read_result_precision#
sensor_read_result_precision
Defined possible sensor read precision.
| Enumerator | |
|---|---|
| SENSOR_READ_RESULT_PRECISION_1 | |
| SENSOR_READ_RESULT_PRECISION_2 | |
| SENSOR_READ_RESULT_PRECISION_3 | |
| SENSOR_READ_RESULT_PRECISION_END | |
sensor_interface_return_value_t#
sensor_interface_return_value_t
Defined sensor interface return values.
| Enumerator | |
|---|---|
| SENSOR_INTERFACE_RETURN_VALUE_OK | |
| SENSOR_INTERFACE_RETURN_VALUE_ALREADY_SET | |
| SENSOR_INTERFACE_RETURN_VALUE_INVALID_SCALE_VALUE | |
| SENSOR_INTERFACE_RETURN_VALUE_ERROR | |
| SENSOR_INTERFACE_RETURN_VALUE_END | |
cc_multilevel_sensor_return_value#
cc_multilevel_sensor_return_value
Defined Multilevel Sensor return values.
| Enumerator | |
|---|---|
| CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK | |
| CC_MULTILEVEL_SENSOR_RETURN_VALUE_ERROR | |
| CC_MULTILEVEL_SENSOR_RETURN_VALUE_NOT_FOUND | |
| CC_MULTILEVEL_SENSOR_RETURN_VALUE_ALREADY_REGISTRATED | |
| CC_MULTILEVEL_SENSOR_RETURN_VALUE_REGISTRATION_LIMIT_REACHED | |
| CC_MULTILEVEL_SENSOR_RETURN_VALUE_END | |
Typedef Documentation#
sensor_type_t#
typedef struct _sensor_type sensor_type_t
Structure that holds the attributes of a sensor type.
sensor_interface_t#
typedef struct _sensor_interface sensor_interface_t
Structure that holds a read result from the read interface.
sensor_administration_t#
typedef struct _sensor_administration sensor_administration_t
Structure that administrate all of the registered sensors.
Function Documentation#
cc_multilevel_sensor_send_sensor_data#
void cc_multilevel_sensor_send_sensor_data (void )
This function will report the registered sensor's measured datas to the Lifeline group.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
cc_multilevel_sensor_config_register_instances#
void cc_multilevel_sensor_config_register_instances (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
cc_multilevel_sensor_init_all_sensor#
void cc_multilevel_sensor_init_all_sensor (void )
Calls the init function for all of the registered sensor interfaces.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
cc_multilevel_sensor_check_scale#
uint8_t cc_multilevel_sensor_check_scale (const sensor_interface_t * i_interface, uint8_t i_scale)
Checks if the wanted scale is a legal one for an interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sensor_interface_t * | [in] | i_interface | Pointer to an existing sensor interface |
| uint8_t | [in] | i_scale | Scale value to check |
If the scale is not set the function will return with the first available scale. The function will iterate from bit 0 to 7 to look for the first scale which is supported. That will be the default scale. Returns
a usable scale value, if the input i_scale is valid that will be return, else the default one.
cc_multilevel_sensor_check_sensor_type_registered#
cc_multilevel_sensor_return_value cc_multilevel_sensor_check_sensor_type_registered (uint8_t endpoint, uint8_t sensor_type_value)
Checks if the wanted sensor type has a registered interface or not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | endpoint | Sensor type value to check, this is the value in sensor_type_t struct's value |
| uint8_t | N/A | sensor_type_value |
Returns
CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if interface is registered for a sensor, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_NOT_FOUND.
cc_multilevel_sensor_registration#
cc_multilevel_sensor_return_value cc_multilevel_sensor_registration (sensor_interface_t * i_new_sensor)
Registers an interface to a specific sensor type.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sensor_interface_t * | [in] | i_new_sensor | Pointer to a filled sensor interface struct |
The number of registered sensor types is maximized with REGISTERED_SENSOR_NUMBER_LIMIT Returns
CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if interface is registered for a sensor.
cc_multilevel_sensor_get_supported_sensors#
cc_multilevel_sensor_return_value cc_multilevel_sensor_get_supported_sensors (uint8_t * o_supported_sensor_buffer)
Fills an input buffer with flags where each flag represents a supported sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | o_supported_sensor_buffer | Pointer to a buffer where the supported sensors' are represented as flags in a byte array. The position of each flag is calculated based on SDS13812. The buffer must be 11 byte long at least. |
Returns
CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if success, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_ERROR.
cc_multilevel_sensor_get_supported_scale#
cc_multilevel_sensor_return_value cc_multilevel_sensor_get_supported_scale (uint8_t sensor_type_value, uint8_t * o_supported_scale)
Fills an input buffer with flags where each flag represents a supported scale.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | sensor_type_value | Sensor type value to check, this is the value in sensor_type_t struct's value |
| uint8_t * | [out] | o_supported_scale | Pointer to a buffer where the supported scales will be represented for a sensor type |
Returns
CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if interface is registered for a sensor.
cc_multilevel_sensor_get_interface#
cc_multilevel_sensor_return_value cc_multilevel_sensor_get_interface (uint8_t endpoint, uint8_t sensor_type_value, sensor_interface_t ** o_interface)
Getter function for a sensor type's interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | endpoint | Sensor type value to check, this is the value in sensor_type_t struct's value |
| uint8_t | [out] | sensor_type_value | This is a double pointer which will hold an interface reference |
| sensor_interface_t ** | N/A | o_interface |
Returns
CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if interface is registered for a sensor, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_NOT_FOUND.
cc_multilevel_sensor_get_default_sensor_type#
cc_multilevel_sensor_return_value cc_multilevel_sensor_get_default_sensor_type (uint8_t * o_default_sensor_type)
Gets the default sensor type value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | o_default_sensor_type | Pointer to a byte buffer which will hold the default sensor type value |
Basically the first registered sensor interface' type is the default one. Returns
CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if there is any registered interface, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_ERROR.
cc_multilevel_sensor_init_iterator#
cc_multilevel_sensor_return_value cc_multilevel_sensor_init_iterator (sensor_interface_iterator_t ** i_iterator)
Initialize an iterator struct for the registered sensor interfaces.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sensor_interface_iterator_t ** | [out] | i_iterator | This is a double pointer which will hold an interface reference to the first registered interface |
If there is any registered interface the iterator will be NULL. Returns
CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if success, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_ERROR..
cc_multilevel_sensor_next_iterator#
void cc_multilevel_sensor_next_iterator (sensor_interface_iterator_t ** i_iterator)
Moves the iterator reference forward to the next registered interface, if the current is the last one then NULL If there is any registered interface the iterator will be NULL.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sensor_interface_iterator_t ** | [out] | i_iterator | This is a double pointer which will hold an interface reference |
cc_multilevel_sensor_get_number_of_registered_sensors#
uint8_t cc_multilevel_sensor_get_number_of_registered_sensors (void )
Returns the number of registered sensor interfaces.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Number of registered sensor interfaces.
cc_multilevel_sensor_reset_administration#
void cc_multilevel_sensor_reset_administration (void )
Removes all of the registered sensor interfaces from the administration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
cc_multilevel_sensor_get_sensor_type#
const sensor_type_t * cc_multilevel_sensor_get_sensor_type (sensor_name_t i_sensor_name)
Returns a sensor_type_t struct from the sensor_types config table.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sensor_name_t | [in] | i_sensor_name | The name of the sensor type, the sensor type attributes' reference will be look for based on this value |
Returns
sensor_type_t struct which includes the type attributes.
cc_multilevel_sensor_init_interface#
sensor_interface_return_value_t cc_multilevel_sensor_init_interface (sensor_interface_t * i_instance, sensor_name_t i_name)
Initialize a sensor interface instance.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sensor_interface_t * | [in] | i_instance | Pointer to an existing sensor interface to init |
| sensor_name_t | [in] | i_name | The name of the sensor type, the sensor type attributes' reference will be look for based on this value |
Sets the whole struct to zero and sets the reference to the appropiate sensor_type_t struct. Returns
Status of the initialization.
cc_multilevel_sensor_add_supported_scale_interface#
sensor_interface_return_value_t cc_multilevel_sensor_add_supported_scale_interface (sensor_interface_t * i_instance, uint8_t i_scale)
Adds a new scale to an existing interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sensor_interface_t * | [in] | i_instance | Pointer to an existing sensor interface which the new scale will be registered to |
| uint8_t | [in] | i_scale | The new scale which will be registered |
Supported scales must be set by this function during initialization. Returns
Status of the new scale value registration.
Macro Definition Documentation#
MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_SEC#
#define MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_SECValue:
(MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_MIN * 60)
MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_MS#
#define MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_MSValue:
(MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_SEC * 1000)
SENSOR_SCALE_AWEIGHTED_DECIBELS#
#define SENSOR_SCALE_AWEIGHTED_DECIBELSValue:
0x01
A-weighted decibels.
SENSOR_SCALE_BECQUEREL_PER_CUBIC_METER#
#define SENSOR_SCALE_BECQUEREL_PER_CUBIC_METERValue:
0x00
Becquerel per cubic meter.
SENSOR_SCALE_BREATHS_PER_MINUTE#
#define SENSOR_SCALE_BREATHS_PER_MINUTEValue:
0x00
Breaths per minute.
SENSOR_SCALE_CUBIC_FEET_PER_MINUTE#
#define SENSOR_SCALE_CUBIC_FEET_PER_MINUTEValue:
0x01
Cubic feet per minute.
SENSOR_SCALE_CUBIC_METER_PER_HOUR#
#define SENSOR_SCALE_CUBIC_METER_PER_HOURValue:
0x00
Cubic meter per hour.
SENSOR_SCALE_DEGREES_RELATIVE_TO_NORTH_POLE#
#define SENSOR_SCALE_DEGREES_RELATIVE_TO_NORTH_POLEValue:
0x01
Degrees relative to north pole.
SENSOR_SCALE_DIMENSIONLESS_VALUE#
#define SENSOR_SCALE_DIMENSIONLESS_VALUEValue:
0x01
Dimensionless value.
SENSOR_SCALE_EUROPEAN_MACROSEISMIC#
#define SENSOR_SCALE_EUROPEAN_MACROSEISMICValue:
0x01
European Macroseismic.
SENSOR_SCALE_METER_PER_SQUARE_SECOND#
#define SENSOR_SCALE_METER_PER_SQUARE_SECONDValue:
0x00
Meter per square second.
SENSOR_SCALE_MICROGRAM_PER_CUBIC_METER#
#define SENSOR_SCALE_MICROGRAM_PER_CUBIC_METERValue:
0x01
Microgram per cubic meter.
SENSOR_SCALE_MICRO_GRAM_PER_CUBIC_METER#
#define SENSOR_SCALE_MICRO_GRAM_PER_CUBIC_METERValue:
0x00
Micro gram per cubic meter.
SENSOR_SCALE_MILLIGRAM_PER_LITER#
#define SENSOR_SCALE_MILLIGRAM_PER_LITERValue:
0x00
Milligram per liter.
SENSOR_SCALE_MILLIMETER_PER_HOUR#
#define SENSOR_SCALE_MILLIMETER_PER_HOURValue:
0x00
Millimeter per hour.
SENSOR_SCALE_MOLE_PER_CUBIC_METER#
#define SENSOR_SCALE_MOLE_PER_CUBIC_METERValue:
0x00
Mole per cubic meter.
SENSOR_SCALE_PICOCURIES_PER_LITER#
#define SENSOR_SCALE_PICOCURIES_PER_LITERValue:
0x01
Picocuries per liter.
SENSOR_SCALE_POUND_PER_SQUARE_INCH#
#define SENSOR_SCALE_POUND_PER_SQUARE_INCHValue:
0x01
Pound per square inch.
SENSOR_SCALE_REVOLUTIONS_PER_MINUTE#
#define SENSOR_SCALE_REVOLUTIONS_PER_MINUTEValue:
0x00
Revolutions per minute.
SENSOR_SCALE_VOLUME_WATER_CONTENT#
#define SENSOR_SCALE_VOLUME_WATER_CONTENTValue:
0x01
Volume water content.
SENSOR_SCALE_WATT_PER_SQUARE_METER#
#define SENSOR_SCALE_WATT_PER_SQUARE_METERValue:
0x00
Watt per square meter.
SENSOR_SCALE_DIMENSIONLESS#
#define SENSOR_SCALE_DIMENSIONLESSValue:
SENSOR_SCALE_DIMENSIONLESS_VALUE
Sensor scale aliases for backward compatibility.
SENSOR_SCALE_METER_SQUARE_SECOND#
#define SENSOR_SCALE_METER_SQUARE_SECONDValue:
SENSOR_SCALE_METER_PER_SQUARE_SECOND
SENSOR_TYPE_AIR_TEMPERATURE#
#define SENSOR_TYPE_AIR_TEMPERATUREValue:
.value = 0x01, .byte_offset = 1, .bit_mask = 0, .max_scale_value = 0x01
Macros for sensor type definitions - allows inlining at call sites for better optimization These expand to compound literals that can be used directly in assignments.
SENSOR_TYPE_GENERAL_PURPOSE#
#define SENSOR_TYPE_GENERAL_PURPOSEValue:
.value = 0x02, .byte_offset = 1, .bit_mask = 1, .max_scale_value = 0x01
SENSOR_TYPE_ILLUMINANCE#
#define SENSOR_TYPE_ILLUMINANCEValue:
.value = 0x03, .byte_offset = 1, .bit_mask = 2, .max_scale_value = 0x01
SENSOR_TYPE_POWER#
#define SENSOR_TYPE_POWERValue:
.value = 0x04, .byte_offset = 1, .bit_mask = 3, .max_scale_value = 0x01
SENSOR_TYPE_HUMIDITY#
#define SENSOR_TYPE_HUMIDITYValue:
.value = 0x05, .byte_offset = 1, .bit_mask = 4, .max_scale_value = 0x01
SENSOR_TYPE_VELOCITY#
#define SENSOR_TYPE_VELOCITYValue:
.value = 0x06, .byte_offset = 1, .bit_mask = 5, .max_scale_value = 0x01
SENSOR_TYPE_DIRECTION#
#define SENSOR_TYPE_DIRECTIONValue:
.value = 0x07, .byte_offset = 1, .bit_mask = 6, .max_scale_value = 0x00
SENSOR_TYPE_ATMOSPHERIC_PRESSURE#
#define SENSOR_TYPE_ATMOSPHERIC_PRESSUREValue:
.value = 0x08, .byte_offset = 1, .bit_mask = 7, .max_scale_value = 0x01
SENSOR_TYPE_BAROMETRIC_PRESSURE#
#define SENSOR_TYPE_BAROMETRIC_PRESSUREValue:
.value = 0x09, .byte_offset = 2, .bit_mask = 0, .max_scale_value = 0x01
SENSOR_TYPE_SOLAR_RADIATION#
#define SENSOR_TYPE_SOLAR_RADIATIONValue:
.value = 0x0A, .byte_offset = 2, .bit_mask = 1, .max_scale_value = 0x00
SENSOR_TYPE_DEW_POINT#
#define SENSOR_TYPE_DEW_POINTValue:
.value = 0x0B, .byte_offset = 2, .bit_mask = 2, .max_scale_value = 0x01
SENSOR_TYPE_RAIN_RATE#
#define SENSOR_TYPE_RAIN_RATEValue:
.value = 0x0C, .byte_offset = 2, .bit_mask = 3, .max_scale_value = 0x01
SENSOR_TYPE_TIDE_LEVEL#
#define SENSOR_TYPE_TIDE_LEVELValue:
.value = 0x0D, .byte_offset = 2, .bit_mask = 4, .max_scale_value = 0x01
SENSOR_TYPE_WEIGHT#
#define SENSOR_TYPE_WEIGHTValue:
.value = 0x0E, .byte_offset = 2, .bit_mask = 5, .max_scale_value = 0x01
SENSOR_TYPE_VOLTAGE#
#define SENSOR_TYPE_VOLTAGEValue:
.value = 0x0F, .byte_offset = 2, .bit_mask = 6, .max_scale_value = 0x01
SENSOR_TYPE_CURRENT#
#define SENSOR_TYPE_CURRENTValue:
.value = 0x10, .byte_offset = 2, .bit_mask = 7, .max_scale_value = 0x01
SENSOR_TYPE_CARBON_DIOXIDE_CO2_LEVEL#
#define SENSOR_TYPE_CARBON_DIOXIDE_CO2_LEVELValue:
.value = 0x11, .byte_offset = 3, .bit_mask = 0, .max_scale_value = 0x00
SENSOR_TYPE_AIR_FLOW#
#define SENSOR_TYPE_AIR_FLOWValue:
.value = 0x12, .byte_offset = 3, .bit_mask = 1, .max_scale_value = 0x01
SENSOR_TYPE_TANK_CAPACITY#
#define SENSOR_TYPE_TANK_CAPACITYValue:
.value = 0x13, .byte_offset = 3, .bit_mask = 2, .max_scale_value = 0x02
SENSOR_TYPE_DISTANCE#
#define SENSOR_TYPE_DISTANCEValue:
.value = 0x14, .byte_offset = 3, .bit_mask = 3, .max_scale_value = 0x02
SENSOR_TYPE_ANGLE_POSITION#
#define SENSOR_TYPE_ANGLE_POSITIONValue:
.value = 0x15, .byte_offset = 3, .bit_mask = 4, .max_scale_value = 0x02
SENSOR_TYPE_ROTATION#
#define SENSOR_TYPE_ROTATIONValue:
.value = 0x16, .byte_offset = 3, .bit_mask = 5, .max_scale_value = 0x01
SENSOR_TYPE_WATER_TEMPERATURE#
#define SENSOR_TYPE_WATER_TEMPERATUREValue:
.value = 0x17, .byte_offset = 3, .bit_mask = 6, .max_scale_value = 0x01
SENSOR_TYPE_SOIL_TEMPERATURE#
#define SENSOR_TYPE_SOIL_TEMPERATUREValue:
.value = 0x18, .byte_offset = 3, .bit_mask = 7, .max_scale_value = 0x01
SENSOR_TYPE_SEISMIC_INTENSITY#
#define SENSOR_TYPE_SEISMIC_INTENSITYValue:
.value = 0x19, .byte_offset = 4, .bit_mask = 0, .max_scale_value = 0x03
SENSOR_TYPE_SEISMIC_MAGNITUDE#
#define SENSOR_TYPE_SEISMIC_MAGNITUDEValue:
.value = 0x1A, .byte_offset = 4, .bit_mask = 1, .max_scale_value = 0x03
SENSOR_TYPE_ULTRAVIOLET#
#define SENSOR_TYPE_ULTRAVIOLETValue:
.value = 0x1B, .byte_offset = 4, .bit_mask = 2, .max_scale_value = 0x00
SENSOR_TYPE_ELECTRICAL_RESISTIVITY#
#define SENSOR_TYPE_ELECTRICAL_RESISTIVITYValue:
.value = 0x1C, .byte_offset = 4, .bit_mask = 3, .max_scale_value = 0x00
SENSOR_TYPE_ELECTRICAL_CONDUCTIVITY#
#define SENSOR_TYPE_ELECTRICAL_CONDUCTIVITYValue:
.value = 0x1D, .byte_offset = 4, .bit_mask = 4, .max_scale_value = 0x00
SENSOR_TYPE_LOUDNESS#
#define SENSOR_TYPE_LOUDNESSValue:
.value = 0x1E, .byte_offset = 4, .bit_mask = 5, .max_scale_value = 0x01
SENSOR_TYPE_MOISTURE#
#define SENSOR_TYPE_MOISTUREValue:
.value = 0x1F, .byte_offset = 4, .bit_mask = 6, .max_scale_value = 0x03
SENSOR_TYPE_FREQUENCY#
#define SENSOR_TYPE_FREQUENCYValue:
.value = 0x20, .byte_offset = 4, .bit_mask = 7, .max_scale_value = 0x01
SENSOR_TYPE_TIME#
#define SENSOR_TYPE_TIMEValue:
.value = 0x21, .byte_offset = 5, .bit_mask = 0, .max_scale_value = 0x00
SENSOR_TYPE_TARGET_TEMPERATURE#
#define SENSOR_TYPE_TARGET_TEMPERATUREValue:
.value = 0x22, .byte_offset = 5, .bit_mask = 1, .max_scale_value = 0x01
SENSOR_TYPE_PARTICULATE_MATTER_2_5#
#define SENSOR_TYPE_PARTICULATE_MATTER_2_5Value:
.value = 0x23, .byte_offset = 5, .bit_mask = 2, .max_scale_value = 0x01
SENSOR_TYPE_FORMALDEHYDE_CH2O_LEVEL#
#define SENSOR_TYPE_FORMALDEHYDE_CH2O_LEVELValue:
.value = 0x24, .byte_offset = 5, .bit_mask = 3, .max_scale_value = 0x00
SENSOR_TYPE_RADON_CONCENTRATION#
#define SENSOR_TYPE_RADON_CONCENTRATIONValue:
.value = 0x25, .byte_offset = 5, .bit_mask = 4, .max_scale_value = 0x01
SENSOR_TYPE_METHANE_CH4_DENSITY#
#define SENSOR_TYPE_METHANE_CH4_DENSITYValue:
.value = 0x26, .byte_offset = 5, .bit_mask = 5, .max_scale_value = 0x00
SENSOR_TYPE_VOLATILE_ORGANIC_COMPOUND_LEVEL#
#define SENSOR_TYPE_VOLATILE_ORGANIC_COMPOUND_LEVELValue:
.value = 0x27, .byte_offset = 5, .bit_mask = 6, .max_scale_value = 0x01
SENSOR_TYPE_CARBON_MONOXIDE_CO_LEVEL#
#define SENSOR_TYPE_CARBON_MONOXIDE_CO_LEVELValue:
.value = 0x28, .byte_offset = 5, .bit_mask = 7, .max_scale_value = 0x01
SENSOR_TYPE_SOIL_HUMIDITY#
#define SENSOR_TYPE_SOIL_HUMIDITYValue:
.value = 0x29, .byte_offset = 6, .bit_mask = 0, .max_scale_value = 0x00
SENSOR_TYPE_SOIL_REACTIVITY#
#define SENSOR_TYPE_SOIL_REACTIVITYValue:
.value = 0x2A, .byte_offset = 6, .bit_mask = 1, .max_scale_value = 0x00
SENSOR_TYPE_SOIL_SALINITY#
#define SENSOR_TYPE_SOIL_SALINITYValue:
.value = 0x2B, .byte_offset = 6, .bit_mask = 2, .max_scale_value = 0x00
SENSOR_TYPE_HEART_RATE#
#define SENSOR_TYPE_HEART_RATEValue:
.value = 0x2C, .byte_offset = 6, .bit_mask = 3, .max_scale_value = 0x00
SENSOR_TYPE_BLOOD_PRESSURE#
#define SENSOR_TYPE_BLOOD_PRESSUREValue:
.value = 0x2D, .byte_offset = 6, .bit_mask = 4, .max_scale_value = 0x01
SENSOR_TYPE_MUSCLE_MASS#
#define SENSOR_TYPE_MUSCLE_MASSValue:
.value = 0x2E, .byte_offset = 6, .bit_mask = 5, .max_scale_value = 0x00
SENSOR_TYPE_FAT_MASS#
#define SENSOR_TYPE_FAT_MASSValue:
.value = 0x2F, .byte_offset = 6, .bit_mask = 6, .max_scale_value = 0x00
SENSOR_TYPE_BONE_MASS#
#define SENSOR_TYPE_BONE_MASSValue:
.value = 0x30, .byte_offset = 6, .bit_mask = 7, .max_scale_value = 0x00
SENSOR_TYPE_TOTAL_BODY_WATER_TBW#
#define SENSOR_TYPE_TOTAL_BODY_WATER_TBWValue:
.value = 0x31, .byte_offset = 7, .bit_mask = 0, .max_scale_value = 0x00
SENSOR_TYPE_BASIS_METABOLIC_RATE_BMR#
#define SENSOR_TYPE_BASIS_METABOLIC_RATE_BMRValue:
.value = 0x32, .byte_offset = 7, .bit_mask = 1, .max_scale_value = 0x00
SENSOR_TYPE_BODY_MASS_INDEX_BMI#
#define SENSOR_TYPE_BODY_MASS_INDEX_BMIValue:
.value = 0x33, .byte_offset = 7, .bit_mask = 2, .max_scale_value = 0x00
SENSOR_TYPE_ACCELERATION_X#
#define SENSOR_TYPE_ACCELERATION_XValue:
.value = 0x34, .byte_offset = 7, .bit_mask = 3, .max_scale_value = 0x00
SENSOR_TYPE_ACCELERATION_Y#
#define SENSOR_TYPE_ACCELERATION_YValue:
.value = 0x35, .byte_offset = 7, .bit_mask = 4, .max_scale_value = 0x00
SENSOR_TYPE_ACCELERATION_Z#
#define SENSOR_TYPE_ACCELERATION_ZValue:
.value = 0x36, .byte_offset = 7, .bit_mask = 5, .max_scale_value = 0x00
SENSOR_TYPE_SMOKE_DENSITY#
#define SENSOR_TYPE_SMOKE_DENSITYValue:
.value = 0x37, .byte_offset = 7, .bit_mask = 6, .max_scale_value = 0x00
SENSOR_TYPE_WATER_FLOW#
#define SENSOR_TYPE_WATER_FLOWValue:
.value = 0x38, .byte_offset = 7, .bit_mask = 7, .max_scale_value = 0x00
SENSOR_TYPE_WATER_PRESSURE#
#define SENSOR_TYPE_WATER_PRESSUREValue:
.value = 0x39, .byte_offset = 8, .bit_mask = 0, .max_scale_value = 0x00
SENSOR_TYPE_RF_SIGNAL_STRENGTH#
#define SENSOR_TYPE_RF_SIGNAL_STRENGTHValue:
.value = 0x3A, .byte_offset = 8, .bit_mask = 1, .max_scale_value = 0x01
SENSOR_TYPE_PARTICULATE_MATTER_10#
#define SENSOR_TYPE_PARTICULATE_MATTER_10Value:
.value = 0x3B, .byte_offset = 8, .bit_mask = 2, .max_scale_value = 0x01
SENSOR_TYPE_RESPIRATORY_RATE#
#define SENSOR_TYPE_RESPIRATORY_RATEValue:
.value = 0x3C, .byte_offset = 8, .bit_mask = 3, .max_scale_value = 0x00
SENSOR_TYPE_RELATIVE_MODULATION_LEVEL#
#define SENSOR_TYPE_RELATIVE_MODULATION_LEVELValue:
.value = 0x3D, .byte_offset = 8, .bit_mask = 4, .max_scale_value = 0x00
SENSOR_TYPE_BOILER_WATER_TEMPERATURE#
#define SENSOR_TYPE_BOILER_WATER_TEMPERATUREValue:
.value = 0x3E, .byte_offset = 8, .bit_mask = 5, .max_scale_value = 0x01
SENSOR_TYPE_DOMESTIC_HOT_WATER_DHW_TEMPERATURE#
#define SENSOR_TYPE_DOMESTIC_HOT_WATER_DHW_TEMPERATUREValue:
.value = 0x3F, .byte_offset = 8, .bit_mask = 6, .max_scale_value = 0x01
SENSOR_TYPE_OUTSIDE_TEMPERATURE#
#define SENSOR_TYPE_OUTSIDE_TEMPERATUREValue:
.value = 0x40, .byte_offset = 8, .bit_mask = 7, .max_scale_value = 0x01
SENSOR_TYPE_EXHAUST_TEMPERATURE#
#define SENSOR_TYPE_EXHAUST_TEMPERATUREValue:
.value = 0x41, .byte_offset = 9, .bit_mask = 0, .max_scale_value = 0x01
SENSOR_TYPE_WATER_CHLORINE_LEVEL#
#define SENSOR_TYPE_WATER_CHLORINE_LEVELValue:
.value = 0x42, .byte_offset = 9, .bit_mask = 1, .max_scale_value = 0x00
SENSOR_TYPE_WATER_ACIDITY#
#define SENSOR_TYPE_WATER_ACIDITYValue:
.value = 0x43, .byte_offset = 9, .bit_mask = 2, .max_scale_value = 0x00
SENSOR_TYPE_WATER_OXIDATION_REDUCTION_POTENTIAL#
#define SENSOR_TYPE_WATER_OXIDATION_REDUCTION_POTENTIALValue:
.value = 0x44, .byte_offset = 9, .bit_mask = 3, .max_scale_value = 0x00
SENSOR_TYPE_HEART_RATE_LF_HF_RATIO#
#define SENSOR_TYPE_HEART_RATE_LF_HF_RATIOValue:
.value = 0x45, .byte_offset = 9, .bit_mask = 4, .max_scale_value = 0x00
SENSOR_TYPE_MOTION_DIRECTION#
#define SENSOR_TYPE_MOTION_DIRECTIONValue:
.value = 0x46, .byte_offset = 9, .bit_mask = 5, .max_scale_value = 0x00
SENSOR_TYPE_APPLIED_FORCE_ON_THE_SENSOR#
#define SENSOR_TYPE_APPLIED_FORCE_ON_THE_SENSORValue:
.value = 0x47, .byte_offset = 9, .bit_mask = 6, .max_scale_value = 0x00
SENSOR_TYPE_RETURN_AIR_TEMPERATURE#
#define SENSOR_TYPE_RETURN_AIR_TEMPERATUREValue:
.value = 0x48, .byte_offset = 9, .bit_mask = 7, .max_scale_value = 0x01
SENSOR_TYPE_SUPPLY_AIR_TEMPERATURE#
#define SENSOR_TYPE_SUPPLY_AIR_TEMPERATUREValue:
.value = 0x49, .byte_offset = 10, .bit_mask = 0, .max_scale_value = 0x01
SENSOR_TYPE_CONDENSER_COIL_TEMPERATURE#
#define SENSOR_TYPE_CONDENSER_COIL_TEMPERATUREValue:
.value = 0x4A, .byte_offset = 10, .bit_mask = 1, .max_scale_value = 0x01
SENSOR_TYPE_EVAPORATOR_COIL_TEMPERATURE#
#define SENSOR_TYPE_EVAPORATOR_COIL_TEMPERATUREValue:
.value = 0x4B, .byte_offset = 10, .bit_mask = 2, .max_scale_value = 0x01
SENSOR_TYPE_LIQUID_LINE_TEMPERATURE#
#define SENSOR_TYPE_LIQUID_LINE_TEMPERATUREValue:
.value = 0x4C, .byte_offset = 10, .bit_mask = 3, .max_scale_value = 0x01
SENSOR_TYPE_DISCHARGE_LINE_TEMPERATURE#
#define SENSOR_TYPE_DISCHARGE_LINE_TEMPERATUREValue:
.value = 0x4D, .byte_offset = 10, .bit_mask = 4, .max_scale_value = 0x01
SENSOR_TYPE_SUCTION_INPUT_PUMP_COMPRESSOR_PRESSURE#
#define SENSOR_TYPE_SUCTION_INPUT_PUMP_COMPRESSOR_PRESSUREValue:
.value = 0x4E, .byte_offset = 10, .bit_mask = 5, .max_scale_value = 0x01
SENSOR_TYPE_DISCHARGE_OUTPUT_PUMP_COMPRESSOR_PRESSURE#
#define SENSOR_TYPE_DISCHARGE_OUTPUT_PUMP_COMPRESSOR_PRESSUREValue:
.value = 0x4F, .byte_offset = 10, .bit_mask = 6, .max_scale_value = 0x01
SENSOR_TYPE_DEFROST_TEMPERATURE_DEFROST#
#define SENSOR_TYPE_DEFROST_TEMPERATURE_DEFROSTValue:
.value = 0x50, .byte_offset = 10, .bit_mask = 7, .max_scale_value = 0x01
SENSOR_TYPE_OZONE_O3#
#define SENSOR_TYPE_OZONE_O3Value:
.value = 0x51, .byte_offset = 11, .bit_mask = 0, .max_scale_value = 0x00
SENSOR_TYPE_SULFUR_DIOXIDE_SO2#
#define SENSOR_TYPE_SULFUR_DIOXIDE_SO2Value:
.value = 0x52, .byte_offset = 11, .bit_mask = 1, .max_scale_value = 0x00
SENSOR_TYPE_NITROGEN_DIOXIDE_NO2#
#define SENSOR_TYPE_NITROGEN_DIOXIDE_NO2Value:
.value = 0x53, .byte_offset = 11, .bit_mask = 2, .max_scale_value = 0x00
SENSOR_TYPE_AMMONIA_NH3#
#define SENSOR_TYPE_AMMONIA_NH3Value:
.value = 0x54, .byte_offset = 11, .bit_mask = 3, .max_scale_value = 0x00
SENSOR_TYPE_LEAD_PB#
#define SENSOR_TYPE_LEAD_PBValue:
.value = 0x55, .byte_offset = 11, .bit_mask = 4, .max_scale_value = 0x00
SENSOR_TYPE_PARTICULATE_MATTER_1#
#define SENSOR_TYPE_PARTICULATE_MATTER_1Value:
.value = 0x56, .byte_offset = 11, .bit_mask = 5, .max_scale_value = 0x00
SENSOR_TYPE_PERSON_COUNTER_ENTERING#
#define SENSOR_TYPE_PERSON_COUNTER_ENTERINGValue:
.value = 0x57, .byte_offset = 11, .bit_mask = 6, .max_scale_value = 0x00
SENSOR_TYPE_PERSON_COUNTER_EXITING#
#define SENSOR_TYPE_PERSON_COUNTER_EXITINGValue:
.value = 0x58, .byte_offset = 11, .bit_mask = 7, .max_scale_value = 0x00
SENSOR_TYPE_CASE#
#define SENSOR_TYPE_CASEValue:
Helper macro to generate a single case in the sensor type lookup Sensor types that are accessed by the application code are allocated statically.
Unused sensor types are optimized out at compile time.
SENSOR_TYPE_FROM_NAME#
#define SENSOR_TYPE_FROM_NAME
Macro to map sensor_name_t enum to corresponding sensor type.
SLI_MAX_RAW_RESULT_BYTES#
#define SLI_MAX_RAW_RESULT_BYTESValue:
4
Structure that holds a read result from the read interface.