Z-Wave Serial API#
Modules#
Enumerations#
enum
NVM_BACKUP_RESTORE_ADDR_SIZE = 2
NVM_EXT_BACKUP_RESTORE_ADDR_SIZE = 4
}
size of the address field of NVM_BACKUP_RESTORE or NVM_EXT_BACKUP_RESTORE frames.
enum
Macros#
#define
SOF 0x01
Start Of Frame.
#define
ACK 0x06
Acknowledge successful frame reception.
#define
NAK 0x15
Not Acknowledge successful frame reception - please retransmit...
#define
CAN 0x18
Frame received (from host) was dropped - waiting for ACK.
Enumeration Documentation#
nvm_backup_restore_addr_size_t#
nvm_backup_restore_addr_size_t
size of the address field of NVM_BACKUP_RESTORE or NVM_EXT_BACKUP_RESTORE frames.
Item value is the size in byte of the address field.
| Enumerator | |
|---|---|
| NVM_BACKUP_RESTORE_ADDR_SIZE | 2 bytes for the legacy NVM backup & restore command |
| NVM_EXT_BACKUP_RESTORE_ADDR_SIZE | 4 bytes for the extended NVM backup & restore command |
power_lock_type_t#
power_lock_type_t
Power Lock Type enumeration.
| Enumerator | |
|---|---|
| POWER_LOCK_TYPE_RADIO | Radio power lock. |
| POWER_LOCK_TYPE_IO | IO power lock (requires Shutdown Manager) |