Z-Wave Serial API#

Modules#

Frame Types

GET_INIT_DATA_FLAG

FUNC_ID

Enumerations#

enum
NVM_BACKUP_RESTORE_ADDR_SIZE = 2
NVM_EXT_BACKUP_RESTORE_ADDR_SIZE = 4
}

size of the address field of NVM_BACKUP_RESTORE or NVM_EXT_BACKUP_RESTORE frames.

enum
POWER_LOCK_TYPE_RADIO = 0
POWER_LOCK_TYPE_IO = 1
}

Power Lock Type enumeration.

Macros#

#define
SOF 0x01

Start Of Frame.

#define
ACK 0x06

Acknowledge successful frame reception.

#define
NAK 0x15

Not Acknowledge successful frame reception - please retransmit...

#define
CAN 0x18

Frame received (from host) was dropped - waiting for ACK.

#define
SAPI_COMMAND_STATUS_FAILURE 0x00
#define
SAPI_COMMAND_STATUS_SUCCESS 0x01

Enumeration Documentation#

nvm_backup_restore_addr_size_t#

nvm_backup_restore_addr_size_t

size of the address field of NVM_BACKUP_RESTORE or NVM_EXT_BACKUP_RESTORE frames.

Item value is the size in byte of the address field.

Enumerator
NVM_BACKUP_RESTORE_ADDR_SIZE

2 bytes for the legacy NVM backup & restore command

NVM_EXT_BACKUP_RESTORE_ADDR_SIZE

4 bytes for the extended NVM backup & restore command


power_lock_type_t#

power_lock_type_t

Power Lock Type enumeration.

Enumerator
POWER_LOCK_TYPE_RADIO

Radio power lock.

POWER_LOCK_TYPE_IO

IO power lock (requires Shutdown Manager)