Switch On/Off#

The Z-Wave certified Switch On/Off application shows a switch implementation, that turns on any device that is connected to power. Examples include lights, appliances, etc.

Role Type

Always On End device (AOS)

Supporting Device Type

Actuator

Device Type

Binary Switch

Generic Type

Switch Binary

Specific Type

Not Used

Requested security keys

S0, S2_UNAUTHENTICATED, and S2_AUTHENTICATED

Supported Command Classes#

The Switch On/Off application implements mandatory and some optional command classes. The table below lists the supported Command Classes, their version, and their required Security class.

Command Class

Version

Required Security Class

Association

2

Highest granted Security Class

Association Group Info

3

Highest granted Security Class

Basic

2

Highest granted Security Class

Binary Switch

2

Highest granted Security Class

Device Reset Locally

1

Highest granted Security Class

Firmware Update Meta Data

5

Highest granted Security Class

Indicator

3

Highest granted Security Class

Manufacturer Specific

2

Highest Granted Security Class

Multi-Channel Association

3

Highest granted Security Class

Powerlevel

1

Highest granted Security Class

Security 0

1

None

Security 2

1

None

Supervision

1

None

Transport Service

2

None

Version

3

Highest granted Security Class

Z-Wave Plus Info

2

None

Basic Command Class mapping#

Basic Command Class is mapped to Binary Switch CC

Basic Command

Mapped Command

Basic Set (Value)

Binary Switch Set (Value)

Basic Report (Current Value, Duration)

Binary Switch Report (Value, Duration)

Association Group configuration#

ID

Name

Node Count

Description

1

Lifeline

X

Supports the following command classes:

  • Device Reset Locally: triggered upon reset.

  • Binary Switch Report: Triggered when the switch changes state.

  • Indicator Report: Triggered when LED0 changes state.

X: For Z-Wave node count is equal to 5 and for Z-Wave Long Range it is 1.

Usage of Buttons and LED Status#

We are differentiating four different types of button presses. The following types are the same for the BTN0 and BTN1 on the WSTK board. The duration values can be configured under the config directory in app_button_press_config.h file in each generated application/project.

Please note external wakeup is not supported on button 1 in case of brd2603a and brd2603c.

Press Type

Duration

Short Press

0 - 400 ms

Medium Press

401 - 1500 ms

Long Press

1501 - 5000 ms

Very Long Press

Every press longer than Long Press

Button

Action

Description

RST

Press

Resets the firmware of an application (like losing power). All volatile memory will be cleared.

BTN0

Short Press

Toggles LED1

BTN1

Short Press

Enter "learn mode" (sending node info frame) to add/remove the device.
Removing the device from a network will reset it.

Very Long Press

Perform a reset to factory default operation of the device, and a Device Reset Locally Notification Command is sent via Lifeline.

LED

Description

LED0

Blinks with 1 Hz when learn mode is active.
Used for Indicator Command Class.

LED1

Switch:

  • LED ON indicates SWITCH ON

  • LED OFF indicates SWITCH OFF

Firmware Update#

This section will describe backward compatibility when upgrading the Switch On/Off application from one SDK to a newer version.

CLI Support#

In case CLI support is needed, please install zw_cli_common component to the project. Please note that the zw_cli_common component will modify the power consumption for every application.

The default baud rate is 9600, which allows the underlying EUSART module to work in EM2. On some development kits (e.g. BRD2603C and BRD2705A), the following command should be applied in Simplicity Studio via the Admin console to adjust the baudrate: serial vcom config speed 9600.

Available CLI commands#

Command

Arguments

Description

help

-

Printing all supported CLI commands and their description.

set_learn_mode

-

Toggling the learn mode functionality. In case the learn mode started, but inclusion does not happen,learn mode will automatically stop after about 30 seconds

factory_reset

-

Executing factory reset

get_dsk

-

Printing out the generated DSK of the device

get_region

-

Printing out the set region of the application

toggle_led

-

Toggling LED1

send_nif

-

Sending Node Information Frame

get_led_state

-

Get the state of the LED1. Can be "on" or "off"