Access Control Features#
ZAP supports access control on all ZCL entities. It's down to the implementation of the SDK to map these features to the required and supported access control SDK features. ZAP generally provides a data model and a mechanism to encode it in the meta-info files and propagate that data to the generation templates, without assigning specific meanings to the data points.
Base Terms#
ZAP access control defines three base terms, as follows:
operation : defined as something that can be done. Example: read, write, invoke.
role: defined as a privilege of an actor. Such as "View privilege", "Administrative role", and son on.
modifiers: defined as special access control conditions, such as fabric sensitive data or fabric scoped data.
The base terms are defined in the metadata XML under a top tag <accessControl>. The following is an example of access control base term definitions:
<accessControl> <operation type="read" description="Read operation"/> <operation type="write" description="Write operation"/> <operation type="invoke" description="Invoke operation"/> <modifier type="fabric-scoped" description="Fabric-scoped data"/> <modifier type="fabric-sensitive" description="Fabric-sensitive data"/> <role type="view" description="View privilege"/> <role type="operate" description="Operate privilege"/> <role type="manage" description="Managing privilege"/> <role type="administer" description="Administrative privilege"/> </accessControl>
This example defines three operations, read, write and invoke, two modifiers and four roles.
Access Triplets#
Each individual access condition can be defined with an access triplet in the XML. Access triplet is a combination of an operation, role and modifier. They are optional, so you can only have one of these. A missing part of triplet generally means permissivenes, which is implementation-specific for the given SDK. An entity that defines it's access can have one or more access triplets.
The following is an example:
<attribute side="server" code="0x0000" define="AT1" type="INT64U" writable="false" optional="true"> <description>at1</description> <access op="write" role="manage" modifier="fabric-scoped"/> </attribute>
This is a definition of an attribute that has an access triplet, declaring it allows write operation by a manage role, with fabric-scoped modifier applied.
Default Permissions#
ZCL entities can define their own individual permissions. However, there is also a global definition of default permissions for given types. These are assumed for the given entity, unless it provides any specific permissions of its own.
Default permissions are declared via a <defaultAccess> tag at the top level of the XML file.
Example:
<defaultAccess type="command"> <access op="invoke"/> </defaultAccess> <defaultAccess type="cluster"> <access op="read"/> <access op="write"/> </defaultAccess> <defaultAccess type="attribute"> <access op="read" role="view"/> <access op="write" role="operate"/> </defaultAccess>
Template Helpers#
The basic template helper to use is the {{#access}} ... {{/access}} iterator. This iterator iterates over all given access triplets.
It supports the following two options:
entity="attribute/command/event"- if the entity can't be determined from context, this sets the entity type.includeDefault="true/false"- determines if default values are included or not.
The following is an example:
{{#zcl_clusters}} Cluster: {{name}} [{{code}}] {{#zcl_attributes}} - attribute: {{name}} [{{code}}] {{#access entity="attribute"}} * Op: {{operation}} / Role: {{role}} / Modifier: {{accessModifier}} {{/access}} {{/zcl_attributes}} {{#zcl_commands}} - command: {{name}} [{{code}}] {{#access entity="command"}} * Op: {{operation}} / Role: {{role}} / Modifier: {{accessModifier}} {{/access}} {{/zcl_commands}} {{#zcl_events}} - event: {{name}} [{{code}}] {{#access entity="event"}} * Op: {{operation}} / Role: {{role}} / Modifier: {{accessModifier}} {{/access}} {{/zcl_events}} {{/zcl_clusters}}