Getting Started with ZAP#
These sections describe different methods to create Zigbee and Matter applications. Note that Simplicity Studio provides a way to create your Zigbee and Matter applications from end to end where all tools come pre-installed along with Simplicity Studio (including ZAP). You may also decide to explore other ways of creating your applications, as described here.
Zigbee Development#
Zigbee application developers can build their applications using Simplicity Studio, which already includes ZAP and other tools that help you build your application from end to end.
Matter Development#
Matter Application developers can build their applications using the following methods:
Simplicity Studio: This includes ZAP and other tools which are needed to build the Matter application end to end.
Note: To update ZAP outside the Simplicity Studio release cycle, see update ZAP in Simplicity Studio and ZAP Installation Guide