Configuration for Silicon Labs Devices#
Silicon Labs devices use Zephyr's standard configuration mechanisms -- Kconfig and Devicetree.
Devicetree bindings documentation describes the contents of Devicetree nodes.
Kconfig search provides documentation for Kconfig entries. Search terms such as
SPI.*SILABSare useful for finding options related to specific drivers for Silicon Labs hardware.
Series 2-specific Configuration#
While Devicetree and Kconfig are generic configuration interfaces, the values used may be specific to the hardware implementation:
SiWx91x-specific Configuration#
While Devicetree and Kconfig are generic configuration interfaces, the values used may be specific to the hardware implementation:
Zephyr Kernel Thread and Scheduling Details#
The Zephyr RTOS kernel has some features that differ from other RTOS kernels such as FreeRTOS or Micrium OS. Zephyr partitions the system into preemptive threads and cooperative threads.
Cooperative threads always have scheduling priority over preemptive threads. They run until they yield or pend on a kernel object.
Meta-IRQ threads are a special type of cooperative thread that can preempt other cooperative threads.
The Bluetooth stack runs as several cooperative threads. On Series 2 devices, the Bluetooth Link Layer runs as a meta-IRQ thread.
Interrupt Priorities#
Silicon Labs devices use the Simplicity SDK HAL, which requires that the base priority register of the ARM Cortex-M CPU is set to 3. A BASEPRI value of 3 means that the highest interrupt priorities (0-2) are not blocked by critical sections such as irq_lock() or spinlocks. See the Zephyr Project interrupt documentation for more details.
In Zephyr, the base priority is configured to be compatible with the Simplicity SDK by enabling CONFIG_ZERO_LATENCY_IRQS and setting CONFIG_ZERO_LATENCY_LEVELS=2. This is done by default in Series 2 and SiWx91x SoC Kconfig files.
Interrupt priorities are configured in Devicetree (DTS) by assigning an interrupt number and priority to the peripheral node:
&eusart1 {
interrupts = <68 0>, <69 0>;
interrupt-names = "rx", "tx";
}For normal interrupts, the numbers configured in Devicetree are automatically offset by the base priority offset. For example, a priority value of 0 in DTS corresponds to a priority of 3 in the ARM Nested Vectored Interrupt Controller (NVIC).
If an ISR is installed in the vector table using the IRQ_ZERO_LATENCY flag, the priority from DTS is used as-is. As noted above, such interrupts will not be blocked by interrupt locks.