Functions

void emberZigbeeKeyEstablishmentHandler ( EmberEUI64 partner, EmberKeyStatus status)
Notifies the application of the status of the request for a Link Key. The application should define EMBER_APPLICATION_HAS_ZIGBEE_KEY_ESTABLISHMENT_HANDLER to implement its own handler.

Detailed Description

These callbacks are contributed by the Multi-Network Stub Library plugin.

Function Documentation

void emberZigbeeKeyEstablishmentHandler ( EmberEUI64 partner,
EmberKeyStatus status
)

Notifies the application of the status of the request for a Link Key. The application should define EMBER_APPLICATION_HAS_ZIGBEE_KEY_ESTABLISHMENT_HANDLER to implement its own handler.

Parameters
partner The IEEE address of the partner device or all zeros if the Key establishment failed.
status The status of the key establishment.