Plugin Commands: Green Power Server
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_COMMISSION |
plugin green-power-server commission [action:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_CRYPTOTEST |
plugin green-power-server cryptotest | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_TABLE_CLEAR |
plugin green-power-server table-clear | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_TABLE_PRINT |
plugin green-power-server table-print | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_TABLE_SET |
plugin green-power-server table-set [index:1] [valid:1] [options:1] [gpdEndpoint:1] [gpdIeeeAddr:8] [sourceId:4] [endpoint:1] [gpdCommand:1] [zigbeeProfile:2] [zigbeeCluster:2] [zigbeeCommandId:2] [payloadSrc:1] [zclPayloadDefault:-1] |
Detailed Description
The Green Power Server plugin contributes CLI commands to the application framework to be used for getting, setting, and displaying information relevant to the Green Power Server cluster.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_COMMISSION |
plugin green-power-server commission [action:1]
- Put the GPS in commissioning mode
- action - INT8U - 1 to enter, 2 to leave
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_CRYPTOTEST |
plugin green-power-server cryptotest
- Crypto test
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_TABLE_CLEAR |
plugin green-power-server table-clear
- Clear all entries within the customized translation table.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_TABLE_PRINT |
plugin green-power-server table-print
- Clear all entries within the customized translation table.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_SERVER_PLUGIN_GREEN_POWER_SERVER_TABLE_SET |
plugin green-power-server table-set [index:1] [valid:1] [options:1] [gpdEndpoint:1] [gpdIeeeAddr:8] [sourceId:4] [endpoint:1] [gpdCommand:1] [zigbeeProfile:2] [zigbeeCluster:2] [zigbeeCommandId:2] [payloadSrc:1] [zclPayloadDefault:-1]
- Clear all entries within the customized translation table.
- index - INT8U - index to translation table
- valid - BOOLEAN - flag indicating if the entry is valid or not
- options - INT8U
- gpdEndpoint - INT8U
- gpdIeeeAddr - IEEE_ADDRESS
- sourceId - INT32U
- endpoint - INT8U - the endpoint for which the translation is valid.
- gpdCommand - INT8U
- zigbeeProfile - INT16U
- zigbeeCluster - INT16U
- zigbeeCommandId - INT16U
- payloadSrc - INT8U
- zclPayloadDefault - OCTET_STRING