Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_APPEND
plugin messaging-server append [message:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_CANCEL
plugin messaging-server cancel [nodeId:2] [srcEndpoint:1] [dstEndpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_CONFIRM_NOT
plugin messaging-server confirm not
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_CONFIRM_REQ
plugin messaging-server confirm req
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_DISPLAY
plugin messaging-server display [nodeId:2] [srcEndpoint:1] [dstEndpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_ID
plugin messaging-server id [messageId:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_CRITICAL
plugin messaging-server importance critical
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_HIGH
plugin messaging-server importance high
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_LOW
plugin messaging-server importance low
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_MEDIUM
plugin messaging-server importance medium
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_INVALID
plugin messaging-server invalid [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_MESSAGE
plugin messaging-server message [message:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_PRINT
plugin messaging-server print [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_RELATIVE_TIME
plugin messaging-server relative-time [time:4] [duration:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TIME
plugin messaging-server time [time:4] [duration:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TRANSMISSION_BOTH
plugin messaging-server transmission both
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TRANSMISSION_IPAN
plugin messaging-server transmission ipan
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TRANSMISSION_NORMAL
plugin messaging-server transmission normal
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_VALID
plugin messaging-server valid [endpoint:1]

Detailed Description

The messaging-server plugin contributes CLI commands to the application framework to be used for manipulating messages in a server context.

Macro Definition Documentation

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_APPEND

plugin messaging-server append [message:-1]

  • Append an additional string to the message contained in the message plugin
    • message - OCTET_STRING - the string to append to the current message
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_CANCEL

plugin messaging-server cancel [nodeId:2] [srcEndpoint:1] [dstEndpoint:1]

  • Cancel the message.
    • nodeId - INT16U - The destination of the message.
    • srcEndpoint - INT8U - The source endpoint of the message.
    • dstEndpoint - INT8U - The destination endpoint of the message.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_CONFIRM_NOT

plugin messaging-server confirm not

  • Set the message confirmation to not used.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_CONFIRM_REQ

plugin messaging-server confirm req

  • Set message confirmation to required.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_DISPLAY

plugin messaging-server display [nodeId:2] [srcEndpoint:1] [dstEndpoint:1]

  • Display the message.
    • nodeId - INT16U - The destination of the message.
    • srcEndpoint - INT8U - The source endpoint of the message.
    • dstEndpoint - INT8U - The destination endpoint of the message.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_ID

plugin messaging-server id [messageId:4]

  • Set the message id for the message contained in the messaging plugin
    • messageId - INT32U - message id
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_CRITICAL

plugin messaging-server importance critical

  • Set the message importance to critical.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_HIGH

plugin messaging-server importance high

  • Set the message importance to high.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_LOW

plugin messaging-server importance low

  • Set the message importance to low.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_MEDIUM

plugin messaging-server importance medium

  • Set the message importance to medium.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_INVALID

plugin messaging-server invalid [endpoint:1]

  • Set the message validity to invalid.
    • endpoint - INT8U - The relevant endpoint.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_MESSAGE

plugin messaging-server message [message:-1]

  • Set the message used by the message plugin.
    • message - OCTET_STRING - The message to set
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_PRINT

plugin messaging-server print [endpoint:1]

  • Print the message info.
    • endpoint - INT8U - The relevant endpoint.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_RELATIVE_TIME

plugin messaging-server relative-time [time:4] [duration:4]

  • Set the relative time on the message.
    • time - INT32U - number of minutes to add to the message time above the current time
    • duration - INT32U - duration in minutes for the message to be valid
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TIME

plugin messaging-server time [time:4] [duration:2]

  • Set the start time and duration for the message used by the message plugin.
    • time - INT32U - start time
    • duration - INT16U - duration
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TRANSMISSION_BOTH

plugin messaging-server transmission both

  • Set the message control bit mask in the message to normal and anonymous.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TRANSMISSION_IPAN

plugin messaging-server transmission ipan

  • Set the message control bit mask in the message to anonymous.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TRANSMISSION_NORMAL

plugin messaging-server transmission normal

  • Sets the message control bit mask to normal transmission.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_VALID

plugin messaging-server valid [endpoint:1]

  • Set the message validity to valid.
    • endpoint - INT8U - The relevant endpoint.