Plugin Commands: OTA Client
Detailed Description
The OTA Client plugin provides Over-the-air commands for upgrading firmware and downloading specific files on the client side.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BLOCK_TEST |
plugin ota-client block-test
- Sends an image block request for a file the server should not have. Test harness only (test case 9.5.6 - Missing File)
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BOOTLOAD |
plugin ota-client bootload [index:1]
- Bootloads the image at the specified index by calling the OTA bootload callback.
- index - INT8U - The index at which to begin bootloading the image
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_INFO |
plugin ota-client info
- Prints the manufacturer ID, Image Type ID, and Version information that are used when a query next image is sent to the server by the client
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAGE_REQUEST |
plugin ota-client page-request [pageRequest:1]
- pageRequest - INT8U - boolean value turning on (1) or off (0) the page request flag
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAUSE_AT |
plugin ota-client pause-at [stopDownloadPercentage:1]
- stopDownloadPercentage - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_START |
plugin ota-client start
- Starts the ota client state machine. The state machine discovers the OTA server, queries for new images, downloads the images and waits for the server command to upgrade
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STATUS |
plugin ota-client status
- Prints information on the current state of the OTA client download.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STOP |
plugin ota-client stop
- Stops the OTA state machine
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_UPGRADE_REQUEST |
plugin ota-client upgrade-request
- Send an OTA server an UpgradeEndRequest
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_VERIFY |
plugin ota-client verify [index:1]
- Perform signature verification on the image at the specified index
- index - INT8U - The index at which to begin verification of the image