Zigbee PRO Stack Library Callbacks
Functions | |
void | emberOrphanNotificationHandler (EmberEUI64 longId) |
bool | emberMacPassthroughFilterHandler (uint8_t *macHeader) |
Invoked by the EmberZNet stack to filter out incoming application MAC passthrough messages. If this returns true for a message the complete message will be passed to emberMacPassthroughMessageHandler() with a type of EMBER_MAC_PASSTHROUGH_APPLICATION. | |
void | emberIncomingCommandHandler (EmberZigbeeCommandType commandType, EmberMessageBuffer commandBuffer, uint8_t indexOfCommand, void *data) |
A protocol layer command has been received by the stack. | |
void | emberOutgoingCommandHandler (EmberZigbeeCommandType commandType, EmberMessageBuffer commandBuffer, uint8_t indexOfCommand, void *data) |
The stack is preparing to send a protocol layer command. |
Detailed Description
These callbacks are contributed by the Zigbee PRO Stack Library plugin.
Function Documentation
void emberIncomingCommandHandler | ( | EmberZigbeeCommandType | commandType, |
EmberMessageBuffer | commandBuffer, |
||
uint8_t | indexOfCommand, |
||
void * | data |
||
) |
A protocol layer command has been received by the stack.
This is called when the stack receives a command that is meant for one of the protocol layers specified in EmberZigbeeCommandType. The implementation can get a flat buffer of bytes representing the command byte plus the command payload by calling ::emberCopyFromLinkedBuffers() with a contents array big enough to hold the command payload.
The commandType argument is one of the values of the EmberZigbeeCommandType enumeration. If the stack receives an 802.15.4 MAC beacon, it will call this function with the commandType argument set to EMBER_ZIGBEE_COMMAND_TYPE_BEACON.
The implementation of this callback should not alter the data contained in the EmberMessageBuffer, since the stack will still be processing the command at the time that this is called.
- Parameters
-
commandType
The type of command received. See EmberZigbeeCommandType. commandBuffer
The EmberMessageBuffer, for the command payload. indexOfCommand
The starting index in the EmberMessageBuffer for the command. This means the first byte at this index will be the command byte itself, and the reset will be the command payload. data
This is a pointer to auxiliary data for the command. ZDO commands pass the EmberApsFrame associated with the packet here. Otherwise, this value is NULL.
bool emberMacPassthroughFilterHandler | ( | uint8_t * | macHeader | ) |
Invoked by the EmberZNet stack to filter out incoming application MAC passthrough messages. If this returns true for a message the complete message will be passed to emberMacPassthroughMessageHandler() with a type of EMBER_MAC_PASSTHROUGH_APPLICATION.
Note that this callback may be invoked in ISR context and should execute as quickly as possible.
Note that this callback may be called more than once per incoming message. Therefore, the callback code should not depend on being called only once, and should return the same value each time it is called with a given header.
If the application includes this callback, it must define EMBER_APPLICATION_HAS_MAC_PASSTHROUGH_FILTER_HANDLER in its CONFIGURATION_HEADER.
- Parameters
-
macHeader
A pointer to the initial portion of the incoming MAC header. This contains the MAC frame control and addressing fields. Subsequent MAC fields, and the MAC payload, may not be present.
- Returns
- true if the messages is an application MAC passthrough message.
void emberOrphanNotificationHandler | ( | EmberEUI64 | longId | ) |
void emberOutgoingCommandHandler | ( | EmberZigbeeCommandType | commandType, |
EmberMessageBuffer | commandBuffer, |
||
uint8_t | indexOfCommand, |
||
void * | data |
||
) |
The stack is preparing to send a protocol layer command.
This is called when the stack is preparing to send a command from one of the protocol layers specified in EmberZigbeeCommandType. The implementation can get a flat buffer of bytes representing the command byte plus the command payload by calling ::emberCopyFromLinkedBuffers() with a contents array big enough to hold the command payload.
The commandType argument is one of the values of the EmberZigbeeCommandType enum. If the stack is preparing to send an 802.15.4 MAC beacon, it will call this function with the commandType argument set to EMBER_ZIGBEE_COMMAND_TYPE_BEACON.
The implementation of this callback may alter the data contained in the EmberMessageBuffer, modify options and flags in the auxillary data, or consume the command itself, either sending the command, or discarding it as it sees fit.
- Parameters
-
commandType
The type of command being sent. See EmberZigbeeCommandType. commandBuffer
The EmberMessageBuffer for the command payload. indexOfCommand
The starting index in the EmberMessageBuffer for the command. This means the first byte at this index will be the command byte itself, and the rest will be the command payload. data
This is a pointer to auxillary data for the command. The field should be NULL if it is not used.