Silicon Labs
zigbee/6.3/af_v2/structEmberAfCommandMetadata
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
    Results 1-5 of 5 for zigbee/6.3/af_v2/structEmberAfCommandMetadata in 0.90 seconds
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    stream_poll stream_read stream_write write ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... c rc: CRC32 checksum of the file data, in hex format 2 .
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS ... framework provides a hardened bootloader, read/write file system, safemode recovery mechanism, ...
    ProductWireless Resource TypeSoftware API documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    Example Example usage. Alphabetical List of Commands ... os pins can only use the strong drive strength. ... read the bus mode of the remote peripheral ... scan high -20dBm Example scan high
    ProductWireless Resource TypeSoftware API documentation
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Modules ... Issue Gecko OS command asynchronously and invoke callback on completion. ... [out] buffer Buffer to hold returned data [in] ... [out] buffer Buffer to hold string result [in]
    ProductWireless Resource TypeSoftware API documentation
      Results 1-5 of 5 for zigbee/6.3/af_v2/structEmberAfCommandMetadata