EmberAfImageBlockRequestCallbackStruct Struct Reference

This is the data structure that is passed to the emberAfImageBlockRequestCallback() to let the application decide what to do.

#include < af-types.h >

Data Fields

const EmberAfOtaImageId * id
uint32_t offset
uint32_t waitTimeSecondsResponse
EmberNodeId source
EmberEUI64 sourceEui
uint16_t minBlockRequestPeriod
uint8_t maxDataSize
uint8_t clientEndpoint
EmberAfImageBlockRequestOptions bitmask

This is the data structure that is passed to the emberAfImageBlockRequestCallback() to let the application decide what to do.

Field Documentation

EmberAfImageBlockRequestOptions EmberAfImageBlockRequestCallbackStruct::bitmask
uint8_t EmberAfImageBlockRequestCallbackStruct::clientEndpoint
const EmberAfOtaImageId * EmberAfImageBlockRequestCallbackStruct::id
uint8_t EmberAfImageBlockRequestCallbackStruct::maxDataSize
uint16_t EmberAfImageBlockRequestCallbackStruct::minBlockRequestPeriod
uint32_t EmberAfImageBlockRequestCallbackStruct::offset
EmberNodeId EmberAfImageBlockRequestCallbackStruct::source
EmberEUI64 EmberAfImageBlockRequestCallbackStruct::sourceEui
uint32_t EmberAfImageBlockRequestCallbackStruct::waitTimeSecondsResponse

The documentation for this struct was generated from the following file:
  • af-types.h