Zigbee Internet Client/Server remote cluster struct.

#include < af-types.h >

Data Fields

EmberAfClusterId clusterId
EmberAfProfileId profileId
uint16_t deviceId
uint8_t endpoint
EmberAfRemoteClusterType type

Zigbee Internet Client/Server remote cluster struct.

Field Documentation

EmberAfClusterId EmberAfRemoteClusterStruct::clusterId
uint16_t EmberAfRemoteClusterStruct::deviceId
uint8_t EmberAfRemoteClusterStruct::endpoint
EmberAfProfileId EmberAfRemoteClusterStruct::profileId
EmberAfRemoteClusterType EmberAfRemoteClusterStruct::type

The documentation for this struct was generated from the following file:
  • af-types.h