... to 1 in uartdrv_config.h. Hardware Flow Control UART hardware flow control uses two ... /RTS hardware support, the driver includes the GPIOINT driver to emulate a hardware implementation of ...
ProductMicrocontrollersResource TypeSoftware API documentation
Description Version API. Macros specifying the EMLIB and CMSIS version. ... Version number of targeted CMSIS package. ... A new version system for EMLIB will be provided in a later release.
ProductMicrocontrollersResource TypeSoftware API documentation
You are viewing documentation for version: 4.2 | Version History ... The control block references a ring buffer for each configured channel. ... You should avoid using it in production.
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... The hardware timer peripheral must be properly clocked from the application. ... All API functions can be called from within interrupt handlers.
Hardware block inside the SE used for generating random numbers. ... following example the device will erase OTP and become inoperable if 4 glitch signals is seen in a 1 minute time period.
Results 1-6 of 6 for zigbee/6.4/structEmberAfDeviceManagementCIN