// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... A pointer to this function is passed to sl_sleeptimer_start_timer().
RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered when a ... sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables
ProductMicrocontrollersResource TypeSoftware API documentation
// Platform//Version 5.0.1 //Security ... PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... A counter in the tamper filter is increased.
A template for this file, containing default values, is in the emdrv/config folder. ... [in] type Abort type – whether to abort only Tx, only Rx, or both.
ProductMicrocontrollersResource TypeSoftware API documentation