CLI commands various options.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
// Common include files:
#include "app/framework/util/common.h"
#include "app/framework/security/af-security.h"
#include "app/framework/util/af-main.h"
#include "app/framework/util/service-discovery.h"
#include "app/util/serial/command-interpreter2.h"
// *****************************************************************************
// Forward Declarations
// *****************************************************************************
void optionPrintRxCommand(void);
void optionRegisterCommand(void);
void optionDiscoverCommand(void);
void optionBindingTablePrintCommand(void);
void optionBindingTableClearCommand(void);
void optionEndDeviceBindCommand(void);
void optionApsRetryCommand(void);
void optionApsSecurityCommand(void);
void optionLinkCommand(void);
void optionBindingTableSetCommand(void);
void optionPrintRouteCommand(void);
void optionInstallCodeCommand(void);
void optionDiscoveryTargetCommand(void);
// *****************************************************************************
// Globals
// *****************************************************************************
#ifndef EMBER_AF_GENERATE_CLI
// option print-rx-msgs enable
// option print-rx-msgs disable
static EmberCommandEntry optionPrintRxCommands[] = {
  { "enable", optionPrintRxCommand, "" },
  { "disable", optionPrintRxCommand, "" },
  { NULL }
};
// option binding-table print
// option binding-table clear
// option binding-table set <index> <cluster> <local ep> <remote ep> <EUI>
static EmberCommandEntry optionBindingCommands[] = {
  { "print", optionBindingTablePrintCommand, "" },
  { "clear", optionBindingTableClearCommand, "" },
  { "set", optionBindingTableSetCommand, "uvuub" },
  { NULL }
};
// option security aps [off|on]
static EmberCommandEntry optionApsSecurityCommands[] = {
  { "on", optionApsSecurityCommand, "" },
  { "off", optionApsSecurityCommand, "" },
  { NULL }
};
static EmberCommandEntry apsRetryCommands[] = {
  { "on", optionApsRetryCommand, "" },
  { "off", optionApsRetryCommand, "" },
  { "def", optionApsRetryCommand, "" },
  { NULL }
};
static EmberCommandEntry optionSecurityCommands[] = {
  { "aps", NULL, (const char *)optionApsSecurityCommands },
  { NULL }
};
EmberCommandEntry emAfOptionCommands[] = {
  { "print-rx-msgs", NULL, (const char *)optionPrintRxCommands },
  { "register", optionRegisterCommand, "" },
  emberCommandEntryAction("disc", optionDiscoverCommand, "vv",
                          "Perform a match descriptor request"),
  emberCommandEntryAction("target", optionDiscoveryTargetCommand, "v",
                          "Set the target address of the CLI discovery"),
  { "binding-table", NULL, (const char *)optionBindingCommands },
  { "edb", optionEndDeviceBindCommand, "u" },
  { "security", NULL, (const char *)optionSecurityCommands },
  { "apsretry", NULL, (const char *)apsRetryCommands },
#ifdef DEBUG_PRINT_FOR_ROUTING_TABLE
  { "route", optionPrintRouteCommand, "" },
#endif
#if EMBER_KEY_TABLE_SIZE > 0
  { "link", optionLinkCommand, "ubb" },
  { "install-code", optionInstallCodeCommand, "ubb" },
#endif
  { NULL }
};
#endif // EMBER_AF_GENERATE_CLI
static EmberNodeId discoveryTargetNodeId = EMBER_RX_ON_WHEN_IDLE_BROADCAST_ADDRESS;
// *****************************************************************************
// Functions
// *****************************************************************************
void emAfCliServiceDiscoveryCallback(const EmberAfServiceDiscoveryResult* result)
{
#if defined(EMBER_AF_PRINT_ENABLE) && defined(EMBER_AF_PRINT_APP)
  if (!emberAfHaveDiscoveryResponseStatus(result->status)) {
    // Do nothing
  } else if (result->zdoRequestClusterId == MATCH_DESCRIPTORS_REQUEST) {
    const EmberAfEndpointList* epList = (const EmberAfEndpointList*)result->responseData;
    emberAfAppPrintln("Match %py from 0x%2X, ep %d",
                      "discover",
                      result->matchAddress,
                      epList->list[0]);
  } else if (result->zdoRequestClusterId == NETWORK_ADDRESS_REQUEST) {
    emberAfAppPrintln("NWK Address response: 0x%2X", result->matchAddress);
  } else if (result->zdoRequestClusterId == IEEE_ADDRESS_REQUEST) {
    const uint8_t* eui64ptr = (uint8_t*)(result->responseData);
    emberAfAppPrint("IEEE Address response: ");
    emberAfPrintBigEndianEui64(eui64ptr);
    emberAfAppPrintln("");
  } else {
    // MISRA requires ..else if.. to have a terminating else.
  }
  if (result->status != EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED) {
    emberAfAppPrintln("Service %py done.",
                      "discover");
  }
#endif //defined(EMBER_AF_PRINT_ENABLE) && defined(EMBER_AF_PRINT_APP)
}
// option print-rx-msgs [enable | disable]
void optionPrintRxCommand(void)
{
  if (emberCurrentCommand->name[0] == 'e') {
    emberAfPrintReceivedMessages = true;
  } else {
    emberAfPrintReceivedMessages = false;
  }
  emberAfAppPrintln("%pd print",
                    (emberAfPrintReceivedMessages
                     ? "enable"
                     : "disable"));
}
// option register
void optionRegisterCommand(void)
{
  emberAfRegistrationStartCallback();
}
void optionDiscoveryTargetCommand(void)
{
  discoveryTargetNodeId = (uint16_t)emberUnsignedCommandArgument(0);
}
// option disc <profileId> <clusterId>
void optionDiscoverCommand(void)
{
  EmberAfProfileId profileId = (uint16_t)emberUnsignedCommandArgument(0);
  EmberAfClusterId clusterId = (uint16_t)emberUnsignedCommandArgument(1);
  emberAfFindDevicesByProfileAndCluster(discoveryTargetNodeId,
                                        profileId,
                                        clusterId,
                                        EMBER_AF_SERVER_CLUSTER_DISCOVERY,
                                        emAfCliServiceDiscoveryCallback);
}
// option binding-table print
void optionBindingTablePrintCommand(void)
{
#if defined(EMBER_AF_PRINT_ENABLE) && defined(EMBER_AF_PRINT_APP)
  uint8_t i;
  EmberBindingTableEntry result;
  const char * typeStrings[] = {
    "EMPTY",
    "UNICA",
    "M2ONE",
    "MULTI",
    "?    ",
  };
  uint8_t bindings = 0;
  emberAfAppPrintln("#  type   nwk  loc   rem   clus   node   eui");
  for (i = 0; i < emberAfGetBindingTableSize(); i++) {
    EmberStatus status = emberGetBinding(i, &result);
    if (status == EMBER_SUCCESS) {
      if (result.type > EMBER_MULTICAST_BINDING) {
        result.type = 4;  // last entry in the string list above
      }
      if (result.type != EMBER_UNUSED_BINDING) {
        bindings++;
        emberAfAppPrint("%d: ", i);
        emberAfAppPrint("%p", typeStrings[result.type]);
        emberAfAppPrint("  %d    0x%x  0x%x  0x%2x 0x%2x ",
                        result.networkIndex,
                        result.local,
                        result.remote,
                        result.clusterId,
                        emberGetBindingRemoteNodeId(i));
        emberAfAppDebugExec(emberAfPrintBigEndianEui64(result.identifier));
        emberAfAppPrintln("");
      }
    } else {
      emberAfAppPrintln("0x%x: emberGetBinding Error: %x", status);
      emberAfAppFlush();
    }
    emberAfAppFlush();
  }
  emberAfAppPrintln("%d of %d bindings used",
                    bindings,
                    emberAfGetBindingTableSize());
#endif //defined(EMBER_AF_PRINT_ENABLE) && defined(EMBER_AF_PRINT_APP)
}
// option binding-table clear
void optionBindingTableClearCommand(void)
{
  emberClearBindingTable();
}
// option edb <endpoint>
void optionEndDeviceBindCommand(void)
{
  uint8_t endpoint = (uint8_t)emberUnsignedCommandArgument(0);
  emberAfSendEndDeviceBind(endpoint);
}
void optionApsRetryCommand(void)
{
  if ( emberCurrentCommand->name[1] == 'e' ) {
    emberAfSetRetryOverride(EMBER_AF_RETRY_OVERRIDE_NONE);
  } else if ( emberCurrentCommand->name[1] == 'n' ) {
    emberAfSetRetryOverride(EMBER_AF_RETRY_OVERRIDE_SET);
  } else if ( emberCurrentCommand->name[1] == 'f' ) {
    emberAfSetRetryOverride(EMBER_AF_RETRY_OVERRIDE_UNSET);
  } else {
    // MISRA requires ..else if.. to have a terminating else.
  }
}
// option security aps <off | on>
void optionApsSecurityCommand(void)
{
  emAfTestApsSecurityOverride = (emberCurrentCommand->name[1] == 'f'
                                 ? APS_TEST_SECURITY_DISABLED
                                 : APS_TEST_SECURITY_ENABLED);
}
// option link <index> <eui64 in big endian format> <key in big endian format>
void optionLinkCommand(void)
{
  EmberEUI64 partnerEUI64;
  EmberKeyData newKey;
  EmberStatus status;
  //uint8_t i;
  uint8_t index = (uint8_t)emberUnsignedCommandArgument(0);
  emberCopyBigEndianEui64Argument(1, partnerEUI64);
  emberCopyKeyArgument(2, &newKey);
  status = emberSetKeyTableEntry(index,
                                 partnerEUI64,
                                 true,
                                 &newKey);
  UNUSED_VAR(status);
  emberAfAppDebugExec(emAfPrintStatus("add link key", status));
  emberAfAppPrintln("");
  emberAfCoreFlush();
}
// option install-code <index> <eui64> <install code>
void optionInstallCodeCommand(void)
{
#if (defined(EMBER_AF_HAS_SECURITY_PROFILE_SE_TEST) \
  || defined(EMBER_AF_HAS_SECURITY_PROFILE_SE_FULL) \
  || defined (EMBER_AF_HAS_SECURITY_PROFILE_Z3))
  EmberEUI64 eui64;
  EmberKeyData key;
  EmberStatus status;
  uint8_t code[16 + 2]; // 6, 8, 12, or 16 bytes plus two-byte CRC
  uint8_t length;
  length = emberCopyStringArgument(2, code, sizeof(code), false);
  // Convert the install code to a key.
  status = emAfInstallCodeToKey(code, length, &key);
  if (EMBER_SUCCESS != status) {
    if (EMBER_SECURITY_DATA_INVALID == status) {
      emberAfAppPrintln("ERR: Calculated CRC does not match");
    } else if (EMBER_BAD_ARGUMENT == status) {
      emberAfAppPrintln("ERR: Install Code must be 8, 10, 14, or 18 bytes in "
                        "length");
    } else {
      emberAfAppPrintln("ERR: AES-MMO hash failed: 0x%x", status);
    }
    return;
  }
  emberCopyBigEndianEui64Argument(1, eui64);
  #ifndef EMBER_AF_HAS_SECURITY_PROFILE_Z3
  // Add the key to the link key table.
  status = emberSetKeyTableEntry((uint8_t)emberUnsignedCommandArgument(0),     // index
                                 eui64,
                                 true,                                       // link key
                                 &key);
  emberAfAppDebugExec(emAfPrintStatus("add link key", status));
  emberAfAppPrintln("");
  emberAfAppFlush();
  #else
  // Add the key to the transient key table.
  // This will be used while the DUT joins.
  if (EMBER_SUCCESS == status) {
    status = emberAddTransientLinkKey(eui64, &key);
    emberAfAppDebugExec(emAfPrintStatus("Set joining link key", status));
    emberAfAppPrintln("");
    emberAfAppFlush();
  }
  #endif
#else
  emberAfAppPrintln("This command only supports the Z3 or SE application profile.");
#endif
}
// option binding-table set <index> <cluster> <local ep> <remote ep> <EUI>
void optionBindingTableSetCommand(void)
{
  EmberBindingTableEntry entry;
  uint8_t index = (uint8_t)emberUnsignedCommandArgument(0);
  uint8_t endpoint = (uint8_t)emberUnsignedCommandArgument(2);
  EmberStatus status = emberAfPushEndpointNetworkIndex(endpoint);
  if (status == EMBER_SUCCESS) {
    entry.type = EMBER_UNICAST_BINDING;
    entry.clusterId = (EmberAfClusterId)emberUnsignedCommandArgument(1);
    entry.local = endpoint;
    entry.remote = (uint8_t)emberUnsignedCommandArgument(3);
    emberCopyBigEndianEui64Argument(4, entry.identifier);
    entry.networkIndex = emberGetCurrentNetwork();
    status = emberSetBinding(index, &entry);
    (void) emberAfPopNetworkIndex();
  }
  emberAfAppPrintln("set bind %d: 0x%x", index, status);
}
#ifdef DEBUG_PRINT_FOR_ROUTING_TABLE
void optionPrintRouteCommand(void)
{
  const char * statusText[] = {
    "active",
    "discov",
    "??    ",
    "unused",
  };
  const char * concentratorText[] = {
    "- ",
    "lo",
    "hi",
  };
  const char * routeRecordStateText[] = {
    "none",
    "sent",
    "need",
  };
  uint8_t i;
  emberAfAppPrintln("Routing Table\n-----------------");
  for (i = 0; i < EMBER_ROUTE_TABLE_SIZE; i++) {
    EmberRouteTableEntry entry;
    if (emberGetRouteTableEntry(i, &entry) == EMBER_SUCCESS) {
      emberAfAppPrintln("%d: dest:0x%2X next:0x%2X status:%p age:%d conc:%p rr-state:%p",
                        i,
                        entry.destination,
                        entry.nextHop,
                        statusText[entry.status],
                        entry.age,
                        concentratorText[entry.concentratorType],
                        routeRecordStateText[entry.routeRecordState]);
    }
    emberAfAppFlush();
  }
}
#endif //  DEBUG_PRINT_FOR_ROUTING_TABLE
Variables#
EmberCommandEntry
EmberCommandEntry
EmberCommandEntry
EmberCommandEntry
EmberCommandEntry
EmberCommandEntry
EmberNodeId
Functions#
void
optionPrintRxCommand(void)
void
optionRegisterCommand(void)
void
optionDiscoverCommand(void)
void
void
void
void
optionApsRetryCommand(void)
void
optionApsSecurityCommand(void)
void
optionLinkCommand(void)
void
void
optionPrintRouteCommand(void)
void
optionInstallCodeCommand(void)
void
void
emAfCliServiceDiscoveryCallback(const EmberAfServiceDiscoveryResult *result)
Variable Documentation#
Function Documentation#
optionPrintRxCommand#
void optionPrintRxCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionRegisterCommand#
void optionRegisterCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionDiscoverCommand#
void optionDiscoverCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionBindingTablePrintCommand#
void optionBindingTablePrintCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionBindingTableClearCommand#
void optionBindingTableClearCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionEndDeviceBindCommand#
void optionEndDeviceBindCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionApsRetryCommand#
void optionApsRetryCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionApsSecurityCommand#
void optionApsSecurityCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionLinkCommand#
void optionLinkCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionBindingTableSetCommand#
void optionBindingTableSetCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
References EmberBindingTableEntry::clusterId , EMBER_SUCCESS , EMBER_UNICAST_BINDING , emberAfPopNetworkIndex , emberAfPushEndpointNetworkIndex , EmberBindingTableEntry::identifier , EmberBindingTableEntry::local , EmberBindingTableEntry::networkIndex , EmberBindingTableEntry::remote ,  and EmberBindingTableEntry::type
optionPrintRouteCommand#
void optionPrintRouteCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionInstallCodeCommand#
void optionInstallCodeCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
optionDiscoveryTargetCommand#
void optionDiscoveryTargetCommand (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
emAfCliServiceDiscoveryCallback#
void emAfCliServiceDiscoveryCallback (const EmberAfServiceDiscoveryResult * result)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| const EmberAfServiceDiscoveryResult * | N/A | result | 
References EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED , emberAfHaveDiscoveryResponseStatus , IEEE_ADDRESS_REQUEST , EmberAfEndpointList::list , MATCH_DESCRIPTORS_REQUEST , EmberAfServiceDiscoveryResult::matchAddress , NETWORK_ADDRESS_REQUEST , EmberAfServiceDiscoveryResult::responseData , EmberAfServiceDiscoveryResult::status ,  and EmberAfServiceDiscoveryResult::zdoRequestClusterId
Referenced by zdoIeeeAddressRequestCommand ,  and zdoNwkAddressRequestCommand