CLI commands for sending ZDO messages.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
// common include file
#include "app/framework/util/common.h"
#include "app/framework/util/af-main.h"

#include "app/util/serial/command-interpreter2.h"

#include "app/util/zigbee-framework/zigbee-device-common.h"

#if defined(EZSP_HOST)
  #include "app/util/zigbee-framework/zigbee-device-host.h"
#else // SOC
  #include "app/util/zigbee-framework/zigbee-device-library.h"
#endif

#include "app/framework/cli/option-cli.h"

//------------------------------------------------------------------------------
// Forward declarations

void zdoNwkAddressRequestCommand(void);
void zdoIeeeAddressRequestCommand(void);
void zdoSimpleCommand(void);
void zdoNodeCommand(void);
void zdoMatchCommand(void);
void zdoBindCommand(void);
void zdoAddClusterCommand(void);
void zdoClearClusterCommand(void);
void zdoNetworkUpdateChannelCommand(void);
void zdoNetworkUpdateScanCommand(void);
void zdoNetworkUpdateSetCommand(void);
void zdoActiveEpCommand(void);
void zdoMgmtLqiCommand(void);
void zdoMgmtBindCommand(void);

EmberStatus matchDescriptorsRequest(EmberNodeId target,
                                    uint16_t profile,
                                    uint8_t inCount,
                                    uint8_t outCount,
                                    uint16_t *inClusters,
                                    uint16_t *outClusters,
                                    EmberApsOption options);

//------------------------------------------------------------------------------
// Globals

#ifndef EMBER_AF_GENERATE_CLI

static const char * addClusterArguments[] = {
  "ZCL Cluster to add.",
  NULL,
};

static EmberCommandEntry zdoClusterCommands[] = {
  emberCommandEntryActionWithDetails("add",
                                     zdoAddClusterCommand,
                                     "v",
                                     "Add a ZCL cluster to the CLI's list.",
                                     addClusterArguments),
  emberCommandEntryAction("clear",
                          zdoClearClusterCommand,
                          "",
                          "Remove all ZCL clusters from the CLI's list"),
  emberCommandEntryTerminator(),
};

static const char * channelChangeArguments[] = {
  "Channel to change to.",
  NULL,
};

static const char * channelScanArguments[] = {
  "Target Node ID",
  "Scan Duration",  // see stack/include/zigbee-device-stack.h for enumeration
  "Scan count",
  NULL,
};

static const char * channelManagerArguments[] = {
  "NWK manager node ID",
  "Channel mask",
  NULL,
};

static EmberCommandEntry zdoNetworkUpdateCommands[] = {
  emberCommandEntryActionWithDetails("chan",
                                     zdoNetworkUpdateChannelCommand,
                                     "uu*",
                                     "Send a channel change command.",
                                     channelChangeArguments),
  emberCommandEntryActionWithDetails("scan",
                                     zdoNetworkUpdateScanCommand,
                                     "vuvw*",
                                     "Tell a remote node to perform a channel scan",
                                     channelScanArguments),
  emberCommandEntryActionWithDetails("set",
                                     zdoNetworkUpdateSetCommand,
                                     "vw",
                                     "Broadcast a new NWK manager Node ID and channel list.",
                                     channelManagerArguments),
  emberCommandEntryTerminator(),
};

static const char * simpleDescriptorArguments[] = {
  "The target node ID",
  "The target endpoint",
  NULL,
};

static const char * zdoMatchCommandArguments[] = {
  "Target node ID",
  "Profile ID",
  NULL,
};

static const char * zdoBindCommandArguments[] = {
  "Dest node ID",
  "local EP",
  "remote EP",
  "cluster ID",
  "THEIR EUI",
  "binding dest EUI",
  NULL,
};

static const char * zdoMgmtLqiCommandArguments[] = {
  "Dest node ID",
  "start index",
  NULL,
};

EmberCommandEntry zdoCommands[] = {
  emberCommandEntryAction("active",
                          zdoActiveEpCommand,
                          "v",
                          "Send an Active EP request"),
  emberCommandEntryActionWithDetails("bind",
                                     zdoBindCommand,
                                     "vuuvbb",
                                     "Sends bind request",
                                     zdoBindCommandArguments),
  emberCommandEntryAction("ieee",
                          zdoIeeeAddressRequestCommand,
                          "v",
                          "Unicast an IEEE address request to the specified node."),
  emberCommandEntrySubMenu("in-cl-list",
                           zdoClusterCommands,
                           "Modify input cluster list"),
  emberCommandEntryActionWithDetails("match",
                                     zdoMatchCommand,
                                     "vv",
                                     "Send a match descriptor request using CLI configured in/out clusters.",
                                     zdoMatchCommandArguments),
  emberCommandEntryActionWithDetails("mgmt-lqi",
                                     zdoMgmtLqiCommand,
                                     "vu",
                                     "Send a MGMT-LQI (LQI Table) request to target",
                                     zdoMgmtLqiCommandArguments),
  emberCommandEntryActionWithDetails("mgmt-bind",
                                     zdoMgmtBindCommand,
                                     "vu",
                                     "Send a MGMT-Bind (Binding Table) request to target",
                                     zdoMgmtLqiCommandArguments), // Binding Table Req uses same args as LQI Table Req
  emberCommandEntryAction("node",
                          zdoNodeCommand,
                          "v",
                          "Send a node descriptor request to target"),
  emberCommandEntryAction("nwk",
                          zdoNwkAddressRequestCommand,
                          "b",
                          "Broadcast a NWK address request for the specified IEEE."),
  emberCommandEntrySubMenu("nwk-upd",
                           zdoNetworkUpdateCommands,
                           "Frequency Agility Commands"),
  emberCommandEntrySubMenu("out-cl-list",
                           zdoClusterCommands,
                           "Modify output cluster list"),
  emberCommandEntryActionWithDetails("simple",
                                     zdoSimpleCommand,
                                     "vu",
                                     "Send a Simple Descriptor request to the target node and endpoint",
                                     simpleDescriptorArguments),
  emberCommandEntryTerminator(),
};

#endif // EMBER_AF_GENERATE_CLI

#define MAX_CLUSTERS_CAN_MATCH 5
uint16_t emAfCliZdoInClusters[MAX_CLUSTERS_CAN_MATCH];
uint16_t emAfCliZdoOutClusters[MAX_CLUSTERS_CAN_MATCH];
uint8_t emAfCliInClCount = 0;
uint8_t emAfCliOutClCount = 0;

//------------------------------------------------------------------------------

// *****************************************
// zdoCommand
//
// zdo nwk <eui64:big-endian>
// zdo ieee <node-id>
// zdo simple <dest> <target ep>
// zdo node <dest>
// zdo match  <dest> <profile>
// zdo bind   <dest> <local ep> <remote ep> <cluster> <THEIR eui> <dest eui>
// zdo in-cl-list add <cluster IDs>
// zdo in-cl-list clear
// zdo out-cl-list add <clusters IDs>
// zdo out-cl-list clear
// zdo nwk-upd chan  <channel>
// zdo nwk-upd set   <nwk mgr id>  <chan mask>
// zdo nwk-upd scan  <target> <duration> <count>
// zdo active <target>
// *****************************************

void zdoNwkAddressRequestCommand(void)
{
  EmberEUI64 eui64;
  emberCopyBigEndianEui64Argument(0, eui64);
  emberAfFindNodeId(eui64,
                    emAfCliServiceDiscoveryCallback);
}

void zdoIeeeAddressRequestCommand(void)
{
  EmberNodeId id = (EmberNodeId)emberUnsignedCommandArgument(0);
  emberAfFindIeeeAddress(id,
                         emAfCliServiceDiscoveryCallback);
}

void zdoSimpleCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  uint8_t targetEndpoint = (uint8_t)emberUnsignedCommandArgument(1);
  EmberStatus status = emberSimpleDescriptorRequest(target,
                                                    targetEndpoint,
                                                    EMBER_AF_DEFAULT_APS_OPTIONS);
  emberAfAppPrintln("ZDO simple desc req %x", status);
}

void zdoNodeCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  EmberStatus status = emberNodeDescriptorRequest(target,
                                                  EMBER_AF_DEFAULT_APS_OPTIONS);
  emberAfAppPrintln("ZDO node desc req %x", status);
}

void zdoMatchCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  uint16_t profile = (uint16_t)emberUnsignedCommandArgument(1);
  EmberStatus status = matchDescriptorsRequest(target,
                                               profile,
                                               emAfCliInClCount,
                                               emAfCliOutClCount,
                                               emAfCliZdoInClusters,
                                               emAfCliZdoOutClusters,
                                               EMBER_AF_DEFAULT_APS_OPTIONS);
  emberAfAppPrintln("ZDO match desc req %x", status);
}

static EmberStatus copyOrLookupEui64(uint8_t argumentNumber,
                                     EmberNodeId nodeId,
                                     EmberEUI64 returnEui64)
{
  EmberStatus status = EMBER_SUCCESS;
  if (0 == emberCopyBigEndianEui64Argument(argumentNumber, returnEui64)) {
    status = emberLookupEui64ByNodeId(nodeId, returnEui64);
    if (status != EMBER_SUCCESS) {
      emberAfAppPrintln("Error:  EUI64 argument is empty and lookup by node ID failed.");
    }
  }
  return status;
}

// For simple bind requests, just put {} as the last argument
//   zdo bind <dest> <local ep> <remote ep> <cluster> <THEIR EUI> {}
//
// More complex requests, you can actually specify the dest EUI64 of,
// the binding, which is NOT the same as the EUI64 of the destination
// of the device receiving the binding.  This allows for a user
// to set multiple bindings on the destination for different devices.
//   zdo bind <dest> <local ep> <remote ep> <cluster> <THEIR EUI> <dest EUI64>
void zdoBindCommand(void)
{
  EmberStatus status;
  EmberEUI64 sourceEui, destEui;  // names relative to binding sent over-the-air
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  uint8_t sourceEndpoint = (uint8_t)emberUnsignedCommandArgument(1);
  uint8_t destinationEndpoint = (uint8_t)emberUnsignedCommandArgument(2);
  uint16_t clusterId = (uint16_t)emberUnsignedCommandArgument(3);

  // NOTE:  The source/dest EUI is relative to the context.
  // In the case of the syntax of the CLI, we take "THEIR EUI64" to mean
  // the recipient of the binding request message.  However, when sending
  // the bind request that EUI64 used by the ZDO command is
  // actually the source for the binding because we are telling the remote
  // device (the destination) to create a binding with a source of itself.
  // And the destination for that binding will be this local device.
  // This is also not to be confused with the (short) destination of the ZDO
  // request itself.
  if (EMBER_SUCCESS != copyOrLookupEui64(4, target, sourceEui)) {
    return;
  }

  // If the last argument is empty, assume an EUI64 of the local device.
  // This allows for the simple case.  If an EUI64 is specified, it will
  // be used instead of the local EUI.  This is used for setting
  // multiple bindings on the same remote device.
  if (0 == emberCopyBigEndianEui64Argument(5, destEui)) {
    emberAfAppPrintln("Using my local EUI64 for dest EUI64 in binding");
    emberAfGetEui64(destEui);
  }

  status = emberBindRequest(target,           // who gets the bind req
                            sourceEui,       // source eui IN the binding
                            sourceEndpoint,
                            clusterId,
                            UNICAST_BINDING, // binding type
                            destEui,         // destination eui IN the binding
                            0,               // groupId for new binding
                            destinationEndpoint,
                            EMBER_AF_DEFAULT_APS_OPTIONS);
  UNUSED_VAR(status);
  emberAfAppPrintln("ZDO bind req %x", status);
}

void zdoAddClusterCommand(void)
{
  uint16_t *clusters;
  uint8_t *clCount;
  if (emberStringCommandArgument(-2, NULL)[0]  == 'i') {
    clusters = emAfCliZdoInClusters;
    clCount = &emAfCliInClCount;
  } else {
    clusters = emAfCliZdoOutClusters;
    clCount = &emAfCliOutClCount;
  }

  if (*clCount < MAX_CLUSTERS_CAN_MATCH) {
    clusters[*clCount] = (uint16_t)emberUnsignedCommandArgument(0);
    (*clCount)++;
  } else {
    emberAfAppPrintln("cluster limit reached");
  }
}

void zdoClearClusterCommand(void)
{
  if (emberStringCommandArgument(-2, NULL)[0]  == 'i') {
    emAfCliInClCount = 0;
  } else {
    emAfCliOutClCount = 0;
  }
}

void zdoNetworkUpdateChannelCommand(void)
{
  uint8_t channel = (uint8_t)emberUnsignedCommandArgument(0);
  uint8_t page = 0;
  EmberStatus status;

  if (emberCommandArgumentCount() > 1) {
    page = (uint8_t)emberUnsignedCommandArgument(1);
  } else {
    // page and channels are encoded in 8 bits as page 7..5 bits
    // channel 4...0 bits
    // 3rd and 4th bits are always 1's
    page = (uint8_t)(channel >> 5) | 0x18;
    channel = channel & 0x1F;
  }

  if (EMBER_SUCCESS != emAfValidateChannelPages(page, channel)) {
    emberAfAppPrintln("invalid page: %d or channel: %d", page, channel);
  } else {
    if (page == EMBER_NO_CHANNEL_PAGE_IN_USE) {
      // Request for 2.4Ghz network if page is zero
      status = emberChannelChangeRequest(channel);
    } else {
      // 31..27 bits for page and 26..0 for channels
      uint32_t pageChannelBitMask = (page << 27 | BIT32(channel));
      status = emberEnergyScanRequest(EMBER_SLEEPY_BROADCAST_ADDRESS,
                                      pageChannelBitMask,
                                      0xFE,
                                      0);
    }
    emberAfAppPrintln("Change channel status: 0x%x", status);
  }
}

void zdoNetworkUpdateScanCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  uint8_t scanDuration = (uint8_t)emberUnsignedCommandArgument(1);
  uint16_t scanCount = (uint16_t)emberUnsignedCommandArgument(2);
  uint32_t scanChannelsMask = EMBER_ALL_802_15_4_CHANNELS_MASK;
  if (scanDuration > 5 || scanCount == 0 || scanCount > 8) {
    emberAfAppPrintln("duration must be in range 0 - 5");
    emberAfAppPrintln("count must be in range 1 - 8");
  } else {
    if (emberCommandArgumentCount() > 3) {
      scanChannelsMask = emberUnsignedCommandArgument(3);
    }

    EmberStatus status = emberEnergyScanRequest(target,
                                                scanChannelsMask,
                                                scanDuration,
                                                scanCount);
    emberAfAppPrint("scan status 0x%x", status);
  }
}

void zdoNetworkUpdateSetCommand(void)
{
  EmberNodeId networkManager = (EmberNodeId)emberUnsignedCommandArgument(0);
  uint32_t activeChannels = emberUnsignedCommandArgument(1);
  EmberStatus status = emberSetNetworkManagerRequest(networkManager,
                                                     activeChannels);
  emberAfAppPrint("network update set status 0x%x", status);
}

void zdoActiveEpCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  EmberStatus status = emberActiveEndpointsRequest(target,
                                                   EMBER_APS_OPTION_RETRY);
  emberAfAppPrint("Active EP request status: 0x%X",
                  status);
}

void zdoMgmtLqiCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  uint8_t index = emberUnsignedCommandArgument(1);
  EmberStatus status = emberLqiTableRequest(target,
                                            index,
                                            EMBER_APS_OPTION_RETRY);
  emberAfAppPrint("LQI Table request: 0x%X", status);
}

void zdoMgmtBindCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  uint8_t index = emberUnsignedCommandArgument(1);
  EmberStatus status = emberBindingTableRequest(target,
                                                index,
                                                EMBER_APS_OPTION_RETRY);
  emberAfAppPrint("Binding Table request: 0x%X", status);
}

void zdoLeaveRequestCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  // CCB 2047
  // - CCB makes the first step to depracate the 'leave and remove children' functionality.
  // - We were proactive here and deprecated it right away.
  // bool removeChildren = (bool)emberUnsignedCommandArgument(1);
  bool rejoin = (bool)emberUnsignedCommandArgument(2);
  EmberEUI64 nullEui64 = { 0, 0, 0, 0, 0, 0, 0, 0 };
  EmberStatus status;

  uint8_t options = 0;
  if (rejoin) {
    options |= EMBER_ZIGBEE_LEAVE_AND_REJOIN;
  }

  status = emberLeaveRequest(target,
                             nullEui64,
                             options,
                             EMBER_APS_OPTION_RETRY);

  emberAfAppPrintln("Leave %p0x%X", "Request: ", status);
}

void zdoPowerDescriptorRequestCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  EmberStatus status = emberPowerDescriptorRequest(target,
                                                   EMBER_APS_OPTION_RETRY);
  emberAfAppPrintln("Power Descriptor %p0x%X", "Request: ", status);
}

void zdoEndDeviceBindRequestCommand(void)
{
  uint8_t endpoint = (uint8_t)emberUnsignedCommandArgument(0);
  EmberStatus status = emberAfSendEndDeviceBind(endpoint);
  emberAfAppPrintln("End Device Bind %p0x%X", "Request: ", status);
}

static void unbindRequest(bool isGroupAddress,
                          void* destination,
                          uint8_t destinationEndpoint)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  uint8_t sourceEndpoint = (uint8_t)emberUnsignedCommandArgument(2);
  EmberAfClusterId clusterId = (EmberAfClusterId)emberUnsignedCommandArgument(3);
  EmberEUI64 sourceEui64;
  EmberEUI64 destinationEui64;
  EmberStatus status;
  EmberNodeId groupAddress = EMBER_NULL_NODE_ID;

  if (EMBER_SUCCESS != copyOrLookupEui64(1, target, sourceEui64)) {
    return;
  }

  if (isGroupAddress) {
    groupAddress = *((EmberNodeId*)destination);
  } else {
    groupAddress = 0;
    MEMMOVE(destinationEui64, destination, EUI64_SIZE);
  }

  status = emberUnbindRequest(target,
                              sourceEui64,
                              sourceEndpoint,
                              clusterId,
                              (isGroupAddress
                               ? MULTICAST_BINDING
                               : UNICAST_BINDING),
                              destinationEui64,
                              groupAddress,
                              destinationEndpoint,
                              EMBER_APS_OPTION_RETRY);
  UNUSED_VAR(status);
  emberAfAppPrintln("Unbind %p %p0x%X",
                    (isGroupAddress
                     ? "Group"
                     : "Unicast"),
                    "Request: ",
                    status);
}

void zdoUnbindGroupCommand(void)
{
  EmberNodeId groupAddress = (EmberNodeId)emberUnsignedCommandArgument(4);
  unbindRequest(true,  // group addressed binding?
                &groupAddress,
                0);   // destination endpoint (unused)
}

void zdoUnbindUnicastCommand(void)
{
  EmberEUI64 destinationEui64;
  uint8_t destinationEndpoint = (uint8_t)emberUnsignedCommandArgument(5);

  // If the destination EUI64 of the binding (not the destination of the
  // actual message) is empty, use our local EUI64.
  if (0 == emberCopyBigEndianEui64Argument(4, destinationEui64)) {
    emberAfAppPrintln("Using my local EUI64 for dest EUI64 in unbinding");
    emberAfGetEui64(destinationEui64);
  }

  unbindRequest(false,   // group addressed binding?
                destinationEui64,
                destinationEndpoint);
}

void zdoRouteRequestCommand(void)
{
  EmberNodeId target = (EmberNodeId)emberUnsignedCommandArgument(0);
  uint8_t index = (uint8_t)emberUnsignedCommandArgument(1);
  EmberStatus status = emberRoutingTableRequest(target,
                                                index,
                                                EMBER_APS_OPTION_RETRY);
  emberAfAppPrintln("Route Table %p0x%X", "Request: ", status);
}

//------------------------------------------------------------------------------
// Platform specific code

#if defined(EZSP_HOST)
EmberStatus matchDescriptorsRequest(EmberNodeId target,
                                    uint16_t profile,
                                    uint8_t inCount,
                                    uint8_t outCount,
                                    uint16_t *inClusters,
                                    uint16_t *outClusters,
                                    EmberApsOption options)
{
  return ezspMatchDescriptorsRequest(target,
                                     profile,
                                     inCount,
                                     outCount,
                                     inClusters,
                                     outClusters,
                                     options);
}

#else

// Copy the list of uint16_t input and output cluster lists into
// message buffers.
EmberStatus matchDescriptorsRequest(EmberNodeId target,
                                    uint16_t profile,
                                    uint8_t inCount,
                                    uint8_t outCount,
                                    uint16_t *inClusters,
                                    uint16_t *outClusters,
                                    EmberApsOption options)
{
  uint8_t i;
  uint8_t output;
  EmberMessageBuffer inClusterBuffer = EMBER_NULL_MESSAGE_BUFFER;
  EmberMessageBuffer outClusterBuffer = EMBER_NULL_MESSAGE_BUFFER;
  EmberStatus status = EMBER_NO_BUFFERS;
  for (output = 0; output < 2; output++) {
    EmberMessageBuffer* bufferPtr;
    uint8_t count;
    uint16_t* list;
    if (output != 0U) {
      count = outCount;
      list = outClusters;
      bufferPtr = &outClusterBuffer;
    } else {  // input
      count = inCount;
      list = inClusters;
      bufferPtr = &inClusterBuffer;
    }
    if (count == 0) {
      continue;
    }

    *bufferPtr = emberAllocateStackBuffer();
    if (*bufferPtr == EMBER_NULL_MESSAGE_BUFFER) {
      goto cleanup;
    }

    for (i = 0; i < count; i++) {
      uint8_t cluster[2];
      cluster[0] = LOW_BYTE(list[i]);
      cluster[1] = HIGH_BYTE(list[i]);
      status = emberAppendToLinkedBuffers(*bufferPtr,
                                          cluster,
                                          2);
      if (EMBER_SUCCESS != status) {
        goto cleanup;
      }
    }
  }
  status = emberMatchDescriptorsRequest(target,
                                        profile,
                                        inClusterBuffer,
                                        outClusterBuffer,
                                        options);
  cleanup:
  if (inClusterBuffer != EMBER_NULL_MESSAGE_BUFFER) {
    emberReleaseMessageBuffer(inClusterBuffer);
  }
  if (outClusterBuffer != EMBER_NULL_MESSAGE_BUFFER) {
    emberReleaseMessageBuffer(outClusterBuffer);
  }
  return status;
}

#endif // !defined(EZSP_HOST)

Functions#

void
void
void
matchDescriptorsRequest(EmberNodeId target, uint16_t profile, uint8_t inCount, uint8_t outCount, uint16_t *inClusters, uint16_t *outClusters, EmberApsOption options)
copyOrLookupEui64(uint8_t argumentNumber, EmberNodeId nodeId, EmberEUI64 returnEui64)
void
unbindRequest(bool isGroupAddress, void *destination, uint8_t destinationEndpoint)

Macro Definition Documentation#

MAX_CLUSTERS_CAN_MATCH#

#define MAX_CLUSTERS_CAN_MATCH
Value:
5

Variable Documentation#

addClusterArguments#

const char* addClusterArguments[]

zdoClusterCommands#

EmberCommandEntry zdoClusterCommands[]

channelChangeArguments#

const char* channelChangeArguments[]

channelScanArguments#

const char* channelScanArguments[]

channelManagerArguments#

const char* channelManagerArguments[]

zdoNetworkUpdateCommands#

EmberCommandEntry zdoNetworkUpdateCommands[]

simpleDescriptorArguments#

const char* simpleDescriptorArguments[]

zdoMatchCommandArguments#

const char* zdoMatchCommandArguments[]

zdoBindCommandArguments#

const char* zdoBindCommandArguments[]

zdoMgmtLqiCommandArguments#

const char* zdoMgmtLqiCommandArguments[]

zdoCommands#

EmberCommandEntry zdoCommands[]

emAfCliZdoInClusters#

uint16_t emAfCliZdoInClusters[MAX_CLUSTERS_CAN_MATCH]

emAfCliZdoOutClusters#

uint16_t emAfCliZdoOutClusters[MAX_CLUSTERS_CAN_MATCH]

emAfCliInClCount#

uint8_t emAfCliInClCount

emAfCliOutClCount#

uint8_t emAfCliOutClCount

Function Documentation#

zdoNwkAddressRequestCommand#

void zdoNwkAddressRequestCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoIeeeAddressRequestCommand#

void zdoIeeeAddressRequestCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoSimpleCommand#

void zdoSimpleCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoNodeCommand#

void zdoNodeCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoMatchCommand#

void zdoMatchCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoBindCommand#

void zdoBindCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoAddClusterCommand#

void zdoAddClusterCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoClearClusterCommand#

void zdoClearClusterCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoNetworkUpdateChannelCommand#

void zdoNetworkUpdateChannelCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoNetworkUpdateScanCommand#

void zdoNetworkUpdateScanCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoNetworkUpdateSetCommand#

void zdoNetworkUpdateSetCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoActiveEpCommand#

void zdoActiveEpCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoMgmtLqiCommand#

void zdoMgmtLqiCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoMgmtBindCommand#

void zdoMgmtBindCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

matchDescriptorsRequest#

EmberStatus matchDescriptorsRequest (EmberNodeId target, uint16_t profile, uint8_t inCount, uint8_t outCount, uint16_t * inClusters, uint16_t * outClusters, EmberApsOption options)
Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/Atarget
uint16_tN/Aprofile
uint8_tN/AinCount
uint8_tN/AoutCount
uint16_t *N/AinClusters
uint16_t *N/AoutClusters
EmberApsOptionN/Aoptions

copyOrLookupEui64#

static EmberStatus copyOrLookupEui64 (uint8_t argumentNumber, EmberNodeId nodeId, EmberEUI64 returnEui64)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/AargumentNumber
EmberNodeIdN/AnodeId
EmberEUI64N/AreturnEui64

zdoLeaveRequestCommand#

void zdoLeaveRequestCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoPowerDescriptorRequestCommand#

void zdoPowerDescriptorRequestCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoEndDeviceBindRequestCommand#

void zdoEndDeviceBindRequestCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

unbindRequest#

static void unbindRequest (bool isGroupAddress, void * destination, uint8_t destinationEndpoint)
Parameters
TypeDirectionArgument NameDescription
boolN/AisGroupAddress
void *N/Adestination
uint8_tN/AdestinationEndpoint

zdoUnbindGroupCommand#

void zdoUnbindGroupCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoUnbindUnicastCommand#

void zdoUnbindUnicastCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

zdoRouteRequestCommand#

void zdoRouteRequestCommand (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A