Debugging Utilities#

EmberZNet debugging utilities.

See ember-debug.h for source code.

Functions#

void
emberDebugAssert(const char *filename, int linenumber)

Prints the filename and line number to the debug serial port.

void
emberDebugMemoryDump(uint8_t *start, uint8_t *end)

Prints the contents of RAM to the debug serial port.

void
emberDebugBinaryPrintf(const char *formatString,...)

Prints binary data to the debug channel.

void
emDebugSendVuartMessage(uint8_t *buff, uint8_t len)

Sends VUART data out the debug channel.

void
emberDebugError(EmberStatus code)

Prints an EmberStatus return code to the serial port.

bool

Turns off all debug output.

void

Restores the state of the debug output.

void
emberDebugPrintf(const char *formatString,...)

Prints text debug messages.

Macros#

#define
#define
#define
#define

This function is obsolete and no longer required to initialize the debug system.

Function Documentation#

emberDebugAssert#

void emberDebugAssert (const char * filename, int linenumber)

Prints the filename and line number to the debug serial port.

Parameters
TypeDirectionArgument NameDescription
const char *N/Afilename

The name of the file where the assert occurred.

intN/Alinenumber

The line number in the file where the assert occurred.


emberDebugMemoryDump#

void emberDebugMemoryDump (uint8_t * start, uint8_t * end)

Prints the contents of RAM to the debug serial port.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/Astart

The start address of the block of RAM to dump.

uint8_t *N/Aend

The end address of the block of RAM to dump (address of the last byte).


emberDebugBinaryPrintf#

void emberDebugBinaryPrintf (const char * formatString, ... )

Prints binary data to the debug channel.

Parameters
TypeDirectionArgument NameDescription
const char *N/AformatString

A string of conversion specification characters describing the arguments to be printed.

...N/A

The arguments to be printed.

This function does not use the normal printf format conventions. To print text debug messages, use emberDebugPrintf(). The format string must contain only these conversion specification characters:

  • B - uint8_t value.

  • W - uint16_t value, printed least significant byte first.

  • D - uint32_t value, printed least significant byte first.

  • F - pointer to null terminated string in Flash (const char *).

  • xxxp - pointer to RAM, length is xxx (max 255).

  • lp - pointer to RAM, length is uint8_t argument.

  • xxxf - pointer to Flash (const char *), length is xxx (max 255).

  • lf - pointer to Flash (const char *), length is uint8_t argument.

  • b - EmberMessageBuffer.

Examples:

emberDebugBinaryPrintf("BWD", status, panId, channelMask);
emberDebugBinaryPrintf("F8p", "string example", eui64);
emberDebugBinaryPrintf("lp64fb", length, bytes, dataTable, buffer);

emDebugSendVuartMessage#

void emDebugSendVuartMessage (uint8_t * buff, uint8_t len)

Sends VUART data out the debug channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/Abuff

A pointer to the data to send.

uint8_tN/Alen

The length of the data to send.


emberDebugError#

void emberDebugError (EmberStatus code)

Prints an EmberStatus return code to the serial port.

Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Acode

The EmberStatus code to print.


emberDebugReportOff#

bool emberDebugReportOff (void )

Turns off all debug output.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The current state (true for on, false for off).


emberDebugReportRestore#

void emberDebugReportRestore (bool state)

Restores the state of the debug output.

Parameters
TypeDirectionArgument NameDescription
boolN/Astate

The state returned from emberDebugReportOff(). This is done so that debug output is not blindly turned on.


emberDebugPrintf#

void emberDebugPrintf (const char * formatString, ... )

Prints text debug messages.

Parameters
TypeDirectionArgument NameDescription
const char *N/AformatString

Takes the following:

...N/A

%%

Percent sign

%c

Single-byte char

%s

RAM string

%p

Flash string (does not follow the printf standard)

%u

Two-byte unsigned decimal

%d

Two-byte signed decimal

%x, %%2x, %%4x

1-, 2-, 4-byte hex value (always 0 padded; does not follow the printf standard)


Macro Definition Documentation#

NO_DEBUG#

#define NO_DEBUG
Value:
0

BASIC_DEBUG#

#define BASIC_DEBUG
Value:
1

FULL_DEBUG#

#define FULL_DEBUG
Value:
2

emberDebugInit#

#define emberDebugInit
Value:
(port)

This function is obsolete and no longer required to initialize the debug system.