Modules#
ZLL Commissioning Client#
API and Callbacks for the ZLL Commissioning Cluster Client Component.
Client side implementation of the ZigBee 3.0 touchlink commissioning mechanism.
API#
Initiate the touch link procedure.
Initiate a touch link to retrieve information about a target device.
Initiate a touch link to cause a target device to identify itself.
Initiate a touch link for the purpose of resetting a target device.
Abort the touch link procedure.
API Documentation#
emberAfZllInitiateTouchLink#
EmberStatus emberAfZllInitiateTouchLink (void)
Initiate the touch link procedure.
N/A |
This function causes the stack to broadcast a series of ScanRequest commands via inter-PAN messaging. The plugin selects the target that sent a ScanResponse command with the strongest RSSI and attempts to link with it. If touch linking completes successfully, the plugin calls emberAfPluginZllCommissioningTouchLinkCompleteCallback with information about the network and the target. If touch linking fails, the plugin calls emberAfPluginZllCommissioningTouchLinkFailedCallback.
Returns
An EmberStatus value that indicates the success or failure of the command.
53
of file app/framework/plugin/zll-commissioning-client/zll-commissioning-client.h
emberAfZllDeviceInformationRequest#
EmberStatus emberAfZllDeviceInformationRequest (void)
Initiate a touch link to retrieve information about a target device.
N/A |
As with a traditional touch link, this function causes the stack to broadcast messages to discover a target device. When the target is selected (based on RSSI), the plugin will retrieve information about it by unicasting a series of DeviceInformationRequest commands via inter-PAN messaging. If the process completes successfully, the plugin calls emberAfPluginZllCommissioningTouchLinkCompleteCallback with information about the target. If touch linking fails, the plugin calls emberAfPluginZllCommissioningTouchLinkFailedCallback.
Returns
An EmberStatus value that indicates the success or failure of the command.
70
of file app/framework/plugin/zll-commissioning-client/zll-commissioning-client.h
emberAfZllIdentifyRequest#
EmberStatus emberAfZllIdentifyRequest (void)
Initiate a touch link to cause a target device to identify itself.
N/A |
As with a traditional touch link, this function causes the stack to broadcast messages to discover a target device. When the target is selected (based on RSSI), the plugin will cause it to identify itself by unicasting an IdentifyRequest command via inter-PAN messaging. If the process completes successfully, the plugin calls emberAfPluginZllCommissioningTouchLinkCompleteCallback with information about the target. If touch linking fails, the plugin calls emberAfPluginZllCommissioningTouchLinkFailedCallback.
Returns
An EmberStatus value that indicates the success or failure of the command.
87
of file app/framework/plugin/zll-commissioning-client/zll-commissioning-client.h
emberAfZllResetToFactoryNewRequest#
EmberStatus emberAfZllResetToFactoryNewRequest (void)
Initiate a touch link for the purpose of resetting a target device.
N/A |
As with a traditional touch link, this function causes the stack to broadcast messages to discover a target device. When the target is selected (based on RSSI), the plugin will reset it by unicasting a ResetToFactoryNewRequest command via inter-PAN messaging. If the process completes successfully, the plugin calls emberAfPluginZllCommissioningTouchLinkCompleteCallback with information about the target. If touch linking fails, the plugin calls emberAfPluginZllCommissioningTouchLinkFailedCallback.
Returns
An EmberStatus value that indicates the success or failure of the command.
103
of file app/framework/plugin/zll-commissioning-client/zll-commissioning-client.h
emberAfZllAbortTouchLink#
void emberAfZllAbortTouchLink (void)
Abort the touch link procedure.
N/A |
This function can be called to cancel the touch link procedure. This can be useful, for example, if the touch link target is incorrect.
110
of file app/framework/plugin/zll-commissioning-client/zll-commissioning-client.h