Comms Hub#

Callbacks for Comms Hub Component.

Callbacks#

bool

Accept a tunnel.

void
emAfPluginCommsHubFunctionTunnelDataReceivedCallback(EmberEUI64 senderDeviceId, uint16_t length, uint8_t *payload)

Notify that tunnel data was received.

void
emberAfPluginCommsHubFunctionSendCallback(uint8_t status, EmberEUI64 destinationDeviceId, uint16_t dataLen, uint8_t *data)

Send.

void
emberAfPluginCommsHubFunctionReceivedCallback(EmberEUI64 senderDeviceId, uint16_t dataLen, uint8_t *data)

Receive.

void
emberAfPluginCommsHubFunctionAlertWANCallback(uint16_t alertCode, uint8_t *gbzAlert, uint16_t gbzAlertLength)

Alert WAN.

void

Tunnel opened.

Callbacks Documentation#

emAfPluginCommsHubFunctionTunnelAcceptCallback#

bool emAfPluginCommsHubFunctionTunnelAcceptCallback (EmberEUI64 deviceId)

Accept a tunnel.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/AdeviceId

An identifier of the device from which a tunnel is requested

Called by the tunnel manager when a tunnel is requested. Check the given device identifier should be checked against the Device Log to verify whether tunnels from the device should be accepted or not.

Returns

  • True if the tunnel should be allowed, false otherwise.


emAfPluginCommsHubFunctionTunnelDataReceivedCallback#

void emAfPluginCommsHubFunctionTunnelDataReceivedCallback (EmberEUI64 senderDeviceId, uint16_t length, uint8_t * payload)

Notify that tunnel data was received.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/AsenderDeviceId

The identifier of the device from which the data was received.

uint16_tN/Alength

The length of the data received

uint8_t *N/Apayload

Data received.

Called by the tunnel manager when data is received over a tunnel. It is responsible for the implementation of the GET, GET_RESPONSE, PUT protocol used when communicating with a sleepy device.


emberAfPluginCommsHubFunctionSendCallback#

void emberAfPluginCommsHubFunctionSendCallback (uint8_t status, EmberEUI64 destinationDeviceId, uint16_t dataLen, uint8_t * data)

Send.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Astatus

The status of the message that was sent Ver.: always

EmberEUI64N/AdestinationDeviceId

The EUI64 of the destination device to which the data was sent Ver.: always

uint16_tN/AdataLen

The length in octets of the data that was sent Ver.: always

uint8_t *N/Adata

Buffer containing the raw octets of the data that was sent Ver.: always

This callback is called by the Comms Hub Function (CHF) plugin to report the status of a message that was previously sent.


emberAfPluginCommsHubFunctionReceivedCallback#

void emberAfPluginCommsHubFunctionReceivedCallback (EmberEUI64 senderDeviceId, uint16_t dataLen, uint8_t * data)

Receive.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/AsenderDeviceId

The EUI64 of the sending device Ver.: always

uint16_tN/AdataLen

The length in octets of the data Ver.: always

uint8_t *N/Adata

Buffer containing the raw octets of the data Ver.: always

This callback is called by the Comms Hub Function (CHF) plugin whenever a message is received.


emberAfPluginCommsHubFunctionAlertWANCallback#

void emberAfPluginCommsHubFunctionAlertWANCallback (uint16_t alertCode, uint8_t * gbzAlert, uint16_t gbzAlertLength)

Alert WAN.

Parameters
TypeDirectionArgument NameDescription
uint16_tN/AalertCode

The 16 bit allert code as defined by GBCS Ver.: always

uint8_t *N/AgbzAlert

Buffer continaing the GBZ formatted Alert Ver.: always

uint16_tN/AgbzAlertLength

The length in octets of the GBZ formatted Alert Ver.: always

Notify the application of an Alert that should be sent to the WAN. The second argument is a pointer to the GBZ alert buffer. The application is responsible for freeing this buffer.


emberAfPluginCommsHubFunctionTunnelOpenedCallback#

void emberAfPluginCommsHubFunctionTunnelOpenedCallback (EmberEUI64 remoteDeviceId)

Tunnel opened.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/AremoteDeviceId

The EUI64 of the remote device for which a tunnel is opened Ver.: always

This function is called by the Comms Hub Function (CHF) plugin when a tunnel is opened.