Network Utility Functions#
API and Callbacks for the Network Utility functionality in the Application Framework.
Network Utility Functions description.
API#
Form a new network using the specified network parameters.
Associate with the network using the specified network parameters.
Find an unused PAN ID and form a new network.
Find a joinable network and join it.
Set the current network to that of the given index and add it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
Set the current network to the callback network and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
Set the current network to that of the given endpoint and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
Remove the topmost network from the stack of networks maintained by the framework and sets the current network to the new topmost network. Every call to this API must be paired with a prior call to emberAfPushNetworkIndex, emberAfPushCallbackNetworkIndex, or emberAfPushEndpointNetworkIndex.
Return the primary endpoint of the given network index or 0xFF if no endpoints belong to the network.emberAfStatus.
Return the primary endpoint of the current network index or 0xFF if no endpoints belong to the current network.
API Documentation#
emberAfFormNetwork#
EmberStatus emberAfFormNetwork (EmberNetworkParameters * parameters)
Form a new network using the specified network parameters.
Type | Direction | Argument Name | Description |
---|---|---|---|
EmberNetworkParameters * | N/A | parameters | Specification of the new network. |
Returns
An ::EmberStatus value that indicates either the successful formation of the new network or the reason that the network formation failed.
2138
of file app/framework/include/af.h
emberAfJoinNetwork#
EmberStatus emberAfJoinNetwork (EmberNetworkParameters * parameters)
Associate with the network using the specified network parameters.
Type | Direction | Argument Name | Description |
---|---|---|---|
EmberNetworkParameters * | N/A | parameters | Specification of the network with which the node should associate. |
Returns
An ::EmberStatus value that indicates either that the association process began successfully or the reason for failure.
2148
of file app/framework/include/af.h
emberAfFindUnusedPanIdAndForm#
EmberStatus emberAfFindUnusedPanIdAndForm (void )
Find an unused PAN ID and form a new network.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
An ::EmberStatus value that indicates either the process begin successfully or the reason for failure.
2156
of file app/framework/include/af.h
emberAfStartSearchForJoinableNetwork#
EmberStatus emberAfStartSearchForJoinableNetwork (void )
Find a joinable network and join it.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
An ::EmberStatus value that indicates either the process begin successfully or the reason for failure.
2162
of file app/framework/include/af.h
emberAfPushNetworkIndex#
EmberStatus emberAfPushNetworkIndex (uint8_t networkIndex)
Set the current network to that of the given index and add it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | networkIndex |
2173
of file app/framework/include/af.h
emberAfPushCallbackNetworkIndex#
EmberStatus emberAfPushCallbackNetworkIndex (void )
Set the current network to the callback network and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
2179
of file app/framework/include/af.h
emberAfPushEndpointNetworkIndex#
EmberStatus emberAfPushEndpointNetworkIndex (uint8_t endpoint)
Set the current network to that of the given endpoint and adds it to the stack of networks maintained by the framework. Every call to this API must be paired with a subsequent call to emberAfPopNetworkIndex.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | endpoint |
2185
of file app/framework/include/af.h
emberAfPopNetworkIndex#
EmberStatus emberAfPopNetworkIndex (void )
Remove the topmost network from the stack of networks maintained by the framework and sets the current network to the new topmost network. Every call to this API must be paired with a prior call to emberAfPushNetworkIndex, emberAfPushCallbackNetworkIndex, or emberAfPushEndpointNetworkIndex.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
2193
of file app/framework/include/af.h
emberAfPrimaryEndpointForNetworkIndex#
uint8_t emberAfPrimaryEndpointForNetworkIndex (uint8_t networkIndex)
Return the primary endpoint of the given network index or 0xFF if no endpoints belong to the network.emberAfStatus.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | networkIndex |
2198
of file app/framework/include/af.h
emberAfPrimaryEndpointForCurrentNetworkIndex#
uint8_t emberAfPrimaryEndpointForCurrentNetworkIndex (void )
Return the primary endpoint of the current network index or 0xFF if no endpoints belong to the current network.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
2203
of file app/framework/include/af.h