You are viewing documentation for version:
A sample policy file that implements the callbacks for the Zigbee Over-the-air bootload cluster server.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
#define OTA_SERVER_NO_RATE_LIMITING_FOR_CLIENT 0
#define OTA_SERVER_CLIENT_USES_MILLISECONDS 1
#define OTA_SERVER_CLIENT_USES_SECONDS 2
#define OTA_SERVER_DISCOVER_CLIENT_DELAY_UNITS 3
#ifdef EMBER_TEST
#define OTA_SERVER_DO_NOT_OVERRIDE_CLIENT_DELAY_UNITS 0xFF
#endif
uint8_t emberAfPluginOtaServerPolicyGetClientDelayUnits(EmberNodeId clientNodeId,
EmberEUI64 clientEui64);
uint8_t emberAfOtaServerImageBlockRequestCallback(EmberAfImageBlockRequestCallbackStruct* data);
void emAfOtaServerPolicyPrint(void);
void emAfOtaServerSetQueryPolicy(uint8_t value);
void emAfOtaServerSetBlockRequestPolicy(uint8_t value);
void emAfOtaServerSetUpgradePolicy(uint8_t value);
bool emAfServerPageRequestTickCallback(uint16_t relativeOffset, uint8_t blockSize);
void emAfSetPageRequestMissedBlockModulus(uint16_t modulus);
void emAfOtaServerSetPageRequestPolicy(uint8_t value);
void emAfOtaServerPolicySetMinBlockRequestPeriod(uint16_t minBlockRequestPeriodMS);
Macros#
#define
OTA_SERVER_NO_RATE_LIMITING_FOR_CLIENT 0
#define
OTA_SERVER_CLIENT_USES_MILLISECONDS 1
#define
OTA_SERVER_CLIENT_USES_SECONDS 2
#define
OTA_SERVER_DISCOVER_CLIENT_DELAY_UNITS 3
API Documentation#
emberAfPluginOtaServerPolicyGetClientDelayUnits#
uint8_t emberAfPluginOtaServerPolicyGetClientDelayUnits (EmberNodeId clientNodeId, EmberEUI64 clientEui64)
GetClientDelayUnits.
ParametersType | Direction | Argument Name | Description | EmberNodeId | N/A | clientNodeId | Ver.: always |
EmberEUI64 | N/A | clientEui64 | Ver.: always |
Called when the server receives an Image Block Request from a client that supports rate limiting using the Minimum Block Period feature. This callback gives the server a chance to decide which units the client uses for the Minimum Block Period, seconds or milliseconds. The server can also return OTA_SERVER_DISCOVER_CLIENT_DELAY_UNITS, which causes the plugin code to test the client by sending it a preset delay value. The length of time the client delays determines which units it uses. For more information on this feature, see the plugin option descriptions under the OTA Server plugin.
For return values, see ota-server-policy.h. An unknown return value will result in the same behavior as if OTA_SERVER_CLIENT_USES_MILLISECONDS had been returned.
Function Documentation#
emAfOtaServerPolicyPrint#
void emAfOtaServerPolicyPrint (void )
ParametersType | Direction | Argument Name | Description | void | N/A | | |
emAfOtaServerSetQueryPolicy#
void emAfOtaServerSetQueryPolicy (uint8_t value)
ParametersType | Direction | Argument Name | Description | uint8_t | N/A | value | |
emAfOtaServerSetBlockRequestPolicy#
void emAfOtaServerSetBlockRequestPolicy (uint8_t value)
ParametersType | Direction | Argument Name | Description | uint8_t | N/A | value | |
emAfOtaServerSetUpgradePolicy#
void emAfOtaServerSetUpgradePolicy (uint8_t value)
ParametersType | Direction | Argument Name | Description | uint8_t | N/A | value | |
emAfServerPageRequestTickCallback#
bool emAfServerPageRequestTickCallback (uint16_t relativeOffset, uint8_t blockSize)
ParametersType | Direction | Argument Name | Description | uint16_t | N/A | relativeOffset | |
uint8_t | N/A | blockSize | |
emAfSetPageRequestMissedBlockModulus#
void emAfSetPageRequestMissedBlockModulus (uint16_t modulus)
ParametersType | Direction | Argument Name | Description | uint16_t | N/A | modulus | |
emAfOtaServerSetPageRequestPolicy#
void emAfOtaServerSetPageRequestPolicy (uint8_t value)
ParametersType | Direction | Argument Name | Description | uint8_t | N/A | value | |
emAfOtaServerPolicySetMinBlockRequestPeriod#
void emAfOtaServerPolicySetMinBlockRequestPeriod (uint16_t minBlockRequestPeriodMS)
ParametersType | Direction | Argument Name | Description | uint16_t | N/A | minBlockRequestPeriodMS | |