Modules#

EmberAfPriceCommonInfo

EmberAfScheduledPrice

Price Common#

API and Callbacks for the Price Common Component.

This component provides common utility functions used by both the Price Server and Price Client components.

API#

uint8_t
emberAfPluginPriceCommonGetCommonMatchingOrUnusedIndex(EmberAfPriceCommonInfo *commonInfos, uint8_t numberOfEntries, uint32_t newIssuerEventId, uint32_t newStartTime, bool expireTimedOut)

Return the best matching or other index to use for inserting new data.

void
emberAfPluginPriceCommonSort(EmberAfPriceCommonInfo *commonInfos, uint8_t *dataArray, uint16_t dataArrayBlockSizeInByte, uint16_t dataArraySize)

Sort price-related data structures.

void
emberAfPluginPriceCommonUpdateDurationForOverlappingEvents(EmberAfPriceCommonInfo *commonInfos, uint8_t numberOfEntries)

Update durations to avoid overlapping the next event.

uint32_t
emberAfPluginPriceCommonSecondsUntilSecondIndexActive(EmberAfPriceCommonInfo *commonInfos, uint8_t numberOfEntries)

Determine the time until the next index becomes active.

uint8_t
emberAfPluginPriceCommonFindValidEntries(uint8_t *validEntries, uint8_t numberOfEntries, EmberAfPriceCommonInfo *commonInfos, uint32_t earliestStartTime, uint32_t minIssuerEventId, uint8_t numberOfCommands)

Find valid entries in the EmberAfPriceCommonInfo structure array.

uint8_t
emberAfPluginPriceCommonServerGetActiveIndex(EmberAfPriceCommonInfo *commonInfos, uint8_t numberOfEntries)

Return the index of the active entry in the EmberAfPriceCommonInfo array.

uint8_t
emberAfPluginPriceCommonServerGetFutureIndex(EmberAfPriceCommonInfo *commonInfos, uint8_t numberOfEntries, uint32_t *secUntilFutureEvent)

Return the index to the most recent entry that will become active in the future.

Macros#

#define
EMBER_AF_PRICE_CLUSTER_SERVER_ENDPOINT_COUNT (1)
#define
EVENT_ID_UNSPECIFIED (0xFFFFFFFFUL)
#define
TARIFF_TYPE_UNSPECIFIED (0xFFu)
#define
ZCL_PRICE_CLUSTER_PRICE_ACKNOWLEDGEMENT_MASK (0x01u)
#define
ZCL_PRICE_CLUSTER_RESERVED_MASK (0xFEu)
#define
ZCL_PRICE_CLUSTER_DURATION16_UNTIL_CHANGED (0xFFFFu)
#define
ZCL_PRICE_CLUSTER_DURATION_SEC_UNTIL_CHANGED (0xFFFFFFFFUL)
#define
ZCL_PRICE_CLUSTER_END_TIME_NEVER (0xFFFFFFFFUL)
#define
ZCL_PRICE_CLUSTER_NUMBER_OF_EVENTS_ALL (0x00u)
#define
ZCL_PRICE_CLUSTER_START_TIME_NOW (0x00000000UL)
#define
ZCL_PRICE_CLUSTER_WILDCARD_ISSUER_ID (0xFFFFFFFFUL)
#define
ZCL_PRICE_INVALID_ENDPOINT_INDEX (0xFFu)
#define
ZCL_PRICE_INVALID_INDEX (0xFFu)
#define
ZCL_PRICE_CLUSTER_DURATION_UNTIL_CHANGED (0xFFFFu)

API Documentation#

emberAfPluginPriceCommonGetCommonMatchingOrUnusedIndex#

uint8_t emberAfPluginPriceCommonGetCommonMatchingOrUnusedIndex (EmberAfPriceCommonInfo * commonInfos, uint8_t numberOfEntries, uint32_t newIssuerEventId, uint32_t newStartTime, bool expireTimedOut)

Return the best matching or other index to use for inserting new data.

Parameters
TypeDirectionArgument NameDescription
EmberAfPriceCommonInfo *N/AcommonInfos

An array of EmberAfPriceCommonInfo structures whose data is used to find the best available index.

uint8_tN/AnumberOfEntries

The number of entries in the EmberAfPriceCommonInfo array.

uint32_tN/AnewIssuerEventId

The issuerEventId of the new data. This is used to see if a match is present.

uint32_tN/AnewStartTime

The startTime of the new data.

boolN/AexpireTimedOut

Treats any timed-out entries as invalid if set to true.

Returns

  • The best index - either a matching index, if found, or an invalid or timed out index.


emberAfPluginPriceCommonSort#

void emberAfPluginPriceCommonSort (EmberAfPriceCommonInfo * commonInfos, uint8_t * dataArray, uint16_t dataArrayBlockSizeInByte, uint16_t dataArraySize)

Sort price-related data structures.

Parameters
TypeDirectionArgument NameDescription
EmberAfPriceCommonInfo *N/AcommonInfos

The destination address to which the command should be sent.

uint8_t *N/AdataArray

The source endpoint used in the transmission.

uint16_tN/AdataArrayBlockSizeInByte

The source endpoint used in the transmission.

uint16_tN/AdataArraySize

The source endpoint used in the transmission.

This semi-generic sorting function can be used to sort all structures that utilizes the EmberAfPriceCommonInfo data type.


emberAfPluginPriceCommonUpdateDurationForOverlappingEvents#

void emberAfPluginPriceCommonUpdateDurationForOverlappingEvents (EmberAfPriceCommonInfo * commonInfos, uint8_t numberOfEntries)

Update durations to avoid overlapping the next event.

Parameters
TypeDirectionArgument NameDescription
EmberAfPriceCommonInfo *N/AcommonInfos

An array of EmberAfPriceCommonInfo structures that will be evaluated.

uint8_tN/AnumberOfEntries

The number of entries in the EmberAfPriceCommonInfo array.


emberAfPluginPriceCommonSecondsUntilSecondIndexActive#

uint32_t emberAfPluginPriceCommonSecondsUntilSecondIndexActive (EmberAfPriceCommonInfo * commonInfos, uint8_t numberOfEntries)

Determine the time until the next index becomes active.

Parameters
TypeDirectionArgument NameDescription
EmberAfPriceCommonInfo *N/AcommonInfos

An array of EmberAfPriceCommonInfo structures that will be evaluated.

uint8_tN/AnumberOfEntries

The number of entries in the EmberAfPriceCommonInfo array.

This function assumes the commonInfos[] array is already sorted by startTime from earliest to latest.


emberAfPluginPriceCommonFindValidEntries#

uint8_t emberAfPluginPriceCommonFindValidEntries (uint8_t * validEntries, uint8_t numberOfEntries, EmberAfPriceCommonInfo * commonInfos, uint32_t earliestStartTime, uint32_t minIssuerEventId, uint8_t numberOfCommands)

Find valid entries in the EmberAfPriceCommonInfo structure array.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/AvalidEntries

An array of the same size as the EmberAfPriceCommonInfo array that will store the valid flag for each entry (true or false).

uint8_tN/AnumberOfEntries

The number of entries in the validEntries array and the commonInfos array.

EmberAfPriceCommonInfo *N/AcommonInfos

The EmberAfPriceCommonInfo array that will be searched for valid entries.

uint32_tN/AearliestStartTime

A minimum start time such that all valid entries have a start time greater than or equal to this value. A minimum event ID such that all valid entries have an issuerEventId greater than or equal to this. The maximum number of valid entries to be returned.

uint32_tN/AminIssuerEventId
uint8_tN/AnumberOfCommands

Returns

  • The number of valid commands found in the commonInfos array.


emberAfPluginPriceCommonServerGetActiveIndex#

uint8_t emberAfPluginPriceCommonServerGetActiveIndex (EmberAfPriceCommonInfo * commonInfos, uint8_t numberOfEntries)

Return the index of the active entry in the EmberAfPriceCommonInfo array.

Parameters
TypeDirectionArgument NameDescription
EmberAfPriceCommonInfo *N/AcommonInfos

The EmberAfPriceCommonInfo array that will be searched for an active entry.

uint8_tN/AnumberOfEntries

The number of entries in the commonInfo array.

Search through array for the most recent active entry. "Issuer Event Id" has higher priority than "start time".

Returns

  • The index of the active entry, or 0xFF if an active entry is not found.


emberAfPluginPriceCommonServerGetFutureIndex#

uint8_t emberAfPluginPriceCommonServerGetFutureIndex (EmberAfPriceCommonInfo * commonInfos, uint8_t numberOfEntries, uint32_t * secUntilFutureEvent)

Return the index to the most recent entry that will become active in the future.

Parameters
TypeDirectionArgument NameDescription
EmberAfPriceCommonInfo *N/AcommonInfos

The EmberAfPriceCommonInfo array that will be searched for the entry. The number of entries in the commonInfo array. The output pointer to the number of seconds until the next active entry.

uint8_tN/AnumberOfEntries
uint32_t *N/AsecUntilFutureEvent

Returns

  • The index of the next-active entry, or 0xFF if an active entry is not found.