Modules#
EmberBeaconClassificationParams
Ember Common Data Types#
See ember-types.h for source code.
Miscellaneous Ember Types#
Type of Ember software version.
EmberReleaseTypeStruct Data that relates release type to the correct string.
EmberReleaseTypeStruct Data that relates release type to the correct string.
EmberReleaseTypeStruct Data that relates release type to the correct string.
EmberReleaseTypeStruct Data that relates release type to the correct string.
16-bit ZigBee network address.
802.15.4 PAN ID.
A structure containing the version information.
EmberReleaseTypeStruct Data that relates release type to the correct string.
Size of EUI64 (an IEEE address) in bytes (8).
Size of an extended PAN identifier in bytes (8).
Size of an encryption key in bytes (16).
Size of Implicit Certificates used for Certificate-based Key Exchange(CBKE).
Size of Public Keys used in Elliptical Cryptography ECMQV algorithms.
Size of Private Keys used in Elliptical Cryptography ECMQV algorithms.
Size of the SMAC used in Elliptical Cryptography ECMQV algorithms.
Size of the DSA signature used in Elliptical Cryptography Digital Signature Algorithms.
The size of AES-128 MMO hash is 16-bytes. This is defined in the core. ZigBee specification.
Size of Implicit Certificates used for Certificate Based Key Exchange using the ECC283K1 curve in bytes.
Size of Public Keys used in SECT283k1 Elliptical Cryptography ECMQV algorithms.
Size of Private Keys used SECT283k1 in Elliptical Cryptography ECMQV algorithms.
Size of the DSA signature used in SECT283k1 Elliptical Cryptography Digital Signature Algorithms.
Return type for Ember functions.
EUI 64-bit ID (an IEEE address).
The maximum 802.15.4 channel number is 26.
The minimum 2.4GHz 802.15.4 channel number is 11.
The minimum SubGhz channel number is 0.
ZigBee protocol specifies that active scans have a duration of 3 (138 msec). See documentation for emberStartScan in include/network-formation.h for more info on duration values.
The SubGhz scan duration is 5.
There are sixteen 802.15.4 channels.
A bitmask to scan all 2.4 GHz 802.15.4 channels.
The maximum channels per page are 27 page bits 31...27, channel bits 26...0.
Sub-GHz channel bitmasks for pages 28, 30, 31.
The maximum SubGhz channel number on pages 28, 30, 31 is 26.
SubGhz channel bitmasks for page 29.
The maximum SubGhz channel number on page 29 is 8.
The minimum SubGhz page number is 28.
The maximum SubGhz page number is 31.
A bitmask for the channel page within a channel mask.
A page-channel mask for a given page and channel mask.
A page-channel mask for a given page and channel.
The network ID of the coordinator in a ZigBee network is 0x0000.
A distinguished network ID that will never be assigned to any node. It is used to indicate the absence of a node ID.
The channel page value used to indicate just the 2.4GHz channels.
A distinguished EUI64 that is commonly used to indicate an invalid EUI64.
A distinguished binding index used to indicate the absence of a binding.
A distinguished network ID that will never be assigned to any node.
A distinguished network ID that will never be assigned to any node. This value is returned when getting the remote node ID from the binding table and the given binding table index refers to a multicast binding entry.
A distinguished network ID that will never be assigned to any node. This value is used when getting the remote node ID from the address or binding tables. It indicates that the address or binding table entry is currently in use but the node ID corresponding to the EUI64 in the table is currently unknown.
A distinguished network ID that will never be assigned to any node. This value is used when getting the remote node ID from the address or binding tables. It indicates that the address or binding table entry is currently in use and network address discovery is underway.
A distinguished address table index used to indicate the absence of an address table entry.
The endpoint where the ZigBee Device Object (ZDO) resides.
The broadcast endpoint, as defined in the ZigBee spec.
The profile ID used by the ZigBee Device Object (ZDO).
The profile ID used to address all the public profiles.
The maximum value for a profile ID in the standard profile range.
The broadcast table entry timeout, which specifies, in quarter seconds, how long an entry persists in the local device's broadcast table.
Ember's Manufacturer ID.
An invalid network index.
Use Ember's default duty cycle limit configurations.
ZigBee Broadcast Addresses#
ZigBee specifies three different broadcast addresses that reach different collections of nodes. Broadcasts are normally sent only to routers. Broadcasts can also be forwarded to end devices, either all of them or only those that do not sleep. Broadcasting to end devices is both significantly more resource-intensive and significantly less reliable than broadcasting to routers.
Broadcast to all routers.
Broadcast to all non-sleepy devices.
Broadcast to all devices, including sleepy end devices.
Ember Concentrator Types#
A concentrator with insufficient memory to store source routes for the entire network. Route records are sent to the concentrator prior to every inbound APS unicast.
A concentrator with sufficient memory to store source routes for the entire network. Remote nodes stop sending route records once the concentrator has successfully received one.
txPowerModes for emberSetTxPowerMode and mfglibSetPower#
The application should call emberSetTxPowerMode() with the txPowerMode parameter set to this value to disable all power mode options, resulting in normal power mode and bi-directional RF transmitter output.
The application should call emberSetTxPowerMode() with the txPowerMode parameter set to this value to enable boost power mode.
The application should call emberSetTxPowerMode() with the txPowerMode parameter set to this value to enable the alternate transmitter output.
The application should call emberSetTxPowerMode() with the txPowerMode parameter set to this value to enable both boost mode and the alternate transmitter output.
Counters Request Definitions#
This is a ZigBee application profile ID that has been assigned to Ember Corporation.
Ember's first private profile ID.
Ember's last private profile ID.
The cluster ID used to request that a node respond with a report of its Ember stack counters. See app/util/counters/counters-ota.h.
The cluster ID used to respond to an EMBER_REPORT_COUNTERS_REQUEST.
The cluster ID used to request that a node respond with a report of its Ember stack counters. The node will also reset its clusters to zero after a successful response. See app/util/counters/counters-ota.h.
The cluster ID used to respond to an EMBER_REPORT_AND_CLEAR_COUNTERS_REQUEST.
The cluster ID used to send and receive over the air certificate messages. This is used to field upgrade devices with Smart Energy Certificates and other security data.
ZDO response status.#
Most responses to ZDO commands contain a status byte. The meaning of this byte is defined by the ZigBee Device Profile.
Network and IEEE Address Request/Response#
Defines for ZigBee device profile cluster IDs follow. These include descriptions of the formats of the messages.Note that each message starts with a 1-byte transaction sequence number. This sequence number is used to match a response command frame to the request frame that it is replying to. The application shall maintain a 1-byte counter that is copied into this field and incremented by one for each command sent. When a value of 0xff is reached, the next command shall re-start the counter with a value of 0x00. Network request: <transaction sequence number: 1> <EUI64:8> <type:1> <start index:1>IEEE request: <transaction sequence number: 1> <node ID:2> <type:1> <start index:1> <type> = 0x00 single address response, ignore the start index = 0x01 extended response -> sends kid's IDs as wellResponse: <transaction sequence number: 1> <status:1> <EUI64:8> <node ID:2> <ID count:1> <start index:1> <child ID:2>*
Node Descriptor Request/Response#
Request: <transaction sequence number: 1> <node ID:2> Response: <transaction sequence number: 1> <status:1> <node ID:2>// <node descriptor: 13>//// Node Descriptor field is divided into subfields of bitmasks as follows:// (Note: All lengths below are given in bits rather than bytes.)// Logical Type: 3// Complex Descriptor Available: 1// User Descriptor Available: 1// (reserved/unused): 3// APS Flags: 3// Frequency Band: 5// MAC capability flags: 8// Manufacturer Code: 16// Maximum buffer size: 8// Maximum incoming transfer size: 16// Server mask: 16// Maximum outgoing transfer size: 16// Descriptor Capability Flags: 8// See ZigBee document 053474, Section 2.3.2.3 for more details.
Power Descriptor Request / Response#
Request: <transaction sequence number: 1> <node ID:2> Response: <transaction sequence number: 1> <status:1> <node ID:2> <current power mode, available power sources:1> <current power source, current power source level:1>// See ZigBee document 053474, Section 2.3.2.4 for more details.
Simple Descriptor Request / Response#
Request: <transaction sequence number: 1> <node ID:2> <endpoint:1>Response: <transaction sequence number: 1> <status:1> <node ID:2> <length:1> <endpoint:1> <app profile ID:2> <app device ID:2> <app device version, app flags:1> <input cluster count:1> <input cluster:2>* <output cluster count:1> <output cluster:2>*
Active Endpoints Request / Response#
Request: <transaction sequence number: 1> <node ID:2>Response: <transaction sequence number: 1> <status:1> <node ID:2> <endpoint count:1> <endpoint:1>*
Match Descriptors Request / Response#
Request: <transaction sequence number: 1> <node ID:2> <app profile ID:2> <input cluster count:1> <input cluster:2>* <output cluster count:1> <output cluster:2>*Response: <transaction sequence number: 1> <status:1> <node ID:2> <endpoint count:1> <endpoint:1>*
Discovery Cache Request / Response#
Request: <transaction sequence number: 1> <source node ID:2> <source EUI64:8>Response: <transaction sequence number: 1> <status (== EMBER_ZDP_SUCCESS):1>
End Device Announce and End Device Announce Response#
Request: <transaction sequence number: 1> <node ID:2> <EUI64:8> <capabilities:1>No response is sent.
System Server Discovery Request / Response#
This is broadcast and only servers which have matching services respond. The response contains the request services that the recipient provides.Request: <transaction sequence number: 1> <server mask:2>Response: <transaction sequence number: 1> <status (== EMBER_ZDP_SUCCESS):1> <server mask:2>
Parent Announce and Parent Announce Response#
This is broadcast and only servers which have matching children respond. The response contains the list of children that the recipient now holds.Request: <transaction sequence number: 1> <number of children:1> <child EUI64:8> <child Age:4>*Response: <transaction sequence number: 1> <number of children:1> <child EUI64:8> <child Age:4>*
ZDO server mask bits#
These are used in server discovery requests and responses.
Find Node Cache Request / Response#
This is broadcast and only discovery servers which have the information for the device of interest, or the device of interest itself, respond. The requesting device can then direct any service discovery requests to the responder.Request: <transaction sequence number: 1> <device of interest ID:2> <d-of-i EUI64:8>Response: <transaction sequence number: 1> <responder ID:2> <device of interest ID:2> <d-of-i EUI64:8>
End Device Bind Request / Response#
Request: <transaction sequence number: 1> <node ID:2> <EUI64:8> <endpoint:1> <app profile ID:2> <input cluster count:1> <input cluster:2>* <output cluster count:1> <output cluster:2>*Response: <transaction sequence number: 1> <status:1>
Binding types and Request / Response#
Bind and unbind have the same formats. There are two possible formats, depending on whether the destination is a group address or a device address. Device addresses include an endpoint, groups don't.Request: <transaction sequence number: 1> <source EUI64:8> <source endpoint:1> <cluster ID:2> <destination address:3 or 10>Destination address: <0x01:1> <destination group:2>Or: <0x03:1> <destination EUI64:8> <destination endpoint:1>Response: <transaction sequence number: 1> <status:1>
LQI Table Request / Response#
Request: <transaction sequence number: 1> <start index:1>Response: <transaction sequence number: 1> <status:1> <neighbor table entries:1> <start index:1> <entry count:1> <entry:22>* <entry> = <extended PAN ID:8> <EUI64:8> <node ID:2> <device type, RX on when idle, relationship:1> <permit joining:1> <depth:1> <LQI:1>The device-type byte has the following fields: Name Mask Valuesdevice type 0x03 0x00 coordinator 0x01 router 0x02 end device 0x03 unknownrx mode 0x0C 0x00 off when idle 0x04 on when idle 0x08 unknownrelationship 0x70 0x00 parent 0x10 child 0x20 sibling 0x30 other 0x40 previous childreserved 0x10The permit-joining byte has the following fields Name Mask Valuespermit joining 0x03 0x00 not accepting join requests 0x01 accepting join requests 0x02 unknownreserved 0xFC
Routing Table Request / Response#
Request: <transaction sequence number: 1> <start index:1>Response: <transaction sequence number: 1> <status:1> <routing table entries:1> <start index:1> <entry count:1> <entry:5>* <entry> = <destination address:2> <status:1> <next hop:2>The status byte has the following fields: Name Mask Valuesstatus 0x07 0x00 active 0x01 discovery underway 0x02 discovery failed 0x03 inactive 0x04 validation underwayflags 0x38 0x08 memory constrained 0x10 many-to-one 0x20 route record requiredreserved 0xC0
Binding Table Request / Response#
Request: <transaction sequence number: 1> <start index:1>Response: <transaction sequence number: 1> <status:1> <binding table entries:1> <start index:1> <entry count:1> <entry:14/21>* <entry> = <source EUI64:8> <source endpoint:1> <cluster ID:2> <dest addr mode:1> <dest:2/8> <dest endpoint:0/1>If Dest. Address Mode = 0x03, then the Long Dest. Address will be used and Dest. endpoint will be included. If Dest. Address Mode = 0x01, then the Short Dest. Address will be used and there will be no Dest. endpoint.
Leave Request / Response#
Request: <transaction sequence number: 1> <EUI64:8> <flags:1> The flag bits are: 0x40 remove children 0x80 rejoinResponse: <transaction sequence number: 1> <status:1>
Permit Joining Request / Response#
Request: <transaction sequence number: 1> <duration:1> <permit authentication:1>Response: <transaction sequence number: 1> <status:1>
Network Update Request / Response#
Request: <transaction sequence number: 1> <scan channels:4> <duration:1> <count:0/1> <manager:0/2> If the duration is in 0x00 ... 0x05, 'count' is present but not 'manager'. Perform 'count' scans of the given duration on the given channels. If duration is 0xFE, 'channels' should have a single channel and 'count' and 'manager' are not present. Switch to the indicated channel. If duration is 0xFF, 'count' is not present. Set the active channels and the network manager ID to the values given. Unicast requests always get a response, which is INVALID_REQUEST if the duration is not a legal value.Response: <transaction sequence number: 1> <status:1> <scanned channels:4> <transmissions:2> <failures:2> <energy count:1> <energy:1>*
Unsupported#
Not mandatory and not supported.
ZDO configuration flags.#
Control which ZDO requests are passed to the application. These are normally controlled via the following configuration definitions:EMBER_APPLICATION_RECEIVES_SUPPORTED_ZDO_REQUESTS EMBER_APPLICATION_HANDLES_UNSUPPORTED_ZDO_REQUESTS EMBER_APPLICATION_HANDLES_ENDPOINT_ZDO_REQUESTS EMBER_APPLICATION_HANDLES_BINDING_ZDO_REQUESTSSee ember-configuration.h for more information.
Enumerations#
Defines the possible types of nodes and the roles that a node might play in a network.
The configuration advertised by the end device to the parent when joining/rejoining.
Defines the options that should be used when initializing the node's network configuration.
Options to allow/disallow rejoins using the default link key.
Options to use when sending a message.
Defines the possible incoming message types.
Defines the possible outgoing message types.
A type of command received by the stack.
indication of the action taken on a packet
A type of packet received by the stack.
Defines the possible join states for a node.
Type for a network scan.
Defines binding types.
To configure non trust center node to assume a concentrator type of the trust center it join to, until it receive many-to-one route request from the trust center. For the trust center node, concentrator type is configured from the concentrator plugin. The stack by default assumes trust center be a low RAM concentrator that make other devices send route record to the trust center even without receiving a many-to-one route request. The assumed concentrator type can be changed by setting appropriate value to emberAssumedTrustCenterConcentratorType.
The decision made by the Trust Center when a node attempts to join.
The Status of the Update Device message sent to the Trust Center. The device may have joined or rejoined insecurely, rejoined securely, or left. MAC Security has been deprecated and therefore there is no secure join.
Notes the last rejoin reason.
Defines the lists of clusters that must be provided for each endpoint.
Either marks an event as inactive or specifies the units for the event execution time.
The type of method used for joining.
Defines the events reported to the application by the emberCounterHandler().
This is the Initial Security Bitmask that controls the use of various security features.
This is the Extended Security Bitmask that controls the use of various extended security features.
This is the Current Security Bitmask that details the use of various security features.
This bitmask describes the presence of fields within the EmberKeyStruct.
This denotes the type of security key.
This denotes the status of an attempt to establish a key with another device.
This enumeration determines whether or not a Trust Center answers trust center link key requests.
This enumeration determines whether or not a Trust Center answers app link key requests.
Duty cycle states.
The types of MAC passthrough messages that an application may receive. This is a bitmask.
Defines the entropy source used by the stack.
Defines the trust center APS encryption mode when sending a newer (alternate) network key to a device. The value settings below do not take effect when sending the initial network key during joining or rejoining.
Functions#
This function allows access to the actual key data bytes of the EmberKeyData structure.
Get access to the actual certificate data bytes of the EmberCertificateData structure.
Get access to the actual public key data bytes of the EmberPublicKeyData structure.
Get access to the actual private key data bytes of the EmberPrivateKeyData structure.
Get access to the actual SMAC (Secured Message Authentication Code) data of the EmberSmacData structure.
Get access to the actual ECDSA signature data of the EmberSignatureData structure.
Get access to the actual certificate data bytes of the Ember283k1CertificateData structure.
Get access to the actual public key data bytes of the Ember283k1PublicKeyData structure.
Get access to the actual private key data bytes of the Ember283k1PrivateKeyData structure.
Get access to the actual ECDSA signature data of the EmberSignature283k1Data structure.
Macros#
Returns true if nodeId (short address) is a broadcast address.
@ brief Defines the CLI enumerations for the EmberJoinDecision enum.
@ brief Defines the CLI enumerations for the EmberDeviceUpdate enum.
@ brief Defines the CLI enumerations for the EmberCounterType enum.
This is an EmberInitialSecurityBitmask value but it does not actually set anything. It is the default mode used by the ZigBee Pro stack. It is defined here so that no legacy code is broken by referencing it.
The short address of the trust center. This address never changes dynamically.
This is the legacy name for the Distributed Trust Center Mode.
This is the legacy name for the Trust Center Global Link Key.
This magic number prevents accidentally changing the key settings. The emberSetMfgSecurityConfig() API will return EMBER_INVALID_CALL unless it is passed in.
Defines the maximum number of counters that are specified as reporting either on 2.4 GHz or Sub-GHz.
Defines the maximum number of PHYs supported.
PHY index for 2.4 GHz radio interface, valid for simultaneous multi radio network.
PHY index for Sub-GHz radio interface, valid for simultaneous multi radio network.
Miscellaneous Ember Types Documentation#
EmberVersionType#
EmberVersionType
Type of Ember software version.
| Enumerator | |
|---|---|
| EMBER_VERSION_TYPE_PRE_RELEASE | |
| EMBER_VERSION_TYPE_ALPHA_1 | |
| EMBER_VERSION_TYPE_ALPHA_2 | |
| EMBER_VERSION_TYPE_ALPHA_3 | |
| EMBER_VERSION_TYPE_BETA_1 | |
| EMBER_VERSION_TYPE_BETA_2 | |
| EMBER_VERSION_TYPE_BETA_3 | |
| EMBER_VERSION_TYPE_GA | |
EmberStackProfile#
EmberStackProfile
EmberReleaseTypeStruct Data that relates release type to the correct string.
| Enumerator | |
|---|---|
| EMBER_STACK_PROFILE_NONE | |
| EMBER_STACK_PROFILE_ZIGBEE_PRO | |
EmberSecurityLevel#
EmberSecurityLevel
EmberReleaseTypeStruct Data that relates release type to the correct string.
| Enumerator | |
|---|---|
| EMBER_SECURITY_LEVEL_NONE | |
| EMBER_SECURITY_LEVEL_Z3 | |
EmberLeaveRequestFlags#
EmberLeaveRequestFlags
EmberReleaseTypeStruct Data that relates release type to the correct string.
| Enumerator | |
|---|---|
| EMBER_ZIGBEE_LEAVE_AND_REJOIN | Leave and rejoin. |
| EMBER_ZIGBEE_LEAVE_WITHOUT_REJOIN | Leave. |
EmberLeaveReason#
EmberLeaveReason
EmberReleaseTypeStruct Data that relates release type to the correct string.
| Enumerator | |
|---|---|
| EMBER_LEAVE_REASON_NONE | |
| EMBER_LEAVE_DUE_TO_NWK_LEAVE_MESSAGE | |
| EMBER_LEAVE_DUE_TO_APS_REMOVE_MESSAGE | |
| EMBER_LEAVE_DUE_TO_ZDO_LEAVE_MESSAGE | |
| EMBER_LEAVE_DUE_TO_ZLL_TOUCHLINK | |
| EMBER_LEAVE_DUE_TO_APP_EVENT_1 | |
EmberMulticastId#
typedef uint16_t EmberMulticastId
16-bit ZigBee network address.
16-bit ZigBee multicast group identifier.
EmberDutyCycleHectoPct#
typedef uint16_t EmberDutyCycleHectoPct
802.15.4 PAN ID.
The percent of duty cycle for a limit.
Duty cycle, limits, and thresholds are reported in units of percent * 100 (i.e., 10000 = 100.00%, 1 = 0.01%).
EMBER_RELEASE_TYPE_TO_STRING_STRUCT_DATA#
#define EMBER_RELEASE_TYPE_TO_STRING_STRUCT_DATAValue:
EmberReleaseTypeStruct Data that relates release type to the correct string.
EXTENDED_PAN_ID_SIZE#
#define EXTENDED_PAN_ID_SIZEValue:
8
Size of an extended PAN identifier in bytes (8).
EMBER_ENCRYPTION_KEY_SIZE#
#define EMBER_ENCRYPTION_KEY_SIZEValue:
16
Size of an encryption key in bytes (16).
EMBER_CERTIFICATE_SIZE#
#define EMBER_CERTIFICATE_SIZEValue:
48
Size of Implicit Certificates used for Certificate-based Key Exchange(CBKE).
EMBER_PUBLIC_KEY_SIZE#
#define EMBER_PUBLIC_KEY_SIZEValue:
22
Size of Public Keys used in Elliptical Cryptography ECMQV algorithms.
EMBER_PRIVATE_KEY_SIZE#
#define EMBER_PRIVATE_KEY_SIZEValue:
21
Size of Private Keys used in Elliptical Cryptography ECMQV algorithms.
EMBER_SMAC_SIZE#
#define EMBER_SMAC_SIZEValue:
16
Size of the SMAC used in Elliptical Cryptography ECMQV algorithms.
EMBER_SIGNATURE_SIZE#
#define EMBER_SIGNATURE_SIZEValue:
42
Size of the DSA signature used in Elliptical Cryptography Digital Signature Algorithms.
EMBER_AES_HASH_BLOCK_SIZE#
#define EMBER_AES_HASH_BLOCK_SIZEValue:
16
The size of AES-128 MMO hash is 16-bytes. This is defined in the core. ZigBee specification.
EMBER_CERTIFICATE_283K1_SIZE#
#define EMBER_CERTIFICATE_283K1_SIZEValue:
74
Size of Implicit Certificates used for Certificate Based Key Exchange using the ECC283K1 curve in bytes.
EMBER_PUBLIC_KEY_283K1_SIZE#
#define EMBER_PUBLIC_KEY_283K1_SIZEValue:
37
Size of Public Keys used in SECT283k1 Elliptical Cryptography ECMQV algorithms.
EMBER_PRIVATE_KEY_283K1_SIZE#
#define EMBER_PRIVATE_KEY_283K1_SIZEValue:
36
Size of Private Keys used SECT283k1 in Elliptical Cryptography ECMQV algorithms.
EMBER_SIGNATURE_283K1_SIZE#
#define EMBER_SIGNATURE_283K1_SIZEValue:
72
Size of the DSA signature used in SECT283k1 Elliptical Cryptography Digital Signature Algorithms.
NULL_BUFFER#
#define NULL_BUFFERValue:
0x0000u
EUI 64-bit ID (an IEEE address).
Incoming and outgoing messages are stored in buffers. These buffers are allocated and freed as needed.
Buffers are 32 bytes in length and can be linked together to hold longer messages.
See packet-buffer.h for APIs related to stack and linked buffers.
EMBER_MAX_802_15_4_CHANNEL_NUMBER#
#define EMBER_MAX_802_15_4_CHANNEL_NUMBERValue:
26
The maximum 802.15.4 channel number is 26.
EMBER_MIN_802_15_4_CHANNEL_NUMBER#
#define EMBER_MIN_802_15_4_CHANNEL_NUMBERValue:
11
The minimum 2.4GHz 802.15.4 channel number is 11.
EMBER_MIN_SUBGHZ_CHANNEL_NUMBER#
#define EMBER_MIN_SUBGHZ_CHANNEL_NUMBERValue:
0
The minimum SubGhz channel number is 0.
EMBER_ACTIVE_SCAN_DURATION#
#define EMBER_ACTIVE_SCAN_DURATIONValue:
3
ZigBee protocol specifies that active scans have a duration of 3 (138 msec). See documentation for emberStartScan in include/network-formation.h for more info on duration values.
EMBER_SUB_GHZ_SCAN_DURATION#
#define EMBER_SUB_GHZ_SCAN_DURATIONValue:
5
The SubGhz scan duration is 5.
EMBER_NUM_802_15_4_CHANNELS#
#define EMBER_NUM_802_15_4_CHANNELSValue:
(EMBER_MAX_802_15_4_CHANNEL_NUMBER - EMBER_MIN_802_15_4_CHANNEL_NUMBER + 1)
There are sixteen 802.15.4 channels.
EMBER_ALL_802_15_4_CHANNELS_MASK#
#define EMBER_ALL_802_15_4_CHANNELS_MASKValue:
0x07FFF800UL
A bitmask to scan all 2.4 GHz 802.15.4 channels.
EMBER_MAX_CHANNELS_PER_PAGE#
#define EMBER_MAX_CHANNELS_PER_PAGEValue:
27
The maximum channels per page are 27 page bits 31...27, channel bits 26...0.
EMBER_ALL_SUBGHZ_CHANNELS_MASK_FOR_PAGES_28_30_31#
#define EMBER_ALL_SUBGHZ_CHANNELS_MASK_FOR_PAGES_28_30_31Value:
0x07FFFFFFUL
Sub-GHz channel bitmasks for pages 28, 30, 31.
EMBER_MAX_SUBGHZ_CHANNEL_NUMBER_ON_PAGES_28_30_31#
#define EMBER_MAX_SUBGHZ_CHANNEL_NUMBER_ON_PAGES_28_30_31Value:
26
The maximum SubGhz channel number on pages 28, 30, 31 is 26.
EMBER_ALL_SUBGHZ_CHANNELS_MASK_FOR_PAGES_29#
#define EMBER_ALL_SUBGHZ_CHANNELS_MASK_FOR_PAGES_29Value:
0x1FF
SubGhz channel bitmasks for page 29.
EMBER_MAX_SUBGHZ_CHANNEL_NUMBER_ON_PAGE_29#
#define EMBER_MAX_SUBGHZ_CHANNEL_NUMBER_ON_PAGE_29Value:
8
The maximum SubGhz channel number on page 29 is 8.
EMBER_MIN_SUGBHZ_PAGE_NUMBER#
#define EMBER_MIN_SUGBHZ_PAGE_NUMBERValue:
28
The minimum SubGhz page number is 28.
EMBER_MAX_SUGBHZ_PAGE_NUMBER#
#define EMBER_MAX_SUGBHZ_PAGE_NUMBERValue:
31
The maximum SubGhz page number is 31.
EMBER_ALL_CHANNEL_PAGE_MASK#
#define EMBER_ALL_CHANNEL_PAGE_MASKValue:
0xF8000000UL
A bitmask for the channel page within a channel mask.
EMBER_PAGE_CHANNEL_MASK_FROM_CHANNEL_MASK#
#define EMBER_PAGE_CHANNEL_MASK_FROM_CHANNEL_MASKValue:
A page-channel mask for a given page and channel mask.
EMBER_PAGE_CHANNEL_MASK_FROM_CHANNEL_NUMBER#
#define EMBER_PAGE_CHANNEL_MASK_FROM_CHANNEL_NUMBERValue:
(page, channel)
A page-channel mask for a given page and channel.
EMBER_ZIGBEE_COORDINATOR_ADDRESS#
#define EMBER_ZIGBEE_COORDINATOR_ADDRESSValue:
0x0000u
The network ID of the coordinator in a ZigBee network is 0x0000.
EMBER_NULL_NODE_ID#
#define EMBER_NULL_NODE_IDValue:
0xFFFFu
A distinguished network ID that will never be assigned to any node. It is used to indicate the absence of a node ID.
EMBER_NO_CHANNEL_PAGE_IN_USE#
#define EMBER_NO_CHANNEL_PAGE_IN_USEValue:
0
The channel page value used to indicate just the 2.4GHz channels.
EMBER_NULL_EUI64#
#define EMBER_NULL_EUI64Value:
{ 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF }A distinguished EUI64 that is commonly used to indicate an invalid EUI64.
EMBER_NULL_BINDING#
#define EMBER_NULL_BINDINGValue:
0xFFu
A distinguished binding index used to indicate the absence of a binding.
EMBER_TABLE_ENTRY_UNUSED_NODE_ID#
#define EMBER_TABLE_ENTRY_UNUSED_NODE_IDValue:
0xFFFFu
A distinguished network ID that will never be assigned to any node.
This value is used when setting or getting the remote node ID in the address table or getting the remote node ID from the binding table. It indicates that the address or binding table entry is not in use.
EMBER_MULTICAST_NODE_ID#
#define EMBER_MULTICAST_NODE_IDValue:
0xFFFEu
A distinguished network ID that will never be assigned to any node. This value is returned when getting the remote node ID from the binding table and the given binding table index refers to a multicast binding entry.
EMBER_UNKNOWN_NODE_ID#
#define EMBER_UNKNOWN_NODE_IDValue:
0xFFFDu
A distinguished network ID that will never be assigned to any node. This value is used when getting the remote node ID from the address or binding tables. It indicates that the address or binding table entry is currently in use but the node ID corresponding to the EUI64 in the table is currently unknown.
EMBER_DISCOVERY_ACTIVE_NODE_ID#
#define EMBER_DISCOVERY_ACTIVE_NODE_IDValue:
0xFFFCu
A distinguished network ID that will never be assigned to any node. This value is used when getting the remote node ID from the address or binding tables. It indicates that the address or binding table entry is currently in use and network address discovery is underway.
EMBER_NULL_ADDRESS_TABLE_INDEX#
#define EMBER_NULL_ADDRESS_TABLE_INDEXValue:
0xFFu
A distinguished address table index used to indicate the absence of an address table entry.
EMBER_ZDO_ENDPOINT#
#define EMBER_ZDO_ENDPOINTValue:
0u
The endpoint where the ZigBee Device Object (ZDO) resides.
EMBER_BROADCAST_ENDPOINT#
#define EMBER_BROADCAST_ENDPOINTValue:
0xFFu
The broadcast endpoint, as defined in the ZigBee spec.
EMBER_ZDO_PROFILE_ID#
#define EMBER_ZDO_PROFILE_IDValue:
0x0000u
The profile ID used by the ZigBee Device Object (ZDO).
EMBER_WILDCARD_PROFILE_ID#
#define EMBER_WILDCARD_PROFILE_IDValue:
0xFFFFu
The profile ID used to address all the public profiles.
EMBER_MAXIMUM_STANDARD_PROFILE_ID#
#define EMBER_MAXIMUM_STANDARD_PROFILE_IDValue:
0x7FFFu
The maximum value for a profile ID in the standard profile range.
EMBER_BROADCAST_TABLE_TIMEOUT_QS#
#define EMBER_BROADCAST_TABLE_TIMEOUT_QSValue:
(20 * 4)
The broadcast table entry timeout, which specifies, in quarter seconds, how long an entry persists in the local device's broadcast table.
EMBER_DC_LIMIT_USE_DEFAULT#
#define EMBER_DC_LIMIT_USE_DEFAULTValue:
0
Use Ember's default duty cycle limit configurations.
ZigBee Broadcast Addresses Documentation#
EMBER_RX_ON_WHEN_IDLE_BROADCAST_ADDRESS#
#define EMBER_RX_ON_WHEN_IDLE_BROADCAST_ADDRESSValue:
0xFFFDu
Broadcast to all non-sleepy devices.
EMBER_SLEEPY_BROADCAST_ADDRESS#
#define EMBER_SLEEPY_BROADCAST_ADDRESSValue:
0xFFFFu
Broadcast to all devices, including sleepy end devices.
Ember Concentrator Types Documentation#
EMBER_LOW_RAM_CONCENTRATOR#
#define EMBER_LOW_RAM_CONCENTRATORValue:
0xFFF8u
A concentrator with insufficient memory to store source routes for the entire network. Route records are sent to the concentrator prior to every inbound APS unicast.
EMBER_HIGH_RAM_CONCENTRATOR#
#define EMBER_HIGH_RAM_CONCENTRATORValue:
0xFFF9u
A concentrator with sufficient memory to store source routes for the entire network. Remote nodes stop sending route records once the concentrator has successfully received one.
txPowerModes for emberSetTxPowerMode and mfglibSetPower Documentation#
EMBER_TX_POWER_MODE_DEFAULT#
#define EMBER_TX_POWER_MODE_DEFAULTValue:
0x0000
The application should call emberSetTxPowerMode() with the txPowerMode parameter set to this value to disable all power mode options, resulting in normal power mode and bi-directional RF transmitter output.
EMBER_TX_POWER_MODE_BOOST#
#define EMBER_TX_POWER_MODE_BOOSTValue:
0x0001
The application should call emberSetTxPowerMode() with the txPowerMode parameter set to this value to enable boost power mode.
EMBER_TX_POWER_MODE_ALTERNATE#
#define EMBER_TX_POWER_MODE_ALTERNATEValue:
0x0002
The application should call emberSetTxPowerMode() with the txPowerMode parameter set to this value to enable the alternate transmitter output.
EMBER_TX_POWER_MODE_BOOST_AND_ALTERNATE#
#define EMBER_TX_POWER_MODE_BOOST_AND_ALTERNATEValue:
The application should call emberSetTxPowerMode() with the txPowerMode parameter set to this value to enable both boost mode and the alternate transmitter output.
Counters Request Definitions Documentation#
EMBER_PRIVATE_PROFILE_ID#
#define EMBER_PRIVATE_PROFILE_IDValue:
0xC00Eu
This is a ZigBee application profile ID that has been assigned to Ember Corporation.
It is used to send for sending messages that have a specific, non-standard, interaction with the Ember stack. Its only current use is for stack counters requests.
EMBER_PRIVATE_PROFILE_ID_START#
#define EMBER_PRIVATE_PROFILE_ID_STARTValue:
0xC00Du
Ember's first private profile ID.
EMBER_PRIVATE_PROFILE_ID_END#
#define EMBER_PRIVATE_PROFILE_ID_ENDValue:
0xC016u
Ember's last private profile ID.
EMBER_REPORT_COUNTERS_REQUEST#
#define EMBER_REPORT_COUNTERS_REQUESTValue:
0x0003u
The cluster ID used to request that a node respond with a report of its Ember stack counters. See app/util/counters/counters-ota.h.
EMBER_REPORT_COUNTERS_RESPONSE#
#define EMBER_REPORT_COUNTERS_RESPONSEValue:
0x8003u
The cluster ID used to respond to an EMBER_REPORT_COUNTERS_REQUEST.
EMBER_REPORT_AND_CLEAR_COUNTERS_REQUEST#
#define EMBER_REPORT_AND_CLEAR_COUNTERS_REQUESTValue:
0x0004u
The cluster ID used to request that a node respond with a report of its Ember stack counters. The node will also reset its clusters to zero after a successful response. See app/util/counters/counters-ota.h.
EMBER_REPORT_AND_CLEAR_COUNTERS_RESPONSE#
#define EMBER_REPORT_AND_CLEAR_COUNTERS_RESPONSEValue:
0x8004u
The cluster ID used to respond to an EMBER_REPORT_AND_CLEAR_COUNTERS_REQUEST.
EMBER_OTA_CERTIFICATE_UPGRADE_CLUSTER#
#define EMBER_OTA_CERTIFICATE_UPGRADE_CLUSTERValue:
0x0005u
The cluster ID used to send and receive over the air certificate messages. This is used to field upgrade devices with Smart Energy Certificates and other security data.
ZDO response status. Documentation#
EmberZdoStatus#
EmberZdoStatus
| Enumerator | |
|---|---|
| EMBER_ZDP_SUCCESS | |
| EMBER_ZDP_INVALID_REQUEST_TYPE | |
| EMBER_ZDP_DEVICE_NOT_FOUND | |
| EMBER_ZDP_INVALID_ENDPOINT | |
| EMBER_ZDP_NOT_ACTIVE | |
| EMBER_ZDP_NOT_SUPPORTED | |
| EMBER_ZDP_TIMEOUT | |
| EMBER_ZDP_NO_MATCH | |
| EMBER_ZDP_NO_ENTRY | |
| EMBER_ZDP_NO_DESCRIPTOR | |
| EMBER_ZDP_INSUFFICIENT_SPACE | |
| EMBER_ZDP_NOT_PERMITTED | |
| EMBER_ZDP_TABLE_FULL | |
| EMBER_ZDP_NOT_AUTHORIZED | |
| EMBER_ZDP_DEVICE_BINDING_TABLE_FULL | |
| EMBER_ZDP_INVALID_INDEX | |
| EMBER_NWK_ALREADY_PRESENT | |
| EMBER_NWK_TABLE_FULL | |
| EMBER_NWK_UNKNOWN_DEVICE | |
Network and IEEE Address Request/Response Documentation#
Node Descriptor Request/Response Documentation#
Power Descriptor Request / Response Documentation#
Simple Descriptor Request / Response Documentation#
Active Endpoints Request / Response Documentation#
Match Descriptors Request / Response Documentation#
Discovery Cache Request / Response Documentation#
End Device Announce and End Device Announce Response Documentation#
System Server Discovery Request / Response Documentation#
Parent Announce and Parent Announce Response Documentation#
ZDO server mask bits Documentation#
EmberZdoServerMask#
EmberZdoServerMask
| Enumerator | |
|---|---|
| EMBER_ZDP_PRIMARY_TRUST_CENTER | |
| EMBER_ZDP_SECONDARY_TRUST_CENTER | |
| EMBER_ZDP_PRIMARY_BINDING_TABLE_CACHE | |
| EMBER_ZDP_SECONDARY_BINDING_TABLE_CACHE | |
| EMBER_ZDP_PRIMARY_DISCOVERY_CACHE | |
| EMBER_ZDP_SECONDARY_DISCOVERY_CACHE | |
| EMBER_ZDP_NETWORK_MANAGER | |
Find Node Cache Request / Response Documentation#
End Device Bind Request / Response Documentation#
Binding types and Request / Response Documentation#
LQI Table Request / Response Documentation#
Routing Table Request / Response Documentation#
Binding Table Request / Response Documentation#
Leave Request / Response Documentation#
Permit Joining Request / Response Documentation#
Network Update Request / Response Documentation#
Unsupported Documentation#
ZDO configuration flags. Documentation#
EmberZdoConfigurationFlags#
EmberZdoConfigurationFlags
| Enumerator | |
|---|---|
| EMBER_APP_RECEIVES_SUPPORTED_ZDO_REQUESTS | |
| EMBER_APP_HANDLES_UNSUPPORTED_ZDO_REQUESTS | |
| EMBER_APP_HANDLES_ZDO_ENDPOINT_REQUESTS | |
| EMBER_APP_HANDLES_ZDO_BINDING_REQUESTS | |
Enumeration Documentation#
EmberNodeType#
EmberNodeType
Defines the possible types of nodes and the roles that a node might play in a network.
| Enumerator | |
|---|---|
| EMBER_UNKNOWN_DEVICE | The device is not joined. |
| EMBER_COORDINATOR | Will relay messages and can act as a parent to other nodes. |
| EMBER_ROUTER | Will relay messages and can act as a parent to other nodes. |
| EMBER_END_DEVICE | Communicates only with its parent and will not relay messages. |
| EMBER_SLEEPY_END_DEVICE | An end device whose radio can be turned off to save power. The application must call emberPollForData() to receive messages. |
| EMBER_S2S_INITIATOR_DEVICE | Sleepy end device which transmits with wake up frames (CSL). |
| EMBER_S2S_TARGET_DEVICE | Sleepy end device which duty cycles the radio Rx (CSL). |
EmberEndDeviceConfiguration#
EmberEndDeviceConfiguration
The configuration advertised by the end device to the parent when joining/rejoining.
| Enumerator | |
|---|---|
| EMBER_END_DEVICE_CONFIG_NONE | |
| EMBER_END_DEVICE_CONFIG_PERSIST_DATA_ON_PARENT | |
EmberNetworkInitBitmask#
EmberNetworkInitBitmask
Defines the options that should be used when initializing the node's network configuration.
| Enumerator | |
|---|---|
| EMBER_NETWORK_INIT_NO_OPTIONS | |
| EMBER_NETWORK_INIT_PARENT_INFO_IN_TOKEN | The Parent Node ID and EUI64 are stored in a token. This prevents the need to perform an Orphan scan on startup. |
| EMBER_NETWORK_INIT_END_DEVICE_REJOIN_ON_REBOOT | Z3 compliant end devices on a network must send a rejoin request on reboot. |
EmberApsRejoinMode#
EmberApsRejoinMode
Options to allow/disallow rejoins using the default link key.
| Enumerator | |
|---|---|
| NO_REJOIN | |
| REJOIN_ANY_LINK_KEY | |
| REJOIN_NON_DEFAULT_LINK_KEY | |
EmberApsOption#
EmberApsOption
Options to use when sending a message.
The discover-route, APS-retry, and APS-indirect options may be used together. Poll response cannot be combined with any other options.
| Enumerator | |
|---|---|
| EMBER_APS_OPTION_NONE | No options. |
| EMBER_APS_OPTION_DSA_SIGN | This signs the application layer message body (APS Frame not included) and appends the ECDSA signature to the end of the message, which is needed by Smart Energy applications and requires the CBKE and ECC libraries. The emberDsaSignHandler() function is called after DSA signing is complete but before the message has been sent by the APS layer. Note that when passing a buffer to the stack for DSA signing, the final byte in the buffer has a special significance as an indicator of how many leading bytes should be ignored for signature purposes. See the API documentation of emberDsaSign() or the dsaSign EZSP command for more details about this requirement. |
| EMBER_APS_OPTION_ENCRYPTION | Send the message using APS Encryption using the Link Key shared with the destination node to encrypt the data at the APS Level. |
| EMBER_APS_OPTION_RETRY | Resend the message using the APS retry mechanism. This option and the enable route discovery option must be enabled for an existing route to be repaired automatically. |
| EMBER_APS_OPTION_ENABLE_ROUTE_DISCOVERY | Send the message with the NWK 'enable route discovery' flag, which causes a route discovery to be initiated if no route to the destination is known. Note that in the mesh stack, this option and the APS retry option must be enabled an existing route to be repaired automatically. |
| EMBER_APS_OPTION_FORCE_ROUTE_DISCOVERY | Send the message with the NWK 'force route discovery' flag, which causes a route discovery to be initiated even if one is known. |
| EMBER_APS_OPTION_SOURCE_EUI64 | Include the source EUI64 in the network frame. |
| EMBER_APS_OPTION_DESTINATION_EUI64 | Include the destination EUI64 in the network frame. |
| EMBER_APS_OPTION_ENABLE_ADDRESS_DISCOVERY | Send a ZDO request to discover the node ID of the destination if it is not already known. |
| EMBER_APS_OPTION_POLL_RESPONSE | This message is being sent in response to a call to emberPollHandler(). It causes the message to be sent immediately instead of being queued up until the next poll from the (end device) destination. |
| EMBER_APS_OPTION_ZDO_RESPONSE_REQUIRED | This incoming message is a valid ZDO request and the application is responsible for sending a ZDO response. This flag is used only within emberIncomingMessageHandler() when EMBER_APPLICATION_RECEIVES_UNSUPPORTED_ZDO_REQUESTS is defined. |
| EMBER_APS_OPTION_FRAGMENT | This message is part of a fragmented message. This option may only be set for unicasts. The groupId field gives the index of this fragment in the low-order byte. If the low-order byte is zero this is the first fragment and the high-order byte contains the number of fragments in the message. |
EmberIncomingMessageType#
EmberIncomingMessageType
Defines the possible incoming message types.
| Enumerator | |
|---|---|
| EMBER_INCOMING_UNICAST | Unicast. |
| EMBER_INCOMING_UNICAST_REPLY | Unicast reply. |
| EMBER_INCOMING_MULTICAST | Multicast. |
| EMBER_INCOMING_MULTICAST_LOOPBACK | Multicast sent by the local device. |
| EMBER_INCOMING_BROADCAST | Broadcast. |
| EMBER_INCOMING_BROADCAST_LOOPBACK | Broadcast sent by the local device. |
EmberOutgoingMessageType#
EmberOutgoingMessageType
Defines the possible outgoing message types.
| Enumerator | |
|---|---|
| EMBER_OUTGOING_DIRECT | Unicast sent directly to an EmberNodeId. |
| EMBER_OUTGOING_VIA_ADDRESS_TABLE | Unicast sent using an entry in the address table. |
| EMBER_OUTGOING_VIA_BINDING | Unicast sent using an entry in the binding table. |
| EMBER_OUTGOING_MULTICAST | Multicast message. This value is passed to emberMessageSentHandler() only. It may not be passed to emberSendUnicast(). |
| EMBER_OUTGOING_MULTICAST_WITH_ALIAS | An aliased multicast message. This value is passed to emberMessageSentHandler() only. It may not be passed to emberSendUnicast(). |
| EMBER_OUTGOING_BROADCAST_WITH_ALIAS | An aliased Broadcast message. This value is passed to emberMessageSentHandler() only. It may not be passed to emberSendUnicast(). |
| EMBER_OUTGOING_BROADCAST | A broadcast message. This value is passed to emberMessageSentHandler() only. It may not be passed to emberSendUnicast(). |
EmberZigbeeCommandType#
EmberZigbeeCommandType
A type of command received by the stack.
This enumeration indicates which protocol layer in the Ember stack an incoming command was meant for, or from which protocol layer an outgoing command is being sent.
| Enumerator | |
|---|---|
| EMBER_ZIGBEE_COMMAND_TYPE_RAW_MAC | Describes an 802.15.4 raw MAC message, unprocessed by the stack. |
| EMBER_ZIGBEE_COMMAND_TYPE_MAC_COMMAND | Describes an 802.15.4 MAC layer command. |
| EMBER_ZIGBEE_COMMAND_TYPE_NWK | Describes a ZigBee Network layer command. |
| EMBER_ZIGBEE_COMMAND_TYPE_APS | Describes a ZigBee Application Support layer command. |
| EMBER_ZIGBEE_COMMAND_TYPE_ZDO | Describes a ZigBee Device Object command. |
| EMBER_ZIGBEE_COMMAND_TYPE_ZCL | Describes a ZigBee Cluster Library command. |
| EMBER_ZIGBEE_COMMAND_TYPE_BEACON | Not a MAC command, but enumerated here for simplicity. |
EmberPacketAction#
EmberPacketAction
indication of the action taken on a packet
| Enumerator | |
|---|---|
| EMBER_DROP_PACKET | |
| EMBER_ACCEPT_PACKET | |
| EMBER_MANGLE_PACKET | |
| EMBER_ACCEPT_PACKET_OVERRIDE_SECURITY | This action allows unencrypted packets to pass through the stack. We only support this action in the network layer for now. WARNING: Using this packet handler action may have serious security implications |
| EMBER_ACCEPT_PACKET_SKIP_NWK_CRYPTO | This action allows unencrypted incoming packets to skip NWK decryption as well as outgoing packets to skip NWK encryption irrespective of the encryption flag in the NWK header. We only support this action in the network layer for now. |
EmberZigbeePacketType#
EmberZigbeePacketType
A type of packet received by the stack.
This enum provides a way to indicate which protocol layer in the Ember stack an incoming packet is meant for, or from which protocol layer an outgoing command is being sent from.
| Enumerator | |
|---|---|
| EMBER_ZIGBEE_PACKET_TYPE_RAW_MAC | Describes an 802.15.4 raw MAC message, unprocessed by the stack. |
| EMBER_ZIGBEE_PACKET_TYPE_MAC_COMMAND | Describes an 802.15.4 MAC layer command. |
| EMBER_ZIGBEE_PACKET_TYPE_NWK_DATA | Describes a ZigBee Network layer data message. |
| EMBER_ZIGBEE_PACKET_TYPE_NWK_COMMAND | Describes a ZigBee Network layer command. |
| EMBER_ZIGBEE_PACKET_TYPE_APS_DATA | Describes a ZigBee Application Support layer data message. |
| EMBER_ZIGBEE_PACKET_TYPE_APS_COMMAND | Describes a ZigBee Application Support layer command. |
| EMBER_ZIGBEE_PACKET_TYPE_ZDO | Describes a ZigBee Device Object command. |
| EMBER_ZIGBEE_PACKET_TYPE_ZCL | Describes a ZigBee Cluster Library command. |
| EMBER_ZIGBEE_PACKET_TYPE_BEACON | Distinguishing between raw MAC and beacons for simplicity |
| EMBER_ZIGBEE_PACKET_TYPE_INTERPAN | Describes a ZigBee Light Link message. |
| EMBER_ZIGBEE_PACKET_TYPE_NWK_DATA_PRE_DECRYPTION | Describes a ZigBee Network layer data message prior to (potential) decryption. |
| EMBER_ZIGBEE_PACKET_TYPE_NWK_COMMAND_PRE_DECRYPTION | Describes a ZigBee Network layer command prior to (potential) decryption. |
EmberNetworkStatus#
EmberNetworkStatus
Defines the possible join states for a node.
| Enumerator | |
|---|---|
| EMBER_NO_NETWORK | The node is not associated with a network in any way. |
| EMBER_JOINING_NETWORK | The node is currently attempting to join a network. |
| EMBER_JOINED_NETWORK | The node is joined to a network. |
| EMBER_JOINED_NETWORK_NO_PARENT | The node is an end device joined to a network but its parent is not responding. |
| EMBER_JOINED_NETWORK_S2S_INITIATOR | The node is a Sleepy-to-Sleepy initiator |
| EMBER_JOINED_NETWORK_S2S_TARGET | The node is a Sleepy-to-Sleepy target |
| EMBER_LEAVING_NETWORK | The node is in the process of leaving its current network. |
EmberNetworkScanType#
EmberNetworkScanType
Type for a network scan.
| Enumerator | |
|---|---|
| EMBER_ENERGY_SCAN | An energy scan scans each channel for its RSSI value. |
| EMBER_ACTIVE_SCAN | An active scan scans each channel for available networks. Use this scan type during network-steering to filter for beacons with available child capacity. The network found callback emberAfNetworkFoundCallback fires for all received beacons, while only beacons matching the capacity criteria and therefore viable for joining are cached |
| EMBER_START_RADIO_OFF_SCAN | A fake scan that is used to turn off the radio. |
| EMBER_STACK_GP_CHANNEL_DELIVERY_SCAN | A green power channel delivery scan. |
| EMBER_ACTIVE_SCAN_ROUTER | An active scan scans each channel for available networks. Use this scan type during network-steering to filter for and cache beacons with available router capacity - Note that this scan type temporarily sets nodeType to EMBER_ROUTER for the duration of the scan process. The network found callback emberAfNetworkFoundCallback fires for all received beacons, while only beacons matching the capacity criteria and therefore viable for joining are cached |
| EMBER_LAST_SCAN_TYPE | |
EmberBindingType#
EmberBindingType
Defines binding types.
| Enumerator | |
|---|---|
| EMBER_UNUSED_BINDING | A binding that is currently not in use. |
| EMBER_UNICAST_BINDING | A unicast binding whose 64-bit identifier is the destination EUI64. |
| EMBER_MANY_TO_ONE_BINDING | A unicast binding whose 64-bit identifier is the many-to-one destination EUI64. Route discovery should be disabled when sending unicasts via many-to-one bindings. |
| EMBER_MULTICAST_BINDING | A multicast binding whose 64-bit identifier is the group address. This binding can be used to send messages to the group and to receive messages sent to the group. |
EmberAssumeTrustCenterConcentratorType#
EmberAssumeTrustCenterConcentratorType
To configure non trust center node to assume a concentrator type of the trust center it join to, until it receive many-to-one route request from the trust center. For the trust center node, concentrator type is configured from the concentrator plugin. The stack by default assumes trust center be a low RAM concentrator that make other devices send route record to the trust center even without receiving a many-to-one route request. The assumed concentrator type can be changed by setting appropriate value to emberAssumedTrustCenterConcentratorType.
| Enumerator | |
|---|---|
| EMBER_ASSUME_TRUST_CENTER_IS_NOT_A_CONCENTRATOR | To assume trust center is not a concentrator. |
| EMBER_ASSUME_TRUST_CENTER_IS_LOW_RAM_CONCENTRATOR | To assume trust center is a low RAM concentrator. |
| EMBER_ASSUME_TRUST_CENTER_IS_HIGH_RAM_CONCENTRATOR | To assume trust center is a high RAM concentrator. |
EmberJoinDecision#
EmberJoinDecision
The decision made by the Trust Center when a node attempts to join.
| Enumerator | |
|---|---|
| EMBER_USE_PRECONFIGURED_KEY | Allow the node to join. The node has the key. |
| EMBER_SEND_KEY_IN_THE_CLEAR | Allow the node to join. Send the key to the node. |
| EMBER_DENY_JOIN | Deny join. |
| EMBER_NO_ACTION | Take no action. |
| EMBER_ALLOW_REJOINS_ONLY | Allow rejoins only. |
EmberDeviceUpdate#
EmberDeviceUpdate
The Status of the Update Device message sent to the Trust Center. The device may have joined or rejoined insecurely, rejoined securely, or left. MAC Security has been deprecated and therefore there is no secure join.
| Enumerator | |
|---|---|
| EMBER_STANDARD_SECURITY_SECURED_REJOIN | |
| EMBER_STANDARD_SECURITY_UNSECURED_JOIN | |
| EMBER_DEVICE_LEFT | |
| EMBER_STANDARD_SECURITY_UNSECURED_REJOIN | |
EmberRejoinReason#
EmberRejoinReason
Notes the last rejoin reason.
| Enumerator | |
|---|---|
| EMBER_REJOIN_REASON_NONE | |
| EMBER_REJOIN_DUE_TO_NWK_KEY_UPDATE | |
| EMBER_REJOIN_DUE_TO_LEAVE_MESSAGE | |
| EMBER_REJOIN_DUE_TO_NO_PARENT | |
| EMBER_REJOIN_DUE_TO_ZLL_TOUCHLINK | |
| EMBER_REJOIN_DUE_TO_END_DEVICE_REBOOT | |
| EMBER_REJOIN_DUE_TO_APP_EVENT_5 | |
| EMBER_REJOIN_DUE_TO_APP_EVENT_4 | |
| EMBER_REJOIN_DUE_TO_APP_EVENT_3 | |
| EMBER_REJOIN_DUE_TO_APP_EVENT_2 | |
| EMBER_REJOIN_DUE_TO_APP_EVENT_1 | |
EmberClusterListId#
EmberClusterListId
Defines the lists of clusters that must be provided for each endpoint.
| Enumerator | |
|---|---|
| EMBER_INPUT_CLUSTER_LIST | Input clusters the endpoint will accept. |
| EMBER_OUTPUT_CLUSTER_LIST | Output clusters the endpoint can send. |
EmberEventUnits#
EmberEventUnits
Either marks an event as inactive or specifies the units for the event execution time.
| Enumerator | |
|---|---|
| EMBER_EVENT_INACTIVE | The event is not scheduled to run. |
| EMBER_EVENT_MS_TIME | The execution time is in approximate milliseconds. |
| EMBER_EVENT_QS_TIME | The execution time is in 'binary' quarter seconds (256 approximate milliseconds each). |
| EMBER_EVENT_MINUTE_TIME | The execution time is in 'binary' minutes (65536 approximate milliseconds each). |
| EMBER_EVENT_ZERO_DELAY | The event is scheduled to run at the earliest opportunity. |
EmberJoinMethod#
EmberJoinMethod
The type of method used for joining.
| Enumerator | |
|---|---|
| EMBER_USE_MAC_ASSOCIATION | Devices normally use MAC association to join a network, which respects the "permit joining" flag in the MAC beacon. This value should be used by default. |
| EMBER_USE_NWK_REJOIN | For networks where the "permit joining" flag is never turned on, devices will need to use a ZigBee NWK Rejoin. This value causes the rejoin to be sent withOUT NWK security and the Trust Center will be asked to send the NWK key to the device. The NWK key sent to the device can be encrypted with the device's corresponding Trust Center link key. That is determined by the EmberJoinDecision on the Trust Center returned by the emberTrustCenterJoinHandler(). |
| EMBER_USE_NWK_REJOIN_HAVE_NWK_KEY | |
| EMBER_USE_CONFIGURED_NWK_STATE | For networks where all network and security information is known ahead of time, a router device may be commissioned such that it does not need to send any messages to begin communicating on the network. |
EmberCounterType#
EmberCounterType
Defines the events reported to the application by the emberCounterHandler().
| Enumerator | |
|---|---|
| EMBER_COUNTER_MAC_RX_BROADCAST | The MAC received a broadcast. |
| EMBER_COUNTER_MAC_TX_BROADCAST | The MAC transmitted a broadcast. |
| EMBER_COUNTER_MAC_RX_UNICAST | The MAC received a unicast. |
| EMBER_COUNTER_MAC_TX_UNICAST_SUCCESS | The MAC successfully transmitted a unicast. |
| EMBER_COUNTER_MAC_TX_UNICAST_RETRY | The MAC retried a unicast. This is a placeholder and is not used by the emberCounterHandler() callback. Instead, the number of MAC retries are returned in the data parameter of the callback for the |
| EMBER_COUNTER_MAC_TX_UNICAST_FAILED | The MAC unsuccessfully transmitted a unicast. |
| EMBER_COUNTER_APS_DATA_RX_BROADCAST | The APS layer received a data broadcast. |
| EMBER_COUNTER_APS_DATA_TX_BROADCAST | The APS layer transmitted a data broadcast. |
| EMBER_COUNTER_APS_DATA_RX_UNICAST | The APS layer received a data unicast. |
| EMBER_COUNTER_APS_DATA_TX_UNICAST_SUCCESS | The APS layer successfully transmitted a data unicast. |
| EMBER_COUNTER_APS_DATA_TX_UNICAST_RETRY | The APS layer retried a data unicast. This is a placeholder and is not used by the |
| EMBER_COUNTER_APS_DATA_TX_UNICAST_FAILED | The APS layer unsuccessfully transmitted a data unicast. |
| EMBER_COUNTER_ROUTE_DISCOVERY_INITIATED | The network layer successfully submitted a new route discovery to the MAC. |
| EMBER_COUNTER_NEIGHBOR_ADDED | An entry was added to the neighbor table. |
| EMBER_COUNTER_NEIGHBOR_REMOVED | An entry was removed from the neighbor table. |
| EMBER_COUNTER_NEIGHBOR_STALE | A neighbor table entry became stale because it had not been heard from. |
| EMBER_COUNTER_JOIN_INDICATION | A node joined or rejoined to the network via this node. |
| EMBER_COUNTER_CHILD_REMOVED | An entry was removed from the child table. |
| EMBER_COUNTER_ASH_OVERFLOW_ERROR | EZSP-UART only. An overflow error occurred in the UART. |
| EMBER_COUNTER_ASH_FRAMING_ERROR | EZSP-UART only. A framing error occurred in the UART. |
| EMBER_COUNTER_ASH_OVERRUN_ERROR | EZSP-UART only. An overrun error occurred in the UART. |
| EMBER_COUNTER_NWK_FRAME_COUNTER_FAILURE | A message was dropped at the Network layer because the NWK frame counter was not higher than the last message seen from that source. |
| EMBER_COUNTER_APS_FRAME_COUNTER_FAILURE | A message was dropped at the APS layer because the APS frame counter was not higher than the last message seen from that source. |
| EMBER_COUNTER_ASH_XOFF | EZSP-UART only. An XOFF was transmitted by the UART. |
| EMBER_COUNTER_APS_LINK_KEY_NOT_AUTHORIZED | An encrypted message was dropped by the APS layer because the sender's key has not been authenticated. As a result, the key is not authorized for use in APS data messages. |
| EMBER_COUNTER_NWK_DECRYPTION_FAILURE | A NWK encrypted message was received but dropped because decryption failed. |
| EMBER_COUNTER_APS_DECRYPTION_FAILURE | An APS encrypted message was received but dropped because decryption failed. |
| EMBER_COUNTER_ALLOCATE_PACKET_BUFFER_FAILURE | The number of failures to allocate a set of linked packet buffers. This doesn't necessarily mean that the packet buffer count was 0 at the time, but that the number requested was greater than the number free. |
| EMBER_COUNTER_RELAYED_UNICAST | The number of relayed unicast packets. |
| EMBER_COUNTER_PHY_TO_MAC_QUEUE_LIMIT_REACHED | The number of times a packet was dropped due to reaching the preset PHY-to-MAC queue limit (emMaxPhyToMacQueueLength). The limit will determine how many messages are accepted by the PHY between calls to emberTick(). After that limit is reached, packets will be dropped. The number of dropped packets will be recorded in this counter. NOTE: For each call to emberCounterHandler() there may be more than 1 packet that was dropped due to the limit reached. The actual number of packets dropped will be returned in the 'data' parameter passed to that function. |
| EMBER_COUNTER_PACKET_VALIDATE_LIBRARY_DROPPED_COUNT | The number of times a packet was dropped due to the packet-validate library checking a packet and rejecting it due to length or other formatting problems. |
| EMBER_COUNTER_TYPE_NWK_RETRY_OVERFLOW | The number of times the NWK retry queue is full and a new message failed to be added. |
| EMBER_COUNTER_PHY_CCA_FAIL_COUNT | The number of times the PHY layer was unable to transmit due to a failed CCA. |
| EMBER_COUNTER_BROADCAST_TABLE_FULL | The number of times a NWK broadcast was dropped because the broadcast table was full. |
| EMBER_COUNTER_PTA_LO_PRI_REQUESTED | The number of times a low-priority packet traffic arbitration request has been made. |
| EMBER_COUNTER_PTA_HI_PRI_REQUESTED | The number of times a high-priority packet traffic arbitration request has been made. |
| EMBER_COUNTER_PTA_LO_PRI_DENIED | The number of times a low-priority packet traffic arbitration request has been denied. |
| EMBER_COUNTER_PTA_HI_PRI_DENIED | The number of times a high-priority packet traffic arbitration request has been denied. |
| EMBER_COUNTER_PTA_LO_PRI_TX_ABORTED | The number of times a low-priority packet traffic arbitration transmission has been aborted. |
| EMBER_COUNTER_PTA_HI_PRI_TX_ABORTED | The number of times a high-priority packet traffic arbitration transmission has been aborted. |
| EMBER_COUNTER_ADDRESS_CONFLICT_SENT | The number of times an address conflict has caused node_id change, and an address conflict error is sent |
| EMBER_COUNTER_TYPE_COUNT | A placeholder giving the number of Ember counter types. |
EmberInitialSecurityBitmask#
EmberInitialSecurityBitmask
This is the Initial Security Bitmask that controls the use of various security features.
| Enumerator | |
|---|---|
| EMBER_DISTRIBUTED_TRUST_CENTER_MODE | Enables Distributed Trust Center Mode for the device forming the network. (Previously known as EMBER_NO_TRUST_CENTER_MODE) |
| EMBER_TRUST_CENTER_GLOBAL_LINK_KEY | Enables a Global Link Key for the Trust Center. All nodes will share the same Trust Center Link Key. |
| EMBER_PRECONFIGURED_NETWORK_KEY_MODE | Enables devices that perform MAC Association with a pre-configured Network Key to join the network. It is only set on the Trust Center. |
| EMBER_HAVE_TRUST_CENTER_EUI64 | This denotes that the EmberInitialSecurityState::preconfiguredTrustCenterEui64 has a value in it containing the trust center EUI64. The device will only join a network and accept commands from a trust center with that EUI64. Normally this bit is NOT set and the EUI64 of the trust center is learned during the join process. When commissioning a device to join onto an existing network that is using a trust center and without sending any messages, this bit must be set and the field EmberInitialSecurityState::preconfiguredTrustCenterEui64 must be populated with the appropriate EUI64. |
| EMBER_TRUST_CENTER_USES_HASHED_LINK_KEY | This denotes that the EmberInitialSecurityState::preconfiguredKey is not the actual Link Key but a Root Key known only to the Trust Center. It is hashed with the IEEE Address of the destination device to create the actual Link Key used in encryption. This is bit is only used by the Trust Center. The joining device need not set this. |
| EMBER_HAVE_PRECONFIGURED_KEY | This denotes that the EmberInitialSecurityState::preconfiguredKey element has valid data that should be used to configure the initial security state. |
| EMBER_HAVE_NETWORK_KEY | This denotes that the EmberInitialSecurityState::networkKey element has valid data that should be used to configure the initial security state. |
| EMBER_GET_LINK_KEY_WHEN_JOINING | This denotes to a joining node that it should attempt to acquire a Trust Center Link Key during joining. This is necessary if the device does not have a pre-configured key, or wants to obtain a new one (since it may be using a well-known key during joining). |
| EMBER_REQUIRE_ENCRYPTED_KEY | This denotes that a joining device should only accept an encrypted network key from the Trust Center (using its pre-configured key). A key sent in-the-clear by the Trust Center will be rejected and the join will fail. This option is only valid when using a pre-configured key. |
| EMBER_NO_FRAME_COUNTER_RESET | This denotes whether the device should NOT reset its outgoing frame counters (both NWK and APS) when emberSetInitialSecurityState() is called. Normally it is advised to reset the frame counter before joining a new network. However, when a device is joining to the same network again (but not using emberRejoinNetwork()), it should keep the NWK and APS frame counters stored in its tokens. NOTE: The application is allowed to dynamically change the behavior via EMBER_EXT_NO_FRAME_COUNTER_RESET field. |
| EMBER_GET_PRECONFIGURED_KEY_FROM_INSTALL_CODE | This denotes that the device should obtain its pre-configured key from an installation code stored in the manufacturing token. The token contains a value that will be hashed to obtain the actual pre-configured key. If that token is not valid, the call to emberSetInitialSecurityState() will fail. |
EmberExtendedSecurityBitmask#
EmberExtendedSecurityBitmask
This is the Extended Security Bitmask that controls the use of various extended security features.
| Enumerator | |
|---|---|
| EMBER_SECURE_NETWORK_KEY_ROTATION | This denotes that the network key update can only happen if the network key update request is unicast and encrypted i.e. broadcast network key update requests will not be processed if bit 1 is set |
| EMBER_JOINER_GLOBAL_LINK_KEY | This denotes whether a joiner node (router or end-device) uses a Global Link Key or a Unique Link Key. |
| EMBER_EXT_NO_FRAME_COUNTER_RESET | This denotes whether the device's outgoing frame counter is allowed to be reset during forming or joining. If the flag is set, the outgoing frame counter is not allowed to be reset. If the flag is not set, the frame counter is allowed to be reset. |
| EMBER_NWK_LEAVE_WITHOUT_REJOIN_NOT_ALLOWED | This denotes whether a device should discard or accept network leave without rejoin commands. |
| EMBER_NWK_LEAVE_REQUEST_NOT_ALLOWED | This denotes whether a router node should discard or accept network Leave Commands. |
EmberCurrentSecurityBitmask#
EmberCurrentSecurityBitmask
This is the Current Security Bitmask that details the use of various security features.
| Enumerator | |
|---|---|
| EMBER_STANDARD_SECURITY_MODE_ | This denotes that the device is running in a network with ZigBee Standard Security. |
| EMBER_DISTRIBUTED_TRUST_CENTER_MODE_ | This denotes that the device is running in a network without a centralized Trust Center. |
| EMBER_TRUST_CENTER_GLOBAL_LINK_KEY_ | This denotes that the device has a Global Link Key. The Trust Center Link Key is the same across multiple nodes. |
| EMBER_HAVE_TRUST_CENTER_LINK_KEY | This denotes that the node has a Trust Center Link Key. |
| EMBER_TRUST_CENTER_USES_HASHED_LINK_KEY_ | This denotes that the Trust Center is using a Hashed Link Key. |
EmberKeyStructBitmask#
EmberKeyStructBitmask
This bitmask describes the presence of fields within the EmberKeyStruct.
| Enumerator | |
|---|---|
| EMBER_KEY_HAS_SEQUENCE_NUMBER | This indicates that the key has a sequence number associated with it. (i.e., a Network Key). |
| EMBER_KEY_HAS_OUTGOING_FRAME_COUNTER | This indicates that the key has an outgoing frame counter and the corresponding value within the EmberKeyStruct has been populated. |
| EMBER_KEY_HAS_INCOMING_FRAME_COUNTER | This indicates that the key has an incoming frame counter and the corresponding value within the EmberKeyStruct has been populated. |
| EMBER_KEY_HAS_PARTNER_EUI64 | This indicates that the key has an associated Partner EUI64 address and the corresponding value within the EmberKeyStruct has been populated. |
| EMBER_KEY_IS_AUTHORIZED | This indicates the key is authorized for use in APS data messages. If the key is not authorized for use in APS data messages it has not yet gone through a key agreement protocol, such as CBKE (i.e., ECC). |
| EMBER_KEY_PARTNER_IS_SLEEPY | This indicates that the partner associated with the link is a sleepy end device. This bit is set automatically if the local device hears a device announce from the partner indicating it is not an 'RX on when idle' device. |
| EMBER_UNCONFIRMED_TRANSIENT_KEY | This indicates that the transient key which is being added is unconfirmed. This bit is set when we add a transient key while the EmberTcLinkKeyRequestPolicy is EMBER_ALLOW_TC_LINK_KEY_REQUEST_AND_GENERATE_NEW_KEY |
| EMBER_KEY_HAS_PSA_ID | This indicates that the actual key data is stored in PSA, and the respective PSA ID is recorded in the psa_id field. |
| EMBER_KEY_HAS_KEY_DATA | This indicates that the keyData field has valid data. On certain parts and depending on the security configuration, keys may live in secure storage and are not exportable. In such cases, keyData will not house the actual key contents. |
EmberKeyType#
EmberKeyType
This denotes the type of security key.
| Enumerator | |
|---|---|
| EMBER_TRUST_CENTER_LINK_KEY | This denotes that the key is a Trust Center Link Key. |
| EMBER_CURRENT_NETWORK_KEY | This denotes that the key is the Current Network Key. |
| EMBER_NEXT_NETWORK_KEY | This denotes that the key is the Next Network Key. |
| EMBER_APPLICATION_LINK_KEY | This denotes that the key is an Application Link Key. |
EmberKeyStatus#
EmberKeyStatus
This denotes the status of an attempt to establish a key with another device.
| Enumerator | |
|---|---|
| EMBER_KEY_STATUS_NONE | |
| EMBER_APP_LINK_KEY_ESTABLISHED | |
| EMBER_TRUST_CENTER_LINK_KEY_ESTABLISHED | |
| EMBER_KEY_ESTABLISHMENT_TIMEOUT | |
| EMBER_KEY_TABLE_FULL | |
| EMBER_TC_RESPONDED_TO_KEY_REQUEST | |
| EMBER_TC_APP_KEY_SENT_TO_REQUESTER | |
| EMBER_TC_RESPONSE_TO_KEY_REQUEST_FAILED | |
| EMBER_TC_REQUEST_KEY_TYPE_NOT_SUPPORTED | |
| EMBER_TC_NO_LINK_KEY_FOR_REQUESTER | |
| EMBER_TC_REQUESTER_EUI64_UNKNOWN | |
| EMBER_TC_RECEIVED_FIRST_APP_KEY_REQUEST | |
| EMBER_TC_TIMEOUT_WAITING_FOR_SECOND_APP_KEY_REQUEST | |
| EMBER_TC_NON_MATCHING_APP_KEY_REQUEST_RECEIVED | |
| EMBER_TC_FAILED_TO_SEND_APP_KEYS | |
| EMBER_TC_FAILED_TO_STORE_APP_KEY_REQUEST | |
| EMBER_TC_REJECTED_APP_KEY_REQUEST | |
| EMBER_TC_FAILED_TO_GENERATE_NEW_KEY | |
| EMBER_TC_FAILED_TO_SEND_TC_KEY | |
| EMBER_TRUST_CENTER_IS_PRE_R21 | |
| EMBER_TC_REQUESTER_VERIFY_KEY_TIMEOUT | |
| EMBER_TC_REQUESTER_VERIFY_KEY_FAILURE | |
| EMBER_TC_REQUESTER_VERIFY_KEY_SUCCESS | |
| EMBER_VERIFY_LINK_KEY_FAILURE | |
| EMBER_VERIFY_LINK_KEY_SUCCESS | |
EmberTcLinkKeyRequestPolicy#
EmberTcLinkKeyRequestPolicy
This enumeration determines whether or not a Trust Center answers trust center link key requests.
| Enumerator | |
|---|---|
| EMBER_DENY_TC_LINK_KEY_REQUESTS | |
| EMBER_ALLOW_TC_LINK_KEY_REQUEST_AND_SEND_CURRENT_KEY | |
| EMBER_ALLOW_TC_LINK_KEY_REQUEST_AND_GENERATE_NEW_KEY | |
EmberAppLinkKeyRequestPolicy#
EmberAppLinkKeyRequestPolicy
This enumeration determines whether or not a Trust Center answers app link key requests.
| Enumerator | |
|---|---|
| EMBER_DENY_APP_LINK_KEY_REQUESTS | |
| EMBER_ALLOW_APP_LINK_KEY_REQUEST | |
EmberKeySettings#
EmberKeySettings
| Enumerator | |
|---|---|
| EMBER_KEY_PERMISSIONS_NONE | |
| EMBER_KEY_PERMISSIONS_READING_ALLOWED | |
| EMBER_KEY_PERMISSIONS_HASHING_ALLOWED | |
EmberDutyCycleState#
EmberDutyCycleState
Duty cycle states.
Applications have no control over the state but the callback exposes state changes to the application.
| Enumerator | |
|---|---|
| EMBER_DUTY_CYCLE_TRACKING_OFF | No duty cycle tracking or metrics are taking place. |
| EMBER_DUTY_CYCLE_LBT_NORMAL | Duty Cycle is tracked and has not exceeded any thresholds. |
| EMBER_DUTY_CYCLE_LBT_LIMITED_THRESHOLD_REACHED | The limited threshold of the total duty cycle allotment was exceeded. |
| EMBER_DUTY_CYCLE_LBT_CRITICAL_THRESHOLD_REACHED | The critical threshold of the total duty cycle allotment was exceeded. |
| EMBER_DUTY_CYCLE_LBT_SUSPEND_LIMIT_REACHED | The suspend limit was reached and all outbound transmissions are blocked. |
EmberMacPassthroughType#
EmberMacPassthroughType
The types of MAC passthrough messages that an application may receive. This is a bitmask.
| Enumerator | |
|---|---|
| EMBER_MAC_PASSTHROUGH_NONE | No MAC passthrough messages. |
| EMBER_MAC_PASSTHROUGH_SE_INTERPAN | SE InterPAN messages. |
| EMBER_MAC_PASSTHROUGH_EMBERNET | EmberNet and first generation (v1) standalone bootloader messages. |
| EMBER_MAC_PASSTHROUGH_EMBERNET_SOURCE | EmberNet messages filtered by their source address. |
| EMBER_MAC_PASSTHROUGH_APPLICATION | Application-specific passthrough messages. |
| EMBER_MAC_PASSTHROUGH_CUSTOM | Custom inter-pan filter. |
EmberMultiPhyNwkConfig#
EmberMultiPhyNwkConfig
| Enumerator | |
|---|---|
| EMBER_MULTI_PHY_ROUTERS_ALLOWED | |
| EMBER_MULTI_PHY_BROADCASTS_ENABLED | |
| EMBER_MULTI_PHY_DISABLED | |
@0#
@0
| Enumerator | |
|---|---|
| PRIORITIZE_BEACONS_BASED_ON_PARENT_CLASSIFICATION | |
| PRIORITIZE_BEACONS_BASED_ON_TC_CONNECTVITY | |
| TC_CONNECTIVITY | |
| LONG_UPTIME | |
| BAD_PARENT_CONNECTIVITY | |
EmberEntropySource#
EmberEntropySource
Defines the entropy source used by the stack.
| Enumerator | |
|---|---|
| EMBER_ENTROPY_SOURCE_ERROR | |
| EMBER_ENTROPY_SOURCE_RADIO | |
| EMBER_ENTROPY_SOURCE_MBEDTLS_TRNG | |
| EMBER_ENTROPY_SOURCE_MBEDTLS | |
@1#
@1
| Enumerator | |
|---|---|
| EMBER_POLL_TIMEOUT_10_SECONDS | |
| EMBER_POLL_TIMEOUT_2_MINUTES | |
| EMBER_POLL_TIMEOUT_4_MINUTES | |
| EMBER_POLL_TIMEOUT_8_MINUTES | |
| EMBER_POLL_TIMEOUT_16_MINUTES | |
| EMBER_POLL_TIMEOUT_32_MINUTES | |
| EMBER_POLL_TIMEOUT_64_MINUTES | |
| EMBER_POLL_TIMEOUT_128_MINUTES | |
| EMBER_POLL_TIMEOUT_256_MINUTES | |
| EMBER_POLL_TIMEOUT_512_MINUTES | |
| EMBER_POLL_TIMEOUT_1024_MINUTES | |
| EMBER_POLL_TIMEOUT_2048_MINUTES | |
| EMBER_POLL_TIMEOUT_4096_MINUTES | |
| EMBER_POLL_TIMEOUT_8192_MINUTES | |
| EMBER_POLL_TIMEOUT_16384_MINUTES | |
EmberTcApsEncryptMode#
EmberTcApsEncryptMode
Defines the trust center APS encryption mode when sending a newer (alternate) network key to a device. The value settings below do not take effect when sending the initial network key during joining or rejoining.
| Enumerator | |
|---|---|
| TC_APS_ENCRYPT_DEFAULT | Default: don't encrypt broadcasts, encrypt unicasts |
| TC_APS_ENCRYPT_ENABLE | Encrypt both broadcasts and unicasts |
| TC_APS_ENCRYPT_DISABLE | Do not encrypt broadcasts and unicasts |
Typedef Documentation#
Function Documentation#
emberKeyContents#
uint8_t* emberKeyContents (EmberKeyData * key)
This function allows access to the actual key data bytes of the EmberKeyData structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberKeyData * | N/A | key | A pointer to an EmberKeyData structure. |
Returns
uint8_t* Returns a pointer to the first byte of the Key data.
emberCertificateContents#
uint8_t* emberCertificateContents (EmberCertificateData * cert)
Get access to the actual certificate data bytes of the EmberCertificateData structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberCertificateData * | N/A | cert | A pointer to an EmberCertificateData structure. |
Returns
uint8_t* Returns a pointer to the first byte of the certificate data.
emberPublicKeyContents#
uint8_t* emberPublicKeyContents (EmberPublicKeyData * key)
Get access to the actual public key data bytes of the EmberPublicKeyData structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberPublicKeyData * | N/A | key | A pointer to an EmberPublicKeyData structure. |
Returns
uint8_t* Returns a pointer to the first byte of the public key data.
emberPrivateKeyContents#
uint8_t* emberPrivateKeyContents (EmberPrivateKeyData * key)
Get access to the actual private key data bytes of the EmberPrivateKeyData structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberPrivateKeyData * | N/A | key | A pointer to an EmberPrivateKeyData structure. |
Returns
uint8_t* Returns a pointer to the first byte of the private key data.
emberSmacContents#
uint8_t* emberSmacContents (EmberSmacData * key)
Get access to the actual SMAC (Secured Message Authentication Code) data of the EmberSmacData structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberSmacData * | N/A | key |
emberSignatureContents#
uint8_t* emberSignatureContents (EmberSignatureData * sig)
Get access to the actual ECDSA signature data of the EmberSignatureData structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberSignatureData * | N/A | sig |
emberCertificate283k1Contents#
uint8_t* emberCertificate283k1Contents (EmberCertificate283k1Data * cert)
Get access to the actual certificate data bytes of the Ember283k1CertificateData structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberCertificate283k1Data * | N/A | cert | A pointer to an ::Ember283k1CertificateData structure. |
Returns
uint8_t* Returns a pointer to the first byte of the certificate data.
emberPublicKey283k1Contents#
uint8_t* emberPublicKey283k1Contents (EmberPublicKey283k1Data * key)
Get access to the actual public key data bytes of the Ember283k1PublicKeyData structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberPublicKey283k1Data * | N/A | key | A pointer to an Ember283k1PublicKeyData structure. |
Returns
uint8_t* Returns a pointer to the first byte of the public key data.
emberPrivateKey283k1Contents#
uint8_t* emberPrivateKey283k1Contents (EmberPrivateKey283k1Data * key)
Get access to the actual private key data bytes of the Ember283k1PrivateKeyData structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberPrivateKey283k1Data * | N/A | key | A pointer to an Ember283k1PrivateKeyData structure. |
Returns
uint8_t* Returns a pointer to the first byte of the private key data.
ember283k1SignatureContents#
uint8_t* ember283k1SignatureContents (EmberSignature283k1Data * sig)
Get access to the actual ECDSA signature data of the EmberSignature283k1Data structure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberSignature283k1Data * | N/A | sig |
Macro Definition Documentation#
emberIsZigbeeBroadcastAddress#
#define emberIsZigbeeBroadcastAddressValue:
(address)
Returns true if nodeId (short address) is a broadcast address.
EMBER_JOIN_DECISION_STRINGS#
#define EMBER_JOIN_DECISION_STRINGSValue:
@ brief Defines the CLI enumerations for the EmberJoinDecision enum.
EMBER_DEVICE_UPDATE_STRINGS#
#define EMBER_DEVICE_UPDATE_STRINGSValue:
@ brief Defines the CLI enumerations for the EmberDeviceUpdate enum.
EMBER_COUNTER_STRINGS#
#define EMBER_COUNTER_STRINGS
@ brief Defines the CLI enumerations for the EmberCounterType enum.
EMBER_STANDARD_SECURITY_MODE#
#define EMBER_STANDARD_SECURITY_MODEValue:
0x0000
This is an EmberInitialSecurityBitmask value but it does not actually set anything. It is the default mode used by the ZigBee Pro stack. It is defined here so that no legacy code is broken by referencing it.
EMBER_TRUST_CENTER_NODE_ID#
#define EMBER_TRUST_CENTER_NODE_IDValue:
0x0000u
The short address of the trust center. This address never changes dynamically.
EMBER_NO_TRUST_CENTER_MODE#
#define EMBER_NO_TRUST_CENTER_MODEValue:
EMBER_DISTRIBUTED_TRUST_CENTER_MODE
This is the legacy name for the Distributed Trust Center Mode.
EMBER_GLOBAL_LINK_KEY#
#define EMBER_GLOBAL_LINK_KEYValue:
EMBER_TRUST_CENTER_GLOBAL_LINK_KEY
This is the legacy name for the Trust Center Global Link Key.
EMBER_MFG_SECURITY_CONFIG_MAGIC_NUMBER#
#define EMBER_MFG_SECURITY_CONFIG_MAGIC_NUMBERValue:
0xCABAD11FUL
This magic number prevents accidentally changing the key settings. The emberSetMfgSecurityConfig() API will return EMBER_INVALID_CALL unless it is passed in.
EMBER_MAX_MAC_ONLY_COUNTERS#
#define EMBER_MAX_MAC_ONLY_COUNTERSValue:
33u
Defines the maximum number of counters that are specified as reporting either on 2.4 GHz or Sub-GHz.
PHY_INDEX_NATIVE#
#define PHY_INDEX_NATIVEValue:
0u
PHY index for 2.4 GHz radio interface, valid for simultaneous multi radio network.
PHY_INDEX_PRO2PLUS#
#define PHY_INDEX_PRO2PLUSValue:
1u
PHY index for Sub-GHz radio interface, valid for simultaneous multi radio network.