ZigBee Device Object (ZDO) functions not provided by the stack. See ZigBee Device Object (ZDO) Information for documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
EmberStatus emberNetworkAddressRequest(EmberEUI64 target,
bool reportKids,
uint8_t childStartIndex);
EmberStatus emberIeeeAddressRequest(EmberNodeId target,
bool reportKids,
uint8_t childStartIndex,
EmberApsOption options);
EmberStatus emberIeeeAddressRequestToTarget(EmberNodeId discoveryNodeId,
bool reportKids,
uint8_t childStartIndex,
EmberApsOption options,
EmberNodeId targetNodeIdOfRequest);
EmberStatus ezspMatchDescriptorsRequest(EmberNodeId target,
uint16_t profile,
uint8_t inCount,
uint8_t outCount,
uint16_t *inClusters,
uint16_t *outClusters,
EmberApsOption options);
EmberStatus ezspEndDeviceBindRequest(EmberNodeId localNodeId,
EmberEUI64 localEui64,
uint8_t endpoint,
uint16_t profile,
uint8_t inCount,
uint8_t outCount,
uint16_t *inClusters,
uint16_t *outClusters,
EmberApsOption options);
EmberNodeId ezspDecodeAddressResponse(uint8_t *response,
EmberEUI64 eui64Return);
Device Discovery Functions#
Request the 16 bit network address of a node whose EUI64 is known.
Request the EUI64 of a node whose 16 bit network address is known.
Service Discovery Functions#
Binding Manager Functions#
An end device bind request to the coordinator. If the coordinator receives a second end device bind request then a binding is created for every matching cluster.
Function to Decode Address Response Messages#
Extract the EUI64 and the node ID from an address response message.
Functions#
Device Discovery Functions Documentation#
emberNetworkAddressRequest#
EmberStatus emberNetworkAddressRequest (EmberEUI64 target, bool reportKids, uint8_t childStartIndex)
Request the 16 bit network address of a node whose EUI64 is known.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | target | The EUI64 of the node. |
| bool | N/A | reportKids | true to request that the target list their children in the response. |
| uint8_t | N/A | childStartIndex | The index of the first child to list in the response. Ignored if |
Returns
An EmberStatus value.
EMBER_SUCCESS - The request was transmitted successfully.
EMBER_NO_BUFFERS - Insufficient message buffers were available to construct the request.
EMBER_NETWORK_DOWN - The node is not part of a network.
EMBER_NETWORK_BUSY - Transmission of the request failed.
emberIeeeAddressRequest#
EmberStatus emberIeeeAddressRequest (EmberNodeId target, bool reportKids, uint8_t childStartIndex, EmberApsOption options)
Request the EUI64 of a node whose 16 bit network address is known.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | target | The network address of the node. |
| bool | N/A | reportKids | true to request that the target list their children in the response. |
| uint8_t | N/A | childStartIndex | The index of the first child to list in the response. Ignored if reportKids is false. |
| EmberApsOption | N/A | options | The options to use when sending the request. See emberSendUnicast() for a description. |
Returns
Service Discovery Functions Documentation#
ezspMatchDescriptorsRequest#
EmberStatus ezspMatchDescriptorsRequest (EmberNodeId target, uint16_t profile, uint8_t inCount, uint8_t outCount, uint16_t * inClusters, uint16_t * outClusters, EmberApsOption options)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | target | The node whose matching endpoints are desired. The request can be sent unicast or broadcast ONLY to the "RX-on-when-idle-address" (0xFFFD) If sent as a broadcast, any node that has matching endpoints will send a response. |
| uint16_t | N/A | profile | The application profile to match. |
| uint8_t | N/A | inCount | The number of input clusters. To not match any input clusters, set this value to 0. |
| uint8_t | N/A | outCount | The number of output clusters. To not match any output clusters, set this value to 0. |
| uint16_t * | N/A | inClusters | The list of input clusters. |
| uint16_t * | N/A | outClusters | The list of output clusters. |
| EmberApsOption | N/A | options | The options to use when sending the unicast request. See emberSendUnicast() for a description. This parameter is ignored if the target is a broadcast address. |
Request the specified node to send a list of its endpoints that match the specified application profile and, optionally, lists of input and/or output clusters.
Returns
An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Binding Manager Functions Documentation#
ezspEndDeviceBindRequest#
EmberStatus ezspEndDeviceBindRequest (EmberNodeId localNodeId, EmberEUI64 localEui64, uint8_t endpoint, uint16_t profile, uint8_t inCount, uint8_t outCount, uint16_t * inClusters, uint16_t * outClusters, EmberApsOption options)
An end device bind request to the coordinator. If the coordinator receives a second end device bind request then a binding is created for every matching cluster.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | localNodeId | The node ID of the local device. |
| EmberEUI64 | N/A | localEui64 | The EUI64 of the local device. |
| uint8_t | N/A | endpoint | The endpoint to be bound. |
| uint16_t | N/A | profile | The application profile of the endpoint. |
| uint8_t | N/A | inCount | The number of input clusters. |
| uint8_t | N/A | outCount | The number of output clusters. |
| uint16_t * | N/A | inClusters | The list of input clusters. |
| uint16_t * | N/A | outClusters | The list of output clusters. |
| EmberApsOption | N/A | options | The options to use when sending the request. See emberSendUnicast() for a description. |
Returns
An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Function to Decode Address Response Messages Documentation#
ezspDecodeAddressResponse#
EmberNodeId ezspDecodeAddressResponse (uint8_t * response, EmberEUI64 eui64Return)
Extract the EUI64 and the node ID from an address response message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | response | The received ZDO message with cluster ID NETWORK_ADDRESS_RESPONSE or IEEE_ADDRESS_RESPONSE. |
| EmberEUI64 | N/A | eui64Return | The EUI64 from the response is copied here. |
Returns
Returns the node ID from the response if the response status was EMBER_ZDP_SUCCESS. Otherwise, returns EMBER_NULL_NODE_ID.
Function Documentation#
emberIeeeAddressRequestToTarget#
EmberStatus emberIeeeAddressRequestToTarget (EmberNodeId discoveryNodeId, bool reportKids, uint8_t childStartIndex, EmberApsOption options, EmberNodeId targetNodeIdOfRequest)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | discoveryNodeId | |
| bool | N/A | reportKids | |
| uint8_t | N/A | childStartIndex | |
| EmberApsOption | N/A | options | |
| EmberNodeId | N/A | targetNodeIdOfRequest |