You are viewing documentation for version:
An in-memory representation of a ZigBee APS frame of an incoming or outgoing message. 
Public Attribute Documentation#
profileId#
uint16_t EmberApsFrame::profileId
The application profile ID that describes the format of the message. 
clusterId#
uint16_t EmberApsFrame::clusterId
The cluster ID for this message. 
sourceEndpoint#
uint8_t EmberApsFrame::sourceEndpoint
The source endpoint. 
destinationEndpoint#
uint8_t EmberApsFrame::destinationEndpoint
The destination endpoint. 
options#
EmberApsOption EmberApsFrame::options
A bitmask of options from the enumeration above. 
groupId#
uint16_t EmberApsFrame::groupId
The group ID for this message, if it is multicast mode. 
sequence#
uint8_t EmberApsFrame::sequence
The sequence number. 
radius#
uint8_t EmberApsFrame::radius