End Devices#

EmberZNet API relating to end device children.

See child.h for source code.

Power Management#

enum
@6 {
EMBER_OUTGOING_MESSAGES = 0x0001
EMBER_INCOMING_MESSAGES = 0x0002
EMBER_RADIO_IS_ON = 0x0004
EMBER_TRANSPORT_ACTIVE = 0x0008
EMBER_APS_LAYER_ACTIVE = 0x0010
EMBER_ASSOCIATING = 0x0020
EMBER_ZLL_TOUCH_LINKING = 0x0040
EMBER_NETWORK_TIMEOUT_REQUEST = 0x0200
EMBER_SEND_ORPHAN_NOTIFICATION = 0x0400
EMBER_MAC_DATA_POLL_SUPER_RETRY = 0x0800
}

Define tasks that are taken into account when dealing with sleep related behavior.

uint16_t

Return a bitmask indicating the stack's current tasks.

bool

Indicate whether the stack is currently in a state where there are no high-priority tasks, allowing the device to sleep.

bool

Indicate whether the parent token has been set by association.

bool

Indicate whether the stack currently has any tasks pending.

bool

Indicate whether the stack is currently in a state that does not require the application to periodically poll.

void

Immediately turn the radio power completely off.

void

Initialize the radio. Typically called coming out of deep sleep.

Send a link power delta request to the parent.

int8_t

Accessor function for recent average RSSI value between this device and the parent (SoC only).

EmberNodeId

Accessor function for the parent's node ID if applicable (SoC only).

: Bit mask that decides which timeout values are acceptable for a child. It defaults to 0xFFFF which covers all the following 15 options:

#define
EMBER_HIGH_PRIORITY_TASKS (EMBER_OUTGOING_MESSAGES | EMBER_INCOMING_MESSAGES | EMBER_RADIO_IS_ON)

A mask of the tasks that prevent a device from sleeping.

Functions#

int8_t
emberChildPower(uint8_t childIndex)

Return radio power value of the child from the given childIndex.

void
emberSetChildPower(uint8_t childIndex, int8_t newPower)

Set the radio power value for a given child index.

emberGetChildData(uint8_t index, EmberChildData *childData)

Get the EUI64 and node type of the child at the provided index. If there is no child at 'index', it returns EMBER_NOT_JOINED. Possible child indexes run from zero to emberMaxChildCount() - 1.

emberSetChildData(uint8_t index, EmberChildData *childData)

Sets the EUI64, node ID, and node type of the child at the provided index in nonvolatile memory. No other data from the childData argument is used or copied. The user is responsible for rebooting the device after calling this API in order to initialize RAM-based child data. Possible child indexes run from zero to emberMaxChildCount() - 1.

void
emberChildJoinHandler(uint8_t index, bool joining)

Called by the stack when a child joins or leaves. 'Joining' is true if the child is joining and false if leaving.

emberSetKeepAliveMode(EmberKeepAliveMode mode)

Request any pending data from the parent node. This function allows an end device to query its parent for any pending data.

void
emberSetMacPollFailureWaitTime(uint32_t waitBeforeRetryIntervalMs)
void
emberPollCompleteHandler(EmberStatus status)
emberSetMessageFlag(EmberNodeId childId)

Set a flag to indicate that a message is pending for a child. The next time that the child polls, it will be informed that it has a pending message. The message is sent from emberPollHandler, which is called when the child requests data.

emberClearMessageFlag(EmberNodeId childId)

Clear a flag to indicate that there are no more messages for a child. The next time the child polls, it will be informed that it does not have any pending messages.

void
emberPollHandler(EmberNodeId childId, bool transmitExpected)

Called to allow the application to send a message in response to a poll from a child.

emberAddChild(EmberNodeId shortId, EmberEUI64 longId, EmberNodeType nodeType)

Add a child to the child/neighbor table only on SoC, allowing direct manipulation of these tables by the application. This can affect the network functionality, and needs to be used wisely. If used appropriately, the application can maintain more than the maximum of children provided by the stack.

emberRemoveChild(EmberEUI64 childEui64)

Remove a node from child/neighbor table only on SoC, allowing direct manipulation of these tables by the application. This can affect the network functionality, and needs to be used wisely.

void
emberRemoveNeighbor(EmberNodeId shortId, EmberEUI64 longId)

Remove a neighbor from neighbor table only on SoC, allowing direct manipulation of neighbor table by the application. This can affect the network functionality, and needs to be used wisely.

uint8_t

Return the number of children the node currently has.

uint8_t

Return the number of router children that the node currently has.

uint8_t

Return the maximum number of children for this node. The return value is undefined for nodes that are not joined to a network.

uint8_t

Return the maximum number of router children for this node. The return value is undefined for nodes that are not joined to a network.

EmberNodeId

Return the parent's node ID. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).

EmberEUI64

Return the parent's EUI64. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).

Macros#

#define
emberChildId (childIndex)

Convert a child index to a node ID.

#define
emberChildIndex (childId)

Convert a node ID to a child index.

Power Management Documentation#

@6#

@6

Define tasks that are taken into account when dealing with sleep related behavior.

As opposed to its subset of EMBER_HIGH_PRIORITY_TASKS, these tasks do not necessarily prevent the device from going to sleep. However, they are taken into account when calculating how long we can sleep until the next event.

Enumerator
EMBER_OUTGOING_MESSAGES

Messages are waiting for transmission.

EMBER_INCOMING_MESSAGES

One or more incoming messages are being processed.

EMBER_RADIO_IS_ON

The radio is currently powered on. On sleepy devices, the radio is turned off when not in use. On non-sleepy devices (EMBER_COORDINATOR, EMBER_ROUTER, or EMBER_END_DEVICE), the radio is always on.

EMBER_TRANSPORT_ACTIVE

The transport layer has messages awaiting an ACK.

EMBER_APS_LAYER_ACTIVE

The ZigBee APS layer has messages awaiting an ACK.

EMBER_ASSOCIATING

The node is currently trying to associate with a ZigBee PRO network.

EMBER_ZLL_TOUCH_LINKING

The node is currently touch linking.

EMBER_NETWORK_TIMEOUT_REQUEST

Network Timeout Request Event.

EMBER_SEND_ORPHAN_NOTIFICATION

Sending Orphan Notification Event.

EMBER_MAC_DATA_POLL_SUPER_RETRY

MAC Data Poll Super Retry Event .


emberCurrentStackTasks#

uint16_t emberCurrentStackTasks (void )

Return a bitmask indicating the stack's current tasks.

Parameters
TypeDirectionArgument NameDescription
voidN/A

The mask EMBER_HIGH_PRIORITY_TASKS defines which tasks are high priority. Devices should not sleep if any high priority tasks are active. Active tasks that are not high priority are waiting for messages to arrive from other devices. If there are active tasks, but no high priority ones, the device may sleep but should periodically wake up and call emberPollForData() in order to receive messages. Parents will hold messages for EMBER_INDIRECT_TRANSMISSION_TIMEOUT milliseconds before discarding them.

Returns

  • A bitmask of the stack's active tasks.


emberOkToNap#

bool emberOkToNap (void )

Indicate whether the stack is currently in a state where there are no high-priority tasks, allowing the device to sleep.

Parameters
TypeDirectionArgument NameDescription
voidN/A

There may be tasks expecting incoming messages, in which case the device should periodically wake up and call emberPollForData() in order to receive messages. This function can only be called when the node type is EMBER_SLEEPY_END_DEVICE

Returns

  • True if the application may sleep but the stack may be expecting incoming messages.


emberParentTokenSet#

bool emberParentTokenSet (void )

Indicate whether the parent token has been set by association.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • True if the parent token has been set.


emberOkToHibernate#

bool emberOkToHibernate (void )

Indicate whether the stack currently has any tasks pending.

Parameters
TypeDirectionArgument NameDescription
voidN/A

If no tasks are pending, emberTick() does not need to be called until the next time a stack API function is called. This function can only be called when the node type is EMBER_SLEEPY_END_DEVICE or

Returns

  • True if the application may sleep for as long as it wishes.


emberOkToLongPoll#

bool emberOkToLongPoll (void )

Indicate whether the stack is currently in a state that does not require the application to periodically poll.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • True if the application may stop polling periodically.


emberStackPowerDown#

void emberStackPowerDown (void )

Immediately turn the radio power completely off.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Calling this function will render all other stack functions except emberStackPowerUp() non-functional until the radio is powered back on.


emberStackPowerUp#

void emberStackPowerUp (void )

Initialize the radio. Typically called coming out of deep sleep.

Parameters
TypeDirectionArgument NameDescription
voidN/A

For non-sleepy devices, also turns the radio on and leaves it in RX mode.


emberSendLinkPowerDeltaRequest#

EmberStatus emberSendLinkPowerDeltaRequest (void )

Send a link power delta request to the parent.

Parameters
TypeDirectionArgument NameDescription
voidN/A

emberGetAvgParentRssi#

int8_t emberGetAvgParentRssi (void )

Accessor function for recent average RSSI value between this device and the parent (SoC only).

Parameters
TypeDirectionArgument NameDescription
voidN/A

emberGetParentId#

EmberNodeId emberGetParentId (void )

Accessor function for the parent's node ID if applicable (SoC only).

Parameters
TypeDirectionArgument NameDescription
voidN/A

emberSetChildTimeoutOptionMask#

EmberStatus emberSetChildTimeoutOptionMask (uint16_t mask)

: Bit mask that decides which timeout values are acceptable for a child. It defaults to 0xFFFF which covers all the following 15 options:

Parameters
TypeDirectionArgument NameDescription
uint16_tN/Amask

#define SECONDS_10 0 #define MINUTES_2 1 #define MINUTES_4 2 #define MINUTES_8 3 #define MINUTES_16 4 #define MINUTES_32 5 #define MINUTES_64 6 #define MINUTES_128 7 #define MINUTES_256 8 #define MINUTES_512 9 #define MINUTES_1024 10 #define MINUTES_2048 11 #define MINUTES_4096 12 #define MINUTES_8192 13 #define MINUTES_16384 14 // ~11 days


Function Documentation#

emberChildPower#

int8_t emberChildPower (uint8_t childIndex)

Return radio power value of the child from the given childIndex.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/AchildIndex

The index.

Returns

  • The power of the child or maximum radio power, which is the power value provided by the user while forming/joining a network if there isn't a child at the childIndex specified.


emberSetChildPower#

void emberSetChildPower (uint8_t childIndex, int8_t newPower)

Set the radio power value for a given child index.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/AchildIndex

The index.

int8_tN/AnewPower

The new power value.


emberGetChildData#

EmberStatus emberGetChildData (uint8_t index, EmberChildData * childData)

Get the EUI64 and node type of the child at the provided index. If there is no child at 'index', it returns EMBER_NOT_JOINED. Possible child indexes run from zero to emberMaxChildCount() - 1.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex

The index of the child of interest.

EmberChildData *N/AchildData

The child's data is copied here.

Returns


emberSetChildData#

EmberStatus emberSetChildData (uint8_t index, EmberChildData * childData)

Sets the EUI64, node ID, and node type of the child at the provided index in nonvolatile memory. No other data from the childData argument is used or copied. The user is responsible for rebooting the device after calling this API in order to initialize RAM-based child data. Possible child indexes run from zero to emberMaxChildCount() - 1.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex

The index of the child.

EmberChildData *N/AchildData

The child's data.

Returns

Note

  • This API only sets the child data to nonvolatile memory. A reboot is required after calling this API to read the nonvolatile child data and set it to RAM structures. This API does not set other child RAM data, such as power and timeout values.


emberChildJoinHandler#

void emberChildJoinHandler (uint8_t index, bool joining)

Called by the stack when a child joins or leaves. 'Joining' is true if the child is joining and false if leaving.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex

The index of the child of interest.

boolN/Ajoining

True if the child is joining, false if the child is leaving.

The index is the same as the value that should be passed to emberGetChildData() to get this child's data. Note that if the child is leaving, emberGetChildData() will return EMBER_NOT_JOINED if called with this index. If the application includes emberChildJoinHandler(), it must define EMBER_APPLICATION_HAS_CHILD_JOIN_HANDLER in its CONFIGURATION_HEADER


emberSetKeepAliveMode#

EmberStatus emberSetKeepAliveMode (EmberKeepAliveMode mode)
Parameters
TypeDirectionArgument NameDescription
EmberKeepAliveModeN/Amode

One of the four configurations in the EmberKeepAliveMode.

@ brief Set the keep alive mode.


emberGetKeepAliveMode#

EmberKeepAliveMode emberGetKeepAliveMode (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

@ brief Get the keep alive mode.

Returns

  • mode One of the four configurations in the EmberKeepAliveMode.


emberPollForData#

EmberStatus emberPollForData (void )

Request any pending data from the parent node. This function allows an end device to query its parent for any pending data.

Parameters
TypeDirectionArgument NameDescription
voidN/A

End devices must call this function periodically to maintain contact with their parent. The parent will remove a child if it has not received a poll from it within the configured timeout.

If the end device has lost contact with its parent, emberPollForData() calls ::emberRejoinNetwork(true) and returns EMBER_ERR_FATAL.

The default values for the timeouts are set in config/ember-configuration-defaults.h and can be overridden in the application's configuration header.

Returns


emberSetMacPollFailureWaitTime#

void emberSetMacPollFailureWaitTime (uint32_t waitBeforeRetryIntervalMs)
Parameters
TypeDirectionArgument NameDescription
uint32_tN/AwaitBeforeRetryIntervalMs

Time in milliseconds the device waits before retrying a data poll when a MAC level data poll fails for any reason. The retry feature can be disabled by setting this value to zero.

@ brief Set the retry interval (in milliseconds) for mac data poll. This function is useful for sleepy end devices. The retry interval is the time in milliseconds the device waits before retrying a data poll when a MAC level data poll fails for any reason. The retry feature can be disabled by setting the retry interval to zero.


emberPollCompleteHandler#

void emberPollCompleteHandler (EmberStatus status)
Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Astatus

An EmberStatus value:

@ brief Called by the stack when a data poll to the parent is complete.

If the application includes emberPollCompleteHandler(), it must define EMBER_APPLICATION_HAS_POLL_COMPLETE_HANDLER within its CONFIGURATION_HEADER


emberSetMessageFlag#

EmberStatus emberSetMessageFlag (EmberNodeId childId)

Set a flag to indicate that a message is pending for a child. The next time that the child polls, it will be informed that it has a pending message. The message is sent from emberPollHandler, which is called when the child requests data.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AchildId

The ID of the child that just polled for data.

Returns


emberClearMessageFlag#

EmberStatus emberClearMessageFlag (EmberNodeId childId)

Clear a flag to indicate that there are no more messages for a child. The next time the child polls, it will be informed that it does not have any pending messages.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AchildId

The ID of the child that no longer has pending messages.

Returns

  • An EmberStatus value.

    • EMBER_SUCCESS - The next time that the child polls, it will be informed that it does not have any pending messages.

    • EMBER_NOT_JOINED - The child identified by childId is not our child.


emberPollHandler#

void emberPollHandler (EmberNodeId childId, bool transmitExpected)

Called to allow the application to send a message in response to a poll from a child.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AchildId

The ID of the child that is requesting data.

boolN/AtransmitExpected

True if the child is expecting an application- supplied data message. False otherwise.

This function is called when a child polls, provided that the pending message flag is set for that child (see emberSetMessageFlag(). The message should be sent to the child using emberSendUnicast() with the EMBER_APS_OPTION_POLL_RESPONSE option.

If the application includes ::emberPollHanlder(), it must define EMBER_APPLICATION_HAS_POLL_HANDLER in its CONFIGURATION_HEADER.


emberAddChild#

EmberStatus emberAddChild (EmberNodeId shortId, EmberEUI64 longId, EmberNodeType nodeType)

Add a child to the child/neighbor table only on SoC, allowing direct manipulation of these tables by the application. This can affect the network functionality, and needs to be used wisely. If used appropriately, the application can maintain more than the maximum of children provided by the stack.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AshortId

The preferred short ID of the node.

EmberEUI64N/AlongId

The long ID of the node.

EmberNodeTypeN/AnodeType

The nodetype e.g., EMBER_ROUTER defining, if this would be added to the child table or neighbor table.

Returns


emberRemoveChild#

EmberStatus emberRemoveChild (EmberEUI64 childEui64)

Remove a node from child/neighbor table only on SoC, allowing direct manipulation of these tables by the application. This can affect the network functionality, and needs to be used wisely.

Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/AchildEui64

The long ID of the node.

Returns


emberRemoveNeighbor#

void emberRemoveNeighbor (EmberNodeId shortId, EmberEUI64 longId)

Remove a neighbor from neighbor table only on SoC, allowing direct manipulation of neighbor table by the application. This can affect the network functionality, and needs to be used wisely.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AshortId

The short ID of the neighbor.

EmberEUI64N/AlongId

The long ID of the neighbor.


emberChildCount#

uint8_t emberChildCount (void )

Return the number of children the node currently has.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The number of children.


emberRouterChildCount#

uint8_t emberRouterChildCount (void )

Return the number of router children that the node currently has.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The number of router children.


emberMaxChildCount#

uint8_t emberMaxChildCount (void )

Return the maximum number of children for this node. The return value is undefined for nodes that are not joined to a network.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The maximum number of children.


emberMaxRouterChildCount#

uint8_t emberMaxRouterChildCount (void )

Return the maximum number of router children for this node. The return value is undefined for nodes that are not joined to a network.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The maximum number of router children.


emberGetParentNodeId#

EmberNodeId emberGetParentNodeId (void )

Return the parent's node ID. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The parent's node ID.


emberGetParentEui64#

EmberEUI64 emberGetParentEui64 (void )

Return the parent's EUI64. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The parent's EUI64.