Meter Mirror#

Callbacks for Meter Mirror Component.

Callbacks#

void
emberAfPluginMeterMirrorMirrorAddedCallback(const EmberEUI64 requestingDeviceIeeeAddress, uint8_t endpoint)

Mirror is added.

void
emberAfPluginMeterMirrorMirrorRemovedCallback(const EmberEUI64 requestingDeviceIeeeAddress, uint8_t endpoint)

Mirror is removed.

void

Reporting is complete.

Callbacks Documentation#

emberAfPluginMeterMirrorMirrorAddedCallback#

void emberAfPluginMeterMirrorMirrorAddedCallback (const EmberEUI64 requestingDeviceIeeeAddress, uint8_t endpoint)

Mirror is added.

Parameters
TypeDirectionArgument NameDescription
const EmberEUI64N/ArequestingDeviceIeeeAddress

Ver.: always

uint8_tN/Aendpoint

Ver.: always

This function is called by the Meter Mirror plugin whenever a RequestMirror command is successfully processed.


emberAfPluginMeterMirrorMirrorRemovedCallback#

void emberAfPluginMeterMirrorMirrorRemovedCallback (const EmberEUI64 requestingDeviceIeeeAddress, uint8_t endpoint)

Mirror is removed.

Parameters
TypeDirectionArgument NameDescription
const EmberEUI64N/ArequestingDeviceIeeeAddress

Ver.: always

uint8_tN/Aendpoint

Ver.: always

This function is called by the Meter Mirror plugin whenever a RemoveMirror command is successfully processed.


emberAfPluginMeterMirrorReportingCompleteCallback#

void emberAfPluginMeterMirrorReportingCompleteCallback (uint8_t endpoint)

Reporting is complete.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint

Ver.: always

This function is called by the Meter Mirror plugin after processing an AttributeReportingStatus attribute set to ReportingComplete. If the application needs to do any post attribute reporting processing, it can do it from within this callback.