Test Harness#

Callbacks for Test Harness Component.

Callbacks#

void
emberAfPluginTestHarnessWriteAttributesResponseCallback(EmberAfClusterId clusterId, uint8_t *buffer, uint16_t bufLen)

Write attributes response callback.

void
emberAfPluginTestHarnessReadAttributesResponseCallback(EmberAfClusterId clusterId, uint8_t *buffer, uint16_t bufLen)

Read attributes response callback.

Callbacks Documentation#

emberAfPluginTestHarnessWriteAttributesResponseCallback#

void emberAfPluginTestHarnessWriteAttributesResponseCallback (EmberAfClusterId clusterId, uint8_t * buffer, uint16_t bufLen)

Write attributes response callback.

Parameters
N/AclusterId

cluster ID

N/Abuffer

buffer

N/AbufLen

buffer length


Definition at line 117 of file app/framework/plugin/test-harness/test-harness.h

emberAfPluginTestHarnessReadAttributesResponseCallback#

void emberAfPluginTestHarnessReadAttributesResponseCallback (EmberAfClusterId clusterId, uint8_t * buffer, uint16_t bufLen)

Read attributes response callback.

Parameters
N/AclusterId

cluster ID

N/Abuffer

buffer

N/AbufLen

buffer length


Definition at line 128 of file app/framework/plugin/test-harness/test-harness.h