User-configurable stack memory allocation defaults.

Note

  • Application developers should not modify any portion of this file. Doing so may cause mysterious bugs. Allocations should be adjusted only by defining the appropriate macros in the application's CONFIGURATION_HEADER.

See Configuration for documentation.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
//  Todo:
//  - explain how to use a configuration header
//  - the documentation of the custom handlers should
//    go in config/ember-configuration.c, not here
//  - the stack profile documentation is out of date

#ifndef SILABS_EMBER_CONFIGURATION_DEFAULTS_H
#define SILABS_EMBER_CONFIGURATION_DEFAULTS_H

#ifdef CONFIGURATION_HEADER
  #include CONFIGURATION_HEADER
#endif

#ifdef SL_COMPONENT_CATALOG_PRESENT
#include "sl_component_catalog.h"
#endif

#if defined(SL_CATALOG_ZIGBEE_GREEN_POWER_PRESENT)
#include "sl_zigbee_green_power_config.h"
#endif

#if defined(SL_CATALOG_ZIGBEE_SECURITY_LINK_KEYS_PRESENT)
#include "sl_zigbee_security_link_keys_config.h"
#endif

#if defined(SL_CATALOG_ZIGBEE_SOURCE_ROUTE_PRESENT)
#include "sl_zigbee_source_route_config.h"
#endif

#if defined(SL_CATALOG_ZIGBEE_DEVICE_CONFIG_PRESENT)
#include "zigbee_device_config.h"
#endif

#if defined(SL_CATALOG_ZIGBEE_PRO_STACK_PRESENT)                         \
  || defined(SL_CATALOG_ZIGBEE_PRO_STACK_MAC_TEST_CMDS_PRESENT)          \
  || defined(SL_CATALOG_ZIGBEE_PRO_STACK_ALT_MAC_PRESENT)                \
  || defined(SL_CATALOG_ZIGBEE_PRO_STACK_NON_DEFAULT_MAC_PRESENT)        \
  || defined(SL_CATALOG_ZIGBEE_PRO_STACK_RAIL_MUX_PRESENT)               \
  || defined(SL_CATALOG_ZIGBEE_PRO_STACK_WITH_HIGH_DATARATE_PHY_PRESENT) \
  || defined(SL_CATALOG_ZIGBEE_PRO_ROUTER_STACK_PRESENT)                 \
  || defined(SL_CATALOG_ZIGBEE_PRO_STACK_WITH_HIGH_DATARATE_PHY_RAIL_MUX)
#include "sl_zigbee_pro_stack_config.h"
#elif defined(SL_CATALOG_ZIGBEE_PRO_LEAF_STACK_PRESENT)         \
  || defined(SL_CATALOG_ZIGBEE_PRO_LEAF_STACK_WITH_CSL_PRESENT) \
  || defined(SL_CATALOG_ZIGBEE_PRO_LEAF_STACK_MAC_TEST_CMDS_PRESENT)
#include "sl_zigbee_pro_leaf_stack_config.h"
#elif defined(EMBER_SCRIPTED_TEST) || defined(ZAPTEST) || defined(IMAGE_BUILDER) || defined(SLI_ZIGBEE_LIBRARY_BUILD) || defined(EZSP_HOST) || defined(RAIL_MAKE_TEST)
#else
#error "No stack configuration header included"
#endif

#if defined(SL_CATALOG_ZIGBEE_LIGHT_LINK_PRESENT)
#include "sl_zigbee_light_link_config.h"
#endif

#if defined(SL_CATALOG_ZIGBEE_NCP_CONFIGURATION_PRESENT)
#include "ncp-configuration-config.h"
#endif

#ifndef EMBER_API_MAJOR_VERSION
  #define EMBER_API_MAJOR_VERSION 2
#endif

#ifndef EMBER_API_MINOR_VERSION
  #define EMBER_API_MINOR_VERSION 0
#endif

#ifndef EMBER_STACK_PROFILE
  #define EMBER_STACK_PROFILE 0
#endif

#if (EMBER_STACK_PROFILE == 2)
#define EMBER_MAX_DEPTH                  15
#define EMBER_SECURITY_LEVEL              5
#define EMBER_MIN_DISCOVERY_TABLE_SIZE    4
#define EMBER_INDIRECT_TRANSMISSION_TIMEOUT 7680
#define EMBER_SEND_MULTICASTS_TO_SLEEPY_ADDRESS false
#ifndef EMBER_MIN_ROUTE_TABLE_SIZE // this value is set to zero on leaf stack
#define EMBER_MIN_ROUTE_TABLE_SIZE       10
#endif
#endif

#ifndef SL_ZIGBEE_STACK_COMPLIANCE_REVISION
  #define SL_ZIGBEE_STACK_COMPLIANCE_REVISION 22
#endif

#ifndef EMBER_MAX_END_DEVICE_CHILDREN
  #define EMBER_MAX_END_DEVICE_CHILDREN 6
#endif

#ifndef DOXYGEN_SHOULD_SKIP_THIS
/* Need to put in a compile time check to make sure that too many child devices
 * aren't specified.
 */

#if EMBER_MAX_END_DEVICE_CHILDREN > 64
  #error "EMBER_MAX_END_DEVICE_CHILDREN can not exceed 64."
#endif

#endif // DOXYGEN_SHOULD_SKIP_THIS

#ifndef EMBER_SECURITY_LEVEL
  #define EMBER_SECURITY_LEVEL 5
#endif

#if !(EMBER_SECURITY_LEVEL == 0 \
      || EMBER_SECURITY_LEVEL == 5)
  #error "Unsupported security level"
#endif

#ifdef EMBER_CHILD_TABLE_SIZE
  #if (EMBER_MAX_END_DEVICE_CHILDREN < EMBER_CHILD_TABLE_SIZE)
    #undef EMBER_CHILD_TABLE_SIZE
  #endif
#endif

#ifndef EMBER_CHILD_TABLE_SIZE
  #define EMBER_CHILD_TABLE_SIZE EMBER_MAX_END_DEVICE_CHILDREN
#endif

#ifndef EMBER_KEY_TABLE_SIZE
  #define EMBER_KEY_TABLE_SIZE 0
#endif

#ifndef EMBER_CERTIFICATE_TABLE_SIZE
  #define EMBER_CERTIFICATE_TABLE_SIZE 0
#else
  #if EMBER_CERTIFICATE_TABLE_SIZE > 1
    #error "EMBER_CERTIFICATE_TABLE_SIZE > 1 is not supported!"
  #endif
#endif

#ifndef EMBER_MAX_DEPTH
  #define EMBER_MAX_DEPTH                15
#elif (EMBER_MAX_DEPTH > 15)
// Depth is a 4-bit field
  #error "EMBER_MAX_DEPTH cannot be greater than 15"
#endif

#ifndef EMBER_MAX_HOPS
  #define EMBER_MAX_HOPS (2 * EMBER_MAX_DEPTH)
#endif

#ifndef EMBER_PACKET_BUFFER_COUNT
  #define EMBER_PACKET_BUFFER_COUNT 75
#endif
#ifndef EMBER_MAX_BEACONS_TO_STORE
// Packet buffers can be maxed out and we dont necessarily want to cache all those
// many beacons. Cap number of beacons to half the available buffers if they are  <= 75
// and set to a constant of 37 (~half of 75) otherwise
// 75 is the default count for EMBER_PACKET_BUFFER_COUNT, which is set to 255 for NCP
  #define EMBER_MAX_BEACONS_TO_STORE ( (EMBER_PACKET_BUFFER_COUNT <= 75) ? (EMBER_PACKET_BUFFER_COUNT >> 1) : 37)
#endif
#ifndef BEACON_STORAGE_TIMEOUT_MS
  #define BEACON_STORAGE_TIMEOUT_MS    (3 * 60 * 1000)  // 3 minutes
#endif
#define EMBER_MAX_NEIGHBOR_TABLE_SIZE 26
#ifndef EMBER_NEIGHBOR_TABLE_SIZE
  #define EMBER_NEIGHBOR_TABLE_SIZE 16
#endif
#if (EMBER_NEIGHBOR_TABLE_SIZE != EMBER_MAX_NEIGHBOR_TABLE_SIZE) && (EMBER_NEIGHBOR_TABLE_SIZE != 16) && (EMBER_NEIGHBOR_TABLE_SIZE != 1)
  #error "Unsupported neighbor table size is configured. Supported values are 1, 16 and 26."
#endif
#ifndef EMBER_INDIRECT_TRANSMISSION_TIMEOUT
  #define EMBER_INDIRECT_TRANSMISSION_TIMEOUT 3000
#endif
#define EMBER_MAX_INDIRECT_TRANSMISSION_TIMEOUT 30000
#if (EMBER_INDIRECT_TRANSMISSION_TIMEOUT \
     > EMBER_MAX_INDIRECT_TRANSMISSION_TIMEOUT)
  #error "Indirect transmission timeout too large."
#endif

#ifndef EMBER_SEND_MULTICASTS_TO_SLEEPY_ADDRESS
  #define EMBER_SEND_MULTICASTS_TO_SLEEPY_ADDRESS false
#endif

/* @brief End Device keep alive support mode
 */
#ifndef EMBER_END_DEVICE_KEEP_ALIVE_SUPPORT_MODE
  #define EMBER_END_DEVICE_KEEP_ALIVE_SUPPORT_MODE  EMBER_KEEP_ALIVE_SUPPORT_ALL
#endif

#define SECONDS_10              0
#define MINUTES_2               1
#define MINUTES_4               2
#define MINUTES_8               3
#define MINUTES_16              4
#define MINUTES_32              5
#define MINUTES_64              6
#define MINUTES_128             7
#define MINUTES_256             8
#define MINUTES_512             9
#define MINUTES_1024            10
#define MINUTES_2048            11
#define MINUTES_4096            12
#define MINUTES_8192            13
#define MINUTES_16384           14

#ifndef EMBER_END_DEVICE_POLL_TIMEOUT
  #define EMBER_END_DEVICE_POLL_TIMEOUT MINUTES_256
#endif

#ifndef EMBER_SHORT_CHILD_TIMEOUT
  #if (EMBER_END_DEVICE_POLL_TIMEOUT == SECONDS_10)
    #define EMBER_SHORT_CHILD_TIMEOUT SECONDS_10
  #else // (EMBER_END_DEVICE_POLL_TIMEOUT == SECONDS_10)
    #define EMBER_SHORT_CHILD_TIMEOUT MINUTES_2
  #endif // (EMBER_END_DEVICE_POLL_TIMEOUT == SECONDS_10)
#endif // EMBER_SHORT_CHILD_TIMEOUT

#ifndef EMBER_LINK_POWER_DELTA_INTERVAL
  #define EMBER_LINK_POWER_DELTA_INTERVAL 300
#endif
#ifndef EMBER_APS_UNICAST_MESSAGE_COUNT
  #define EMBER_APS_UNICAST_MESSAGE_COUNT 10
#endif

#ifndef SL_ZIGBEE_APS_DUPLICATE_REJECTION_MAX_ENTRIES
// NOTE a size of 1 is basically the same thing as no duplicate rejection
#define SL_ZIGBEE_APS_DUPLICATE_REJECTION_MAX_ENTRIES 5
#endif

#ifndef EMBER_BINDING_TABLE_SIZE
  #define EMBER_BINDING_TABLE_SIZE 0
#endif
#ifndef EMBER_ADDRESS_TABLE_SIZE
  #define EMBER_ADDRESS_TABLE_SIZE 8
#endif
#ifndef EMBER_ROUTE_TABLE_SIZE //in leaf stack this value is defined to be 0
    #define EMBER_ROUTE_TABLE_SIZE 16
#elif defined(EMBER_MIN_ROUTE_TABLE_SIZE) \
  && EMBER_ROUTE_TABLE_SIZE < EMBER_MIN_ROUTE_TABLE_SIZE
  #error "EMBER_ROUTE_TABLE_SIZE is less than required by stack profile."
#endif

#ifndef EMBER_DISCOVERY_TABLE_SIZE
  #ifdef EMBER_MIN_DISCOVERY_TABLE_SIZE
    #define EMBER_DISCOVERY_TABLE_SIZE EMBER_MIN_DISCOVERY_TABLE_SIZE
  #else
    #define EMBER_DISCOVERY_TABLE_SIZE 8
  #endif
#elif defined(EMBER_MIN_DISCOVERY_TABLE_SIZE) \
  && EMBER_DISCOVERY_TABLE_SIZE < EMBER_MIN_DISCOVERY_TABLE_SIZE
  #error "EMBER_DISCOVERY_TABLE_SIZE is less than required by stack profile."
#endif

#ifndef EMBER_MULTICAST_TABLE_SIZE
  #define EMBER_MULTICAST_TABLE_SIZE 8
#endif
#ifndef EMBER_SOURCE_ROUTE_TABLE_SIZE
  #define EMBER_SOURCE_ROUTE_TABLE_SIZE 0
#endif

#ifndef EMBER_MAX_SOURCE_ROUTE_RELAY_COUNT
  #define EMBER_MAX_SOURCE_ROUTE_RELAY_COUNT  11
#endif

/* The minimum broadcast table size per the Zigbee Pro spec is 9. */
#define EMBER_DEFAULT_BROADCAST_TABLE_SIZE 15

#ifndef EMBER_BROADCAST_TABLE_SIZE
  #define EMBER_BROADCAST_TABLE_SIZE EMBER_DEFAULT_BROADCAST_TABLE_SIZE
#elif EMBER_BROADCAST_TABLE_SIZE < EMBER_DEFAULT_BROADCAST_TABLE_SIZE
  #error "EMBER_BROADCAST_TABLE_SIZE is less than the minimum value of 15."
#elif 254 < EMBER_BROADCAST_TABLE_SIZE
  #error "EMBER_BROADCAST_TABLE_SIZE is larger than the maximum value of 254."
#endif

#ifndef EMBER_RETRY_QUEUE_SIZE
  #define EMBER_RETRY_QUEUE_SIZE 16
#endif

#ifndef EMBER_STORE_AND_FORWARD_QUEUE_SIZE
    #define EMBER_STORE_AND_FORWARD_QUEUE_SIZE 5
#endif

#if !defined(EMBER_ASSERT_OUTPUT_DISABLED) \
  && !defined(EMBER_ASSERT_SERIAL_PORT)
  #define EMBER_ASSERT_SERIAL_PORT 1
#endif

#ifndef EMBER_FRAGMENT_DELAY_MS
  #define EMBER_FRAGMENT_DELAY_MS 0
#endif

#define EMBER_FRAGMENT_MAX_WINDOW_SIZE 8

#ifndef EMBER_FRAGMENT_WINDOW_SIZE
  #define EMBER_FRAGMENT_WINDOW_SIZE 1
#elif EMBER_FRAGMENT_MAX_WINDOW_SIZE < EMBER_FRAGMENT_WINDOW_SIZE
  #error "EMBER_FRAGMENT_WINDOW_SIZE is too large."
#endif

#ifndef EMBER_REQUEST_KEY_TIMEOUT
  #define EMBER_REQUEST_KEY_TIMEOUT 0
#elif EMBER_REQUEST_KEY_TIMEOUT > 10
  #error "EMBER_REQUEST_KEY_TIMEOUT is too large."
#endif

#ifndef EMBER_TRANSIENT_KEY_TIMEOUT_S
  #define EMBER_TRANSIENT_KEY_TIMEOUT_S (300)
#endif

#ifndef EMBER_TRANSIENT_KEY_SESSION_TIMEOUT_VAL
  #define EMBER_TRANSIENT_KEY_SESSION_TIMEOUT_VAL 0xFFFF
#endif

#ifndef EMBER_PAN_ID_CONFLICT_REPORT_THRESHOLD
  #define EMBER_PAN_ID_CONFLICT_REPORT_THRESHOLD 2
#endif

#define EMBER_MAX_NETWORK_RETRIES 15
#ifndef EMBER_ZIGBEE_NUM_NETWORK_RETRIES_DEFAULT
  #define EMBER_ZIGBEE_NUM_NETWORK_RETRIES_DEFAULT 15
#endif
#if (EMBER_ZIGBEE_NUM_NETWORK_RETRIES_DEFAULT > EMBER_MAX_NETWORK_RETRIES)
  #error "Unsupported network retry attempts is configured. Supported values are 0..15"
#endif

#ifndef EMBER_TASK_COUNT
 #define EMBER_TASK_COUNT (5)
#endif

#define EMBER_MAX_SUPPORTED_NETWORKS 2
#ifdef UC_BUILD
#if (SLI_ZIGBEE_SECONDARY_NETWORK_ENABLED == 0)
#define EMBER_SUPPORTED_NETWORKS 1
#else
#define EMBER_SUPPORTED_NETWORKS 2
#endif
#if (defined(SL_CATALOG_ZIGBEE_NCP_FRAMEWORK_PRESENT) \
  && (defined(SL_CATALOG_ZIGBEE_MULTI_PAN_PRESENT) || defined(SL_CATALOG_ZIGBEE_MULTI_NETWORK_PRESENT)))
#undef EMBER_SUPPORTED_NETWORKS
#define EMBER_SUPPORTED_NETWORKS 2
#endif
#else // !UC_BUILD
#ifndef EMBER_SUPPORTED_NETWORKS
#ifdef EMBER_TEST
 #define EMBER_SUPPORTED_NETWORKS 2
#else
 #define EMBER_SUPPORTED_NETWORKS 1
#endif
#endif
#endif // UC_BUILD

#ifndef EMBER_ZLL_GROUP_ADDRESSES
  #define EMBER_ZLL_GROUP_ADDRESSES 1
#endif

#ifndef EMBER_ZLL_RSSI_THRESHOLD
  #define EMBER_ZLL_RSSI_THRESHOLD -128
#endif

#ifndef EMBER_GP_PROXY_TABLE_SIZE
  #define EMBER_GP_PROXY_TABLE_SIZE 5
#endif

#ifndef EMBER_GP_SINK_TABLE_SIZE
  #define EMBER_GP_SINK_TABLE_SIZE 0
#endif

#ifndef EMBER_GP_INCOMING_FC_TOKEN_TIMEOUT
#define EMBER_GP_INCOMING_FC_TOKEN_TIMEOUT 7 // between 0 seconds (never) to 60 seconds
#endif

#ifndef EMBER_GP_INCOMING_FC_TOKEN_TABLE_SIZE
#define EMBER_GP_INCOMING_FC_TOKEN_TABLE_SIZE 0 //EMBER_GP_PROXY_TABLE_SIZE
#endif

#ifndef EMBER_GP_INCOMING_FC_IN_SINK_TOKEN_TIMEOUT
#define EMBER_GP_INCOMING_FC_IN_SINK_TOKEN_TIMEOUT 7 // between 0 seconds (never) to 60 seconds
#endif

#ifndef EMBER_GP_INCOMING_FC_IN_SINK_TOKEN_TABLE_SIZE
#define EMBER_GP_INCOMING_FC_IN_SINK_TOKEN_TABLE_SIZE 0 //EMBER_GP_SINK_TABLE_SIZE
#endif

#define EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED 2
#if EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED > EMBER_SUPPORTED_NETWORKS
  #undef EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED
  #define EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED EMBER_SUPPORTED_NETWORKS
#endif

#ifdef UC_BUILD

#if (SLI_ZIGBEE_PRIMARY_NETWORK_DEVICE_TYPE == SLI_ZIGBEE_NETWORK_DEVICE_TYPE_COORDINATOR_OR_ROUTER \
     || SLI_ZIGBEE_PRIMARY_NETWORK_DEVICE_TYPE == SLI_ZIGBEE_NETWORK_DEVICE_TYPE_ROUTER)
// Primary network is coordinator or router
  #define NETWORK_0_ZC_AND_ZR_COUNT (1)
#else
// Primary network is end device
  #define NETWORK_0_ZC_AND_ZR_COUNT (0)
#endif

#if (SLI_ZIGBEE_SECONDARY_NETWORK_ENABLED > 0                                                             \
     && (SLI_ZIGBEE_SECONDARY_NETWORK_DEVICE_TYPE == SLI_ZIGBEE_NETWORK_DEVICE_TYPE_COORDINATOR_OR_ROUTER \
         || SLI_ZIGBEE_SECONDARY_NETWORK_DEVICE_TYPE == SLI_ZIGBEE_NETWORK_DEVICE_TYPE_ROUTER))
// Secondary network is coordinator or router
  #define NETWORK_1_ZC_AND_ZR_COUNT (1)
#else
// Secondary network not enabled or it is end device
  #define NETWORK_1_ZC_AND_ZR_COUNT (0)
#endif
// Handle the NCP Multi pan case and set the EMBER_ZC_AND_ZR_DEVICE_COUNT to 2
#if defined(SL_CATALOG_ZIGBEE_NCP_FRAMEWORK_PRESENT) && defined(SL_CATALOG_ZIGBEE_MULTI_PAN_PRESENT)
  #undef EMBER_ZC_AND_ZR_DEVICE_COUNT
  #define EMBER_ZC_AND_ZR_DEVICE_COUNT 2
#elif (defined(EMBER_NO_STACK) && !defined(EMBER_ZC_AND_ZR_DEVICE_COUNT))
// For no stack application such nodetest/sniffer.
#define EMBER_ZC_AND_ZR_DEVICE_COUNT (1)
#else
#define EMBER_ZC_AND_ZR_DEVICE_COUNT (NETWORK_0_ZC_AND_ZR_COUNT + NETWORK_1_ZC_AND_ZR_COUNT)
#endif

#if (EMBER_ZC_AND_ZR_DEVICE_COUNT > EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED)
  #error "Exceeded the maximum number of supported ZC and ZR devices."
#endif

#else // !UC_BUILD

#if defined(EMBER_AF_NCP) && defined(EMBER_AF_PLUGIN_MULTI_PAN_LIBRARY)
  #undef EMBER_AF_ZC_AND_ZR_DEVICE_COUNT    // ToDo: Remove #if part, would not need it with UC apps.
  #define EMBER_AF_ZC_AND_ZR_DEVICE_COUNT 2 // For Multi-PAN NCP
#elif defined(EMBER_NO_STACK) && !defined(EMBER_AF_ZC_AND_ZR_DEVICE_COUNT)
// For no stack application such nodetest/sniffer.
  #define EMBER_AF_ZC_AND_ZR_DEVICE_COUNT 1
#endif

#if (EMBER_AF_ZC_AND_ZR_DEVICE_COUNT > EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED)
  #error "Exceeded the maximum number of supported ZC and ZR devices."
#endif

#endif // UC_BUILD

// This table temporarily keeps track of devices that are joining
// To allow "n" devices to join simulataneously, this table needs to be capable of
// holding n entries. Since this space is only used when necessary and times out fairly
// quickly, we set it to 64 (same as max child table size) to prevent all the additional
// code to allow configuration of this table size
#ifndef SL_ZIGBEE_TRANSIENT_DEVICE_MGMT_MAX_CAPACITY
  #define SL_ZIGBEE_TRANSIENT_DEVICE_MGMT_MAX_CAPACITY 64
#endif

#ifndef SL_ZIGBEE_TRANSIENT_DEVICE_DEFAULT_TIMEOUT_MS
  #ifdef SL_CATALOG_ZIGBEE_DELAYED_JOIN_PRESENT
    #define SL_ZIGBEE_TRANSIENT_DEVICE_DEFAULT_TIMEOUT_MS (65535u)
    #define SL_ZIGBEE_TRANSIENT_DEVICE_MINIMUM_TIMEOUT_MS (10000u)
  #else
    #define SL_ZIGBEE_TRANSIENT_DEVICE_DEFAULT_TIMEOUT_MS (10000u)
  #endif
#endif

//Allows the aps acks for APSME commands to be turned off or on
//This should be "true" by default but to keep it consistend with the current stack behaviour this is "false" by default.
#ifndef SL_ZIGBEE_ENABLE_APS_ACKS_FOR_COMMANDS
  #define SL_ZIGBEE_ENABLE_APS_ACKS_FOR_COMMANDS (false)
#endif

#ifndef EMBER_CUSTOM_MAC_FILTER_TABLE_SIZE
  #define EMBER_CUSTOM_MAC_FILTER_TABLE_SIZE 2
#endif

#ifdef SL_CATALOG_RAIL_LIB_PRESENT
  #include "rail_ieee802154.h"
  #ifndef EMBER_RADIO_802154_CCA_MODE
    #define EMBER_RADIO_802154_CCA_MODE RAIL_IEEE802154_CCA_MODE_RSSI
  #endif // EMBER_RADIO_802154_CCA_MODE
#endif // SL_CATALOG_RAIL_LIB_PRESENT

#ifdef EMBER_TEST
  #undef EMBER_RADIO_802154_CCA_MODE
  #define EMBER_RADIO_802154_CCA_MODE 0
#endif

#ifndef SL_ZIGBEE_ZDO_BEACON_SURVEY_MAX_UNIQUE_NETWORKS
  #define SL_ZIGBEE_ZDO_BEACON_SURVEY_MAX_UNIQUE_NETWORKS 8
#endif

#endif //__EMBER_CONFIGURATION_DEFAULTS_H__

Macros#

#define

The major version number of the Ember stack release that the application is built against.

#define

The minor version number of the Ember stack release that the application is built against.

#define

Specify the stack profile. The default is Profile 0.

#define

The maximum number of end device children that a router will support.

#define

The security level used for security at the MAC and network layers. The supported values are 0 (no security) and 5 (payload is encrypted and a four-byte MIC is used for authentication).

#define
EMBER_CHILD_TABLE_SIZE EMBER_MAX_END_DEVICE_CHILDREN

The maximum number of children that a node may have.

#define

The maximum number of link and master keys that a node can store, not including the Trust Center Link Key. The stack maintains special storage for the Trust Center Link Key.

#define

The number of entries for the field upgradeable certificate table. Normally, certificates, such as SE certs, are stored in the runtime-unmodifiable MFG area. However, those devices wishing to add new certificates after manufacturing will have to use the normal token space. This defines the size of that table. For most devices 0 is appropriate since there is no need to change certificates in the field. For those wishing to field upgrade devices with new certificates, 1 is the correct size. Anything more is wasting SimEEPROM.

#define

The maximum depth of the tree in ZigBee 2006. This implicitly determines the maximum diameter of the network (EMBER_MAX_HOPS) if that value is not overridden.

#define
EMBER_MAX_HOPS (2 * EMBER_MAX_DEPTH)

The maximum number of hops for a message.

#define

The number of Packet Buffers available to the Stack. The default is 75.

#define
EMBER_MAX_BEACONS_TO_STORE ( (EMBER_PACKET_BUFFER_COUNT <= 75) ? (EMBER_PACKET_BUFFER_COUNT >> 1) : 37)

The maximum number of beacons to record when performing an active scan to find networks. Legacy APIs such as emberJoinNetwork and the several emberFindAndRejoinNetwork APIs set the number of beacons to record to 1, while the Network Steering plugin will attempt to record the maximum number of beacons.

#define

The amount of time after which any caches beacons are purged from the cache in RAM. Each beacon stored consumes one packet buffer. The timeout for beacons begins once the first beacon is added to the cache.

#define

The maximum number of router neighbors the stack can keep track of.

#define

The maximum amount of time (in milliseconds) that the MAC will hold a message for indirect transmission to a child.

#define

Define the behavior for the address that the multicasts are sent to. The normal address is RxOnWhenIdle=true (0xFFFD). However, setting this to true can change locally generated multicasts to be sent to the sleepy broadcast address (0xFFFF). Changing the default is NOT Zigbee Pro compliant and may not be inter-operable.

#define
EMBER_END_DEVICE_KEEP_ALIVE_SUPPORT_MODE EMBER_KEEP_ALIVE_SUPPORT_ALL
#define

The default index into the R21 Child Aging timeout The default value is a timeout of 256 minutes.

#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define

The temporary, short timeout that is given to a joining or insecurely rejoining child. The child is expected to send a network encrypted packet to set its timeout to the default value.

#define

The maximum number of APS retried messages that the stack can transmit at any time. Here, transmitting describes the time between the call to emberSendUnicast() and the subsequent callback to emberMessageSentHandler().

#define

Size of 1 is basically the same thing as no duplicate rejection.

#define

The maximum number of bindings supported by the stack. The default is 0 bindings. Each binding consumes 2 bytes of RAM.

#define

The maximum number of EUI64<->network address associations that the stack can maintain. The default value is 8.

#define

The maximum number of destinations to which a node can route messages. This include both messages originating at this node and those relayed for others. The default value is 16.

#define

The number of simultaneous route discoveries that a node will support.

#define

The maximum number of multicast groups that the device may be a member of. The default value is 8.

#define

The number of source route table entries if the source route library is not included. The maximum source route table size is 255 entries, since a one-byte index is used, and the index 0xFF is reserved. The default value is 0.

#define

The maximum number of broadcasts during a single broadcast timeout period. The minimum and default value is 15 and can only be changed on compatible Ember stacks. Be very careful when changing the broadcast table size as it affects timing of the broadcasts and the number of possible broadcasts. Additionally, this value must be universal for all devices in the network. Otherwise, a single router can overwhelm all its neighbors with more broadcasts than they can support. In general, this value should be left alone.

#define
EMBER_BROADCAST_TABLE_SIZE EMBER_DEFAULT_BROADCAST_TABLE_SIZE
#define

Settings to control if and where assert information will be printed.

#define

The time the stack will wait (in milliseconds) between sending blocks of a fragmented message. The default value is 0.

#define

The maximum number of blocks of a fragmented message that can be sent in a single window is defined to be 8.

#define

The number of blocks of a fragmented message that can be sent in a single window. The maximum is EMBER_FRAGMENT_MAX_WINDOW_SIZE. The default value is 1.

#define

The length of time that the device will wait for an answer to its Application Key Request. For the Trust Center, this is the time it will hold the first request and wait for a second matching request. If both arrive within this time period, the Trust Center will reply to both with the new key. If both requests are not received, the Trust Center will discard the request. The time is in minutes, with the maximum time being 10 minutes. A value of 0 minutes indicates that the Trust Center will not buffer the request but instead respond immediately. Only 1 outstanding request is supported at a time.

#define

The length of time, in seconds, that a trust center will store a transient link key that a device can use to join its network. A transient key is added with a call to sl_zb_sec_man_import_transient_key. After the transient key is added, it will be removed once this amount of time has passed. A joining device will not be able to use that key to join until it is added again on the trust center. The default value is 300 seconds, i.e., 5 minutes.

#define

A reserved emberTransientKeyTimeoutS value that, when stored with a "transient" key, prevents its removal from the transient key table when the session is active. Note that some standard security procedures (e.g. Zigbee Direct) require session keys to remain active indefinitely for the duration of the of the exchange.

#define

The number of PAN ID conflict reports that must be received by the network manager within one minute to trigger a PAN ID change. Very rarely, a corrupt beacon can pass the CRC check and trigger a false PAN id conflict. This is more likely to happen in very large dense networks. Setting this value to 2 or 3 dramatically reduces the chances of a spurious PAN ID change. The maximum value is 63. The default value is 2.

#define

The number of network level retries before network layer gives up sending a message, and return with an error. This could be seen as an extension to mac retries, and can take a range between 0..15. Setting the value to 0 disables network retries.

#define

The number of event tasks that can be tracked for the purpose of processor idling. The Ember Zigbee Pro Stack requires two tasks, an application and associated libraries may use additional tasks, though typically no more than 5 are needed for most applications.

#define

The number of networks supported by the stack.

#define

The number of unique group identifiers that this device requires.

#define

The RSSI threshold applied to incoming scan requests.

#define

The number of proxy table entries supported.

#define

The number of sink table entries supported.

#define

The timeout (seconds) to restore the GPD incoming security frame counter in the Flash (0 being never).

#define

The maximum table size to restore the GPD incoming security frame counter in the Flash (being either 0 or EMBER_GP_PROXY_TABLE_SIZE).

#define

The timeout (seconds) to restore the GPD incoming security frame counter in the Flash (0 being never).

#define

The maximum table size to restore the GPD incoming security frame counter in the Flash (being either 0 or EMBER_GP_SINK_TABLE_SIZE).

#define

The maximum number of ZC and ZR devices can be supported in a multi network mode. All the ZC and ZR devices are expected to be on the same channel with different PAN IDs. Multi network with multiple ZC and ZR devices are supported only on EFR platform.

#define

The maximum number of ZC and ZR devices can be supported in a multi network mode. All the ZC and ZR devices are expected to be on the same channel with different PAN IDs. Multi network with multiple ZC and ZR devices are supported only on EFR platform.

#define

The number of ZC and ZR device types are present in the application. This configuration is used to expand the various stack tables and events required to support the multi PAN application. Note that for SoC, this define is generated by app builder based on the device type(s) present in the application.

#define
EMBER_ZC_AND_ZR_DEVICE_COUNT (NETWORK_0_ZC_AND_ZR_COUNT + NETWORK_1_ZC_AND_ZR_COUNT)
#define

The 802.15.4 CCA mode that should be used at startup. The default value is RAIL_IEEE802154_CCA_MODE_RSSI. This value is configured in the radio during initialization. The user may override this value at runtime using emberSetRadioIeee802154CcaMode.

Macro Definition Documentation#

EMBER_API_MAJOR_VERSION#

#define EMBER_API_MAJOR_VERSION
Value:
2

The major version number of the Ember stack release that the application is built against.


Definition at line 115 of file stack/config/ember-configuration-defaults.h

EMBER_API_MINOR_VERSION#

#define EMBER_API_MINOR_VERSION
Value:
0

The minor version number of the Ember stack release that the application is built against.


Definition at line 122 of file stack/config/ember-configuration-defaults.h

EMBER_STACK_PROFILE#

#define EMBER_STACK_PROFILE
Value:
0

Specify the stack profile. The default is Profile 0.

You can set this to Profile 1 (Zigbee) or Profile 2 (Zigbee Pro) in your application's configuration header (.h) file using:

#define EMBER_STACK_PROFILE 1

or

#define EMBER_STACK_PROFILE 2

Definition at line 138 of file stack/config/ember-configuration-defaults.h

SL_ZIGBEE_STACK_COMPLIANCE_REVISION#

#define SL_ZIGBEE_STACK_COMPLIANCE_REVISION
Value:
22

Definition at line 153 of file stack/config/ember-configuration-defaults.h

EMBER_MAX_END_DEVICE_CHILDREN#

#define EMBER_MAX_END_DEVICE_CHILDREN
Value:
6

The maximum number of end device children that a router will support.


Definition at line 159 of file stack/config/ember-configuration-defaults.h

EMBER_SECURITY_LEVEL#

#define EMBER_SECURITY_LEVEL
Value:
5

The security level used for security at the MAC and network layers. The supported values are 0 (no security) and 5 (payload is encrypted and a four-byte MIC is used for authentication).


Definition at line 178 of file stack/config/ember-configuration-defaults.h

EMBER_CHILD_TABLE_SIZE#

#define EMBER_CHILD_TABLE_SIZE
Value:
EMBER_MAX_END_DEVICE_CHILDREN

The maximum number of children that a node may have.

For the mesh stack, this defaults to the value of EMBER_MAX_END_DEVICE_CHILDREN. In the mesh stack router children are not stored in the child table.

Each child table entry requires 4 bytes of RAM and a 10 byte token.

Application definitions for EMBER_CHILD_TABLE_SIZE that are larger than the default value are ignored and the default value used instead.


Definition at line 205 of file stack/config/ember-configuration-defaults.h

EMBER_KEY_TABLE_SIZE#

#define EMBER_KEY_TABLE_SIZE
Value:
0

The maximum number of link and master keys that a node can store, not including the Trust Center Link Key. The stack maintains special storage for the Trust Center Link Key.

For the Trust Center, this controls how many totally unique Trust Center Link Keys may be stored. The rest of the devices in the network will use a global or hashed link key.

For normal nodes, this controls the number of Application Link Keys it can store. The Trust Center Link Key is stored separately from this table.


Definition at line 222 of file stack/config/ember-configuration-defaults.h

EMBER_CERTIFICATE_TABLE_SIZE#

#define EMBER_CERTIFICATE_TABLE_SIZE
Value:
0

The number of entries for the field upgradeable certificate table. Normally, certificates, such as SE certs, are stored in the runtime-unmodifiable MFG area. However, those devices wishing to add new certificates after manufacturing will have to use the normal token space. This defines the size of that table. For most devices 0 is appropriate since there is no need to change certificates in the field. For those wishing to field upgrade devices with new certificates, 1 is the correct size. Anything more is wasting SimEEPROM.


Definition at line 235 of file stack/config/ember-configuration-defaults.h

EMBER_MAX_DEPTH#

#define EMBER_MAX_DEPTH
Value:
15

The maximum depth of the tree in ZigBee 2006. This implicitly determines the maximum diameter of the network (EMBER_MAX_HOPS) if that value is not overridden.


Definition at line 248 of file stack/config/ember-configuration-defaults.h

EMBER_MAX_HOPS#

#define EMBER_MAX_HOPS
Value:
(2 * EMBER_MAX_DEPTH)

The maximum number of hops for a message.

The default maximum number of hops is two times the maximum depth (EMBER_MAX_DEPTH). This is the fallback value when the radius is not supplied by the Application (i.e., 0) or the stack is sending a message.


Definition at line 261 of file stack/config/ember-configuration-defaults.h

EMBER_PACKET_BUFFER_COUNT#

#define EMBER_PACKET_BUFFER_COUNT
Value:
75

The number of Packet Buffers available to the Stack. The default is 75.

Each buffer requires 36 bytes of RAM (32 for the buffer itself plus 4 bytes of overhead).


Definition at line 271 of file stack/config/ember-configuration-defaults.h

EMBER_MAX_BEACONS_TO_STORE#

#define EMBER_MAX_BEACONS_TO_STORE
Value:
( (EMBER_PACKET_BUFFER_COUNT <= 75) ? (EMBER_PACKET_BUFFER_COUNT >> 1) : 37)

The maximum number of beacons to record when performing an active scan to find networks. Legacy APIs such as emberJoinNetwork and the several emberFindAndRejoinNetwork APIs set the number of beacons to record to 1, while the Network Steering plugin will attempt to record the maximum number of beacons.

It is important not to consume all packet buffers in a system, else the transmission and reception of packets will fail, since TX and RX packets are held in packet buffers.


Definition at line 288 of file stack/config/ember-configuration-defaults.h

BEACON_STORAGE_TIMEOUT_MS#

#define BEACON_STORAGE_TIMEOUT_MS
Value:
(3 * 60 * 1000)

The amount of time after which any caches beacons are purged from the cache in RAM. Each beacon stored consumes one packet buffer. The timeout for beacons begins once the first beacon is added to the cache.


Definition at line 295 of file stack/config/ember-configuration-defaults.h

EMBER_MAX_NEIGHBOR_TABLE_SIZE#

#define EMBER_MAX_NEIGHBOR_TABLE_SIZE
Value:
26

The maximum number of router neighbors the stack can keep track of.

A neighbor is a node within radio range. The maximum allowed value is 26. End device children are stored in the child table, not the neighbor table. The default is 16. Setting this value lower than 8 is not recommended.

Each neighbor table entry consumes 18 bytes of RAM (6 for the table itself and 12 bytes of security data).


Definition at line 309 of file stack/config/ember-configuration-defaults.h

EMBER_NEIGHBOR_TABLE_SIZE#

#define EMBER_NEIGHBOR_TABLE_SIZE
Value:
16

Definition at line 311 of file stack/config/ember-configuration-defaults.h

EMBER_INDIRECT_TRANSMISSION_TIMEOUT#

#define EMBER_INDIRECT_TRANSMISSION_TIMEOUT
Value:
3000

The maximum amount of time (in milliseconds) that the MAC will hold a message for indirect transmission to a child.

The default is 3000 milliseconds (3 sec). The maximum value is 30 seconds (30000 milliseconds). Larger values will cause rollover confusion.


Definition at line 324 of file stack/config/ember-configuration-defaults.h

EMBER_MAX_INDIRECT_TRANSMISSION_TIMEOUT#

#define EMBER_MAX_INDIRECT_TRANSMISSION_TIMEOUT
Value:
30000

Definition at line 326 of file stack/config/ember-configuration-defaults.h

EMBER_SEND_MULTICASTS_TO_SLEEPY_ADDRESS#

#define EMBER_SEND_MULTICASTS_TO_SLEEPY_ADDRESS
Value:
false

Define the behavior for the address that the multicasts are sent to. The normal address is RxOnWhenIdle=true (0xFFFD). However, setting this to true can change locally generated multicasts to be sent to the sleepy broadcast address (0xFFFF). Changing the default is NOT Zigbee Pro compliant and may not be inter-operable.


Definition at line 339 of file stack/config/ember-configuration-defaults.h

EMBER_END_DEVICE_KEEP_ALIVE_SUPPORT_MODE#

#define EMBER_END_DEVICE_KEEP_ALIVE_SUPPORT_MODE
Value:
EMBER_KEEP_ALIVE_SUPPORT_ALL

Definition at line 345 of file stack/config/ember-configuration-defaults.h

SECONDS_10#

#define SECONDS_10
Value:
0

The default index into the R21 Child Aging timeout The default value is a timeout of 256 minutes.


Definition at line 351 of file stack/config/ember-configuration-defaults.h

MINUTES_2#

#define MINUTES_2
Value:
1

Definition at line 352 of file stack/config/ember-configuration-defaults.h

MINUTES_4#

#define MINUTES_4
Value:
2

Definition at line 353 of file stack/config/ember-configuration-defaults.h

MINUTES_8#

#define MINUTES_8
Value:
3

Definition at line 354 of file stack/config/ember-configuration-defaults.h

MINUTES_16#

#define MINUTES_16
Value:
4

Definition at line 355 of file stack/config/ember-configuration-defaults.h

MINUTES_32#

#define MINUTES_32
Value:
5

Definition at line 356 of file stack/config/ember-configuration-defaults.h

MINUTES_64#

#define MINUTES_64
Value:
6

Definition at line 357 of file stack/config/ember-configuration-defaults.h

MINUTES_128#

#define MINUTES_128
Value:
7

Definition at line 358 of file stack/config/ember-configuration-defaults.h

MINUTES_256#

#define MINUTES_256
Value:
8

Definition at line 359 of file stack/config/ember-configuration-defaults.h

MINUTES_512#

#define MINUTES_512
Value:
9

Definition at line 360 of file stack/config/ember-configuration-defaults.h

MINUTES_1024#

#define MINUTES_1024
Value:
10

Definition at line 361 of file stack/config/ember-configuration-defaults.h

MINUTES_2048#

#define MINUTES_2048
Value:
11

Definition at line 362 of file stack/config/ember-configuration-defaults.h

MINUTES_4096#

#define MINUTES_4096
Value:
12

Definition at line 363 of file stack/config/ember-configuration-defaults.h

MINUTES_8192#

#define MINUTES_8192
Value:
13

Definition at line 364 of file stack/config/ember-configuration-defaults.h

MINUTES_16384#

#define MINUTES_16384
Value:
14

Definition at line 365 of file stack/config/ember-configuration-defaults.h

EMBER_END_DEVICE_POLL_TIMEOUT#

#define EMBER_END_DEVICE_POLL_TIMEOUT
Value:
MINUTES_256

Definition at line 368 of file stack/config/ember-configuration-defaults.h

EMBER_SHORT_CHILD_TIMEOUT#

#define EMBER_SHORT_CHILD_TIMEOUT
Value:
MINUTES_2

The temporary, short timeout that is given to a joining or insecurely rejoining child. The child is expected to send a network encrypted packet to set its timeout to the default value.


Definition at line 379 of file stack/config/ember-configuration-defaults.h

EMBER_LINK_POWER_DELTA_INTERVAL#

#define EMBER_LINK_POWER_DELTA_INTERVAL
Value:
300

Definition at line 384 of file stack/config/ember-configuration-defaults.h

EMBER_APS_UNICAST_MESSAGE_COUNT#

#define EMBER_APS_UNICAST_MESSAGE_COUNT
Value:
10

The maximum number of APS retried messages that the stack can transmit at any time. Here, transmitting describes the time between the call to emberSendUnicast() and the subsequent callback to emberMessageSentHandler().

Note

  • A message will typically use one packet buffer for the message header and one or more packet buffers for the payload. The default is 10 messages.

Each APS retried message consumes 6 bytes of RAM and two or more packet buffers.


Definition at line 400 of file stack/config/ember-configuration-defaults.h

SL_ZIGBEE_APS_DUPLICATE_REJECTION_MAX_ENTRIES#

#define SL_ZIGBEE_APS_DUPLICATE_REJECTION_MAX_ENTRIES
Value:
5

Size of 1 is basically the same thing as no duplicate rejection.


Definition at line 407 of file stack/config/ember-configuration-defaults.h

EMBER_BINDING_TABLE_SIZE#

#define EMBER_BINDING_TABLE_SIZE
Value:
0

The maximum number of bindings supported by the stack. The default is 0 bindings. Each binding consumes 2 bytes of RAM.


Definition at line 414 of file stack/config/ember-configuration-defaults.h

EMBER_ADDRESS_TABLE_SIZE#

#define EMBER_ADDRESS_TABLE_SIZE
Value:
8

The maximum number of EUI64<->network address associations that the stack can maintain. The default value is 8.

Address table entries are 10 bytes in size.


Definition at line 422 of file stack/config/ember-configuration-defaults.h

EMBER_ROUTE_TABLE_SIZE#

#define EMBER_ROUTE_TABLE_SIZE
Value:
16

The maximum number of destinations to which a node can route messages. This include both messages originating at this node and those relayed for others. The default value is 16.

Route table entries are 6 bytes in size.


Definition at line 432 of file stack/config/ember-configuration-defaults.h

EMBER_DISCOVERY_TABLE_SIZE#

#define EMBER_DISCOVERY_TABLE_SIZE
Value:
8

The number of simultaneous route discoveries that a node will support.

Discovery table entries are 9 bytes in size.


Definition at line 447 of file stack/config/ember-configuration-defaults.h

EMBER_MULTICAST_TABLE_SIZE#

#define EMBER_MULTICAST_TABLE_SIZE
Value:
8

The maximum number of multicast groups that the device may be a member of. The default value is 8.

Multicast table entries are 3 bytes in size.


Definition at line 460 of file stack/config/ember-configuration-defaults.h

EMBER_SOURCE_ROUTE_TABLE_SIZE#

#define EMBER_SOURCE_ROUTE_TABLE_SIZE
Value:
0

The number of source route table entries if the source route library is not included. The maximum source route table size is 255 entries, since a one-byte index is used, and the index 0xFF is reserved. The default value is 0.

Source route table entries are 4 bytes in size.


Definition at line 470 of file stack/config/ember-configuration-defaults.h

EMBER_MAX_SOURCE_ROUTE_RELAY_COUNT#

#define EMBER_MAX_SOURCE_ROUTE_RELAY_COUNT
Value:
11

Definition at line 474 of file stack/config/ember-configuration-defaults.h

EMBER_DEFAULT_BROADCAST_TABLE_SIZE#

#define EMBER_DEFAULT_BROADCAST_TABLE_SIZE
Value:
15

The maximum number of broadcasts during a single broadcast timeout period. The minimum and default value is 15 and can only be changed on compatible Ember stacks. Be very careful when changing the broadcast table size as it affects timing of the broadcasts and the number of possible broadcasts. Additionally, this value must be universal for all devices in the network. Otherwise, a single router can overwhelm all its neighbors with more broadcasts than they can support. In general, this value should be left alone.

Broadcast table entries are 6 bytes in size.


Definition at line 490 of file stack/config/ember-configuration-defaults.h

EMBER_BROADCAST_TABLE_SIZE#

#define EMBER_BROADCAST_TABLE_SIZE
Value:
EMBER_DEFAULT_BROADCAST_TABLE_SIZE

Definition at line 493 of file stack/config/ember-configuration-defaults.h

EMBER_RETRY_QUEUE_SIZE#

#define EMBER_RETRY_QUEUE_SIZE
Value:
16

Definition at line 501 of file stack/config/ember-configuration-defaults.h

EMBER_STORE_AND_FORWARD_QUEUE_SIZE#

#define EMBER_STORE_AND_FORWARD_QUEUE_SIZE
Value:
5

Definition at line 505 of file stack/config/ember-configuration-defaults.h

EMBER_ASSERT_SERIAL_PORT#

#define EMBER_ASSERT_SERIAL_PORT
Value:
1

Settings to control if and where assert information will be printed.

The output can be suppressed by defining EMBER_ASSERT_OUTPUT_DISABLED. The serial port to which the output is sent can be changed by defining EMBER_ASSERT_SERIAL_PORT as the desired port.

The default is to have the assert output on and sent to serial port 1.


Definition at line 519 of file stack/config/ember-configuration-defaults.h

EMBER_FRAGMENT_DELAY_MS#

#define EMBER_FRAGMENT_DELAY_MS
Value:
0

The time the stack will wait (in milliseconds) between sending blocks of a fragmented message. The default value is 0.


Definition at line 526 of file stack/config/ember-configuration-defaults.h

EMBER_FRAGMENT_MAX_WINDOW_SIZE#

#define EMBER_FRAGMENT_MAX_WINDOW_SIZE
Value:
8

The maximum number of blocks of a fragmented message that can be sent in a single window is defined to be 8.


Definition at line 532 of file stack/config/ember-configuration-defaults.h

EMBER_FRAGMENT_WINDOW_SIZE#

#define EMBER_FRAGMENT_WINDOW_SIZE
Value:
1

The number of blocks of a fragmented message that can be sent in a single window. The maximum is EMBER_FRAGMENT_MAX_WINDOW_SIZE. The default value is 1.


Definition at line 539 of file stack/config/ember-configuration-defaults.h

EMBER_REQUEST_KEY_TIMEOUT#

#define EMBER_REQUEST_KEY_TIMEOUT
Value:
0

The length of time that the device will wait for an answer to its Application Key Request. For the Trust Center, this is the time it will hold the first request and wait for a second matching request. If both arrive within this time period, the Trust Center will reply to both with the new key. If both requests are not received, the Trust Center will discard the request. The time is in minutes, with the maximum time being 10 minutes. A value of 0 minutes indicates that the Trust Center will not buffer the request but instead respond immediately. Only 1 outstanding request is supported at a time.

The Zigbee Pro Compliant value is 0.


Definition at line 557 of file stack/config/ember-configuration-defaults.h

EMBER_TRANSIENT_KEY_TIMEOUT_S#

#define EMBER_TRANSIENT_KEY_TIMEOUT_S
Value:
(300)

The length of time, in seconds, that a trust center will store a transient link key that a device can use to join its network. A transient key is added with a call to sl_zb_sec_man_import_transient_key. After the transient key is added, it will be removed once this amount of time has passed. A joining device will not be able to use that key to join until it is added again on the trust center. The default value is 300 seconds, i.e., 5 minutes.


Definition at line 571 of file stack/config/ember-configuration-defaults.h

EMBER_TRANSIENT_KEY_SESSION_TIMEOUT_VAL#

#define EMBER_TRANSIENT_KEY_SESSION_TIMEOUT_VAL
Value:
0xFFFF

A reserved emberTransientKeyTimeoutS value that, when stored with a "transient" key, prevents its removal from the transient key table when the session is active. Note that some standard security procedures (e.g. Zigbee Direct) require session keys to remain active indefinitely for the duration of the of the exchange.


Definition at line 581 of file stack/config/ember-configuration-defaults.h

EMBER_PAN_ID_CONFLICT_REPORT_THRESHOLD#

#define EMBER_PAN_ID_CONFLICT_REPORT_THRESHOLD
Value:
2

The number of PAN ID conflict reports that must be received by the network manager within one minute to trigger a PAN ID change. Very rarely, a corrupt beacon can pass the CRC check and trigger a false PAN id conflict. This is more likely to happen in very large dense networks. Setting this value to 2 or 3 dramatically reduces the chances of a spurious PAN ID change. The maximum value is 63. The default value is 2.


Definition at line 593 of file stack/config/ember-configuration-defaults.h

EMBER_MAX_NETWORK_RETRIES#

#define EMBER_MAX_NETWORK_RETRIES
Value:
15

The number of network level retries before network layer gives up sending a message, and return with an error. This could be seen as an extension to mac retries, and can take a range between 0..15. Setting the value to 0 disables network retries.


Definition at line 601 of file stack/config/ember-configuration-defaults.h

EMBER_ZIGBEE_NUM_NETWORK_RETRIES_DEFAULT#

#define EMBER_ZIGBEE_NUM_NETWORK_RETRIES_DEFAULT
Value:
15

Definition at line 603 of file stack/config/ember-configuration-defaults.h

EMBER_TASK_COUNT#

#define EMBER_TASK_COUNT
Value:
(5)

The number of event tasks that can be tracked for the purpose of processor idling. The Ember Zigbee Pro Stack requires two tasks, an application and associated libraries may use additional tasks, though typically no more than 5 are needed for most applications.


Definition at line 615 of file stack/config/ember-configuration-defaults.h

EMBER_MAX_SUPPORTED_NETWORKS#

#define EMBER_MAX_SUPPORTED_NETWORKS
Value:
2

The number of networks supported by the stack.


Definition at line 620 of file stack/config/ember-configuration-defaults.h

EMBER_SUPPORTED_NETWORKS#

#define EMBER_SUPPORTED_NETWORKS
Value:
1

Definition at line 623 of file stack/config/ember-configuration-defaults.h

EMBER_ZLL_GROUP_ADDRESSES#

#define EMBER_ZLL_GROUP_ADDRESSES
Value:
1

The number of unique group identifiers that this device requires.


Definition at line 645 of file stack/config/ember-configuration-defaults.h

EMBER_ZLL_RSSI_THRESHOLD#

#define EMBER_ZLL_RSSI_THRESHOLD
Value:
-128

The RSSI threshold applied to incoming scan requests.


Definition at line 651 of file stack/config/ember-configuration-defaults.h

EMBER_GP_PROXY_TABLE_SIZE#

#define EMBER_GP_PROXY_TABLE_SIZE
Value:
5

The number of proxy table entries supported.


Definition at line 657 of file stack/config/ember-configuration-defaults.h

EMBER_GP_SINK_TABLE_SIZE#

#define EMBER_GP_SINK_TABLE_SIZE
Value:
0

The number of sink table entries supported.


Definition at line 663 of file stack/config/ember-configuration-defaults.h

EMBER_GP_INCOMING_FC_TOKEN_TIMEOUT#

#define EMBER_GP_INCOMING_FC_TOKEN_TIMEOUT
Value:
7

The timeout (seconds) to restore the GPD incoming security frame counter in the Flash (0 being never).


Definition at line 669 of file stack/config/ember-configuration-defaults.h

EMBER_GP_INCOMING_FC_TOKEN_TABLE_SIZE#

#define EMBER_GP_INCOMING_FC_TOKEN_TABLE_SIZE
Value:
0

The maximum table size to restore the GPD incoming security frame counter in the Flash (being either 0 or EMBER_GP_PROXY_TABLE_SIZE).


Definition at line 675 of file stack/config/ember-configuration-defaults.h

EMBER_GP_INCOMING_FC_IN_SINK_TOKEN_TIMEOUT#

#define EMBER_GP_INCOMING_FC_IN_SINK_TOKEN_TIMEOUT
Value:
7

The timeout (seconds) to restore the GPD incoming security frame counter in the Flash (0 being never).


Definition at line 681 of file stack/config/ember-configuration-defaults.h

EMBER_GP_INCOMING_FC_IN_SINK_TOKEN_TABLE_SIZE#

#define EMBER_GP_INCOMING_FC_IN_SINK_TOKEN_TABLE_SIZE
Value:
0

The maximum table size to restore the GPD incoming security frame counter in the Flash (being either 0 or EMBER_GP_SINK_TABLE_SIZE).


Definition at line 687 of file stack/config/ember-configuration-defaults.h

EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED#

#define EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED
Value:
2

The maximum number of ZC and ZR devices can be supported in a multi network mode. All the ZC and ZR devices are expected to be on the same channel with different PAN IDs. Multi network with multiple ZC and ZR devices are supported only on EFR platform.


Definition at line 694 of file stack/config/ember-configuration-defaults.h

EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED#

#define EMBER_MULTI_NETWORK_MAX_ZC_AND_ZR_DEVICES_SUPPORTED
Value:
EMBER_SUPPORTED_NETWORKS

The maximum number of ZC and ZR devices can be supported in a multi network mode. All the ZC and ZR devices are expected to be on the same channel with different PAN IDs. Multi network with multiple ZC and ZR devices are supported only on EFR platform.


Definition at line 697 of file stack/config/ember-configuration-defaults.h

NETWORK_0_ZC_AND_ZR_COUNT#

#define NETWORK_0_ZC_AND_ZR_COUNT
Value:
(1)

The number of ZC and ZR device types are present in the application. This configuration is used to expand the various stack tables and events required to support the multi PAN application. Note that for SoC, this define is generated by app builder based on the device type(s) present in the application.


Definition at line 711 of file stack/config/ember-configuration-defaults.h

NETWORK_1_ZC_AND_ZR_COUNT#

#define NETWORK_1_ZC_AND_ZR_COUNT
Value:
(0)

Definition at line 724 of file stack/config/ember-configuration-defaults.h

EMBER_ZC_AND_ZR_DEVICE_COUNT#

#define EMBER_ZC_AND_ZR_DEVICE_COUNT
Value:
(NETWORK_0_ZC_AND_ZR_COUNT + NETWORK_1_ZC_AND_ZR_COUNT)

Definition at line 734 of file stack/config/ember-configuration-defaults.h

SL_ZIGBEE_TRANSIENT_DEVICE_MGMT_MAX_CAPACITY#

#define SL_ZIGBEE_TRANSIENT_DEVICE_MGMT_MAX_CAPACITY
Value:
64

Definition at line 763 of file stack/config/ember-configuration-defaults.h

SL_ZIGBEE_TRANSIENT_DEVICE_DEFAULT_TIMEOUT_MS#

#define SL_ZIGBEE_TRANSIENT_DEVICE_DEFAULT_TIMEOUT_MS
Value:
(10000u)

Definition at line 771 of file stack/config/ember-configuration-defaults.h

SL_ZIGBEE_ENABLE_APS_ACKS_FOR_COMMANDS#

#define SL_ZIGBEE_ENABLE_APS_ACKS_FOR_COMMANDS
Value:
(false)

Definition at line 778 of file stack/config/ember-configuration-defaults.h

EMBER_CUSTOM_MAC_FILTER_TABLE_SIZE#

#define EMBER_CUSTOM_MAC_FILTER_TABLE_SIZE
Value:
2

Definition at line 782 of file stack/config/ember-configuration-defaults.h

SL_ZIGBEE_ZDO_BEACON_SURVEY_MAX_UNIQUE_NETWORKS#

#define SL_ZIGBEE_ZDO_BEACON_SURVEY_MAX_UNIQUE_NETWORKS
Value:
8

The 802.15.4 CCA mode that should be used at startup. The default value is RAIL_IEEE802154_CCA_MODE_RSSI. This value is configured in the radio during initialization. The user may override this value at runtime using emberSetRadioIeee802154CcaMode.

Note

  • The value of this macro is used at startup for SoC and NCP applications only. A host application does not use this value, nor does it set the CCA mode at startup by default.

the number of beacons to store when performing a beacon survey scan


Definition at line 810 of file stack/config/ember-configuration-defaults.h