This data structure contains the transient key data that is used during Zigbee 3.0 joining.
Public Attribute Documentation#
eui64#
EmberEUI64 EmberTransientKeyData::eui64
Definition at line
2333
of file stack/include/ember-types.h
incomingFrameCounter#
uint32_t EmberTransientKeyData::incomingFrameCounter
Definition at line
2334
of file stack/include/ember-types.h
bitmask#
EmberKeyStructBitmask EmberTransientKeyData::bitmask
Definition at line
2335
of file stack/include/ember-types.h
remainingTimeSeconds#
uint16_t EmberTransientKeyData::remainingTimeSeconds
Definition at line
2336
of file stack/include/ember-types.h
networkIndex#
uint8_t EmberTransientKeyData::networkIndex
Definition at line
2337
of file stack/include/ember-types.h
keyData#
EmberKeyData EmberTransientKeyData::keyData
Definition at line
2339
of file stack/include/ember-types.h
psa_id#
uint32_t EmberTransientKeyData::psa_id
Definition at line
2340
of file stack/include/ember-types.h
@3#
union EmberTransientKeyData::@2 EmberTransientKeyData::@3
Definition at line
2341
of file stack/include/ember-types.h