Cluster Commands: Configuration Cluster#
This group describes the CLI commands for the Configuration Cluster cluster. Listed below is a description of the cluster:
This cluster allows for the OTA configuration of firmware parameters.
Macros#
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_SET_TOKEN
zcl ota-config setToken [token:2] [data:-1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_LOCK
zcl ota-config lock
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_READ
zcl ota-config read [token:2]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_CONFIGURATION_CLUSTER_UNLOCK
zcl ota-config unlock [data:-1]