Ember ZigBee Light Link (ZLL) Data Types#
See zll-types.h for source code.
Modules#
ZigBee Light Link Types#
A bitmask indicating the state of the ZLL device. This maps directly to the ZLL information field in the scan response.
The key encryption algorithms supported by the stack.
This enumeration indicates whether or not the stack processes ZLL messages.
The list of primary ZLL channels.
The list of secondary ZLL channels.
A distinguished network identifier in the ZLL network address space that indicates no free network identifiers were assigned to the device.
The minimum network identifier in the ZLL network address space.
The maximum network identifier in the ZLL network address space.
A distinguished group identifier in the ZLL group address space that indicates no free group identifiers were assigned to the device.
The minimum group identifier in the ZLL group address space.
The maximum group identifier in the ZLL group address space.
The ZigBee Light Link Commissioning cluster ID.
The ZigBee Light Link Profile ID.
The key encryption bitmask corresponding to encryption key index EMBER_ZLL_KEY_INDEX_DEVELOPMENT.
The key encryption bitmask corresponding to encryption key index EMBER_ZLL_KEY_INDEX_MASTER.
THe key encryption bitmask corresponding to encryption key index EMBER_ZLL_KEY_INDEX_CERTIFICATION.
The encryption key for use during development and certification in conjunction with EMBER_ZLL_KEY_INDEX_CERTIFICATION.
The pre-configured link key for use during development and certification in conjunction with EMBER_ZLL_KEY_INDEX_CERTIFICATION.
Variables#
ZigBee Light Link Types Documentation#
EmberZllState#
EmberZllState
A bitmask indicating the state of the ZLL device. This maps directly to the ZLL information field in the scan response.
| Enumerator | |
|---|---|
| EMBER_ZLL_STATE_NONE | No state. |
| EMBER_ZLL_STATE_FACTORY_NEW | The device is factory new. |
| EMBER_ZLL_STATE_ADDRESS_ASSIGNMENT_CAPABLE | The device is capable of assigning addresses to other devices. |
| EMBER_ZLL_STATE_LINK_INITIATOR | The device is initiating a link operation. |
| EMBER_ZLL_STATE_LINK_PRIORITY_REQUEST | The device is requesting link priority. |
| EMBER_ZLL_STATE_PROFILE_INTEROP | The device is a ZigBee 3.0 device. |
| EMBER_ZLL_STATE_NON_ZLL_NETWORK | The device is on a non-ZLL network. |
| EMBER_ZLL_TOKEN_POINTS_TO_PSA_ID | Internal use: the ZLL token's key values point to a PSA key identifier |
EmberZllKeyIndex#
EmberZllKeyIndex
The key encryption algorithms supported by the stack.
| Enumerator | |
|---|---|
| EMBER_ZLL_KEY_INDEX_DEVELOPMENT | The key encryption algorithm for use during development. |
| EMBER_ZLL_KEY_INDEX_MASTER | The key encryption algorithm shared by all certified devices. |
| EMBER_ZLL_KEY_INDEX_CERTIFICATION | The key encryption algorithm for use during development and certification. |
EmberZllPolicy#
EmberZllPolicy
This enumeration indicates whether or not the stack processes ZLL messages.
| Enumerator | |
|---|---|
| EMBER_ZLL_POLICY_DISABLED | Initial state - all touchlinking is disabled. |
| EMBER_ZLL_POLICY_ENABLED | Indicates that ZLL processing is enabled. |
| EMBER_ZLL_POLICY_TARGET | Indicates that ZLL target is enabled. |
| EMBER_ZLL_POLICY_STEALING_ENABLED | Indicates that stealing and network update are enabled for non factory new devices. |
| EMBER_ZLL_POLICY_REMOTE_RESET_ENABLED | Indicates that remote reset is enabled for non factory new devices. |
Variable Documentation#
bitmask#
uint32_t EmberZllInitialSecurityState::bitmask
This bitmask is unused. All values are reserved for future use.
keyIndex#
EmberZllKeyIndex EmberZllInitialSecurityState::keyIndex
The key encryption algorithm advertised by the application.
encryptionKey#
EmberKeyData EmberZllInitialSecurityState::encryptionKey
The encryption key for use by algorithms that require it.
preconfiguredKey#
EmberKeyData EmberZllInitialSecurityState::preconfiguredKey
The pre-configured link key used during classical ZigBee commissioning.