Information about the ZLL network and specific device that responded to a ZLL scan request.

Public Attribute Documentation#

zigbeeNetwork#

sl_zigbee_zigbee_network_t sl_zigbee_zll_network_t::zigbeeNetwork

Definition at line 137 of file stack/include/zll-types.h

securityAlgorithm#

sl_zigbee_zll_security_algorithm_data_t sl_zigbee_zll_network_t::securityAlgorithm

Definition at line 138 of file stack/include/zll-types.h

eui64#

sl_802154_long_addr_t sl_zigbee_zll_network_t::eui64

Definition at line 139 of file stack/include/zll-types.h

nodeId#

sl_802154_short_addr_t sl_zigbee_zll_network_t::nodeId

Definition at line 140 of file stack/include/zll-types.h

state#

sl_zigbee_zll_state_t sl_zigbee_zll_network_t::state

Definition at line 141 of file stack/include/zll-types.h

nodeType#

sl_zigbee_node_type_t sl_zigbee_zll_network_t::nodeType

Definition at line 142 of file stack/include/zll-types.h

numberSubDevices#

uint8_t sl_zigbee_zll_network_t::numberSubDevices

Definition at line 143 of file stack/include/zll-types.h

totalGroupIdentifiers#

uint8_t sl_zigbee_zll_network_t::totalGroupIdentifiers

Definition at line 144 of file stack/include/zll-types.h

rssiCorrection#

uint8_t sl_zigbee_zll_network_t::rssiCorrection

Definition at line 145 of file stack/include/zll-types.h