ZLL Commissioning#
Callbacks for ZLL Commissioning Component.
Callbacks#
void
sl_zigbee_af_zll_commissioning_client_touch_link_failed_cb(sl_zigbee_af_zll_commissioning_status_t status)
Touch link failed.
Macros#
#define
sl_zigbee_af_zll_commissioning_touch_link_failed_cb sl_zigbee_af_zll_commissioning_client_touch_link_failed_cb
Callbacks Documentation#
sl_zigbee_af_zll_commissioning_client_touch_link_failed_cb#
void sl_zigbee_af_zll_commissioning_client_touch_link_failed_cb (sl_zigbee_af_zll_commissioning_status_t status)
Touch link failed.
Parameters
N/A | status | The reason the touch link failed. Ver.: always |
This function is called by the ZLL Commissioning Client plugin if touch linking fails.
Definition at line
138
of file app/framework/plugin/zll-commissioning-client/zll-commissioning-client.h
Macro Definition Documentation#
sl_zigbee_af_zll_commissioning_touch_link_failed_cb#
#define sl_zigbee_af_zll_commissioning_touch_link_failed_cbValue:
sl_zigbee_af_zll_commissioning_client_touch_link_failed_cb
Definition at line
143
of file app/framework/plugin/zll-commissioning-client/zll-commissioning-client.h